<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックDo we have any XML library compatible to USB drivers from the KSDKv2.0?</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Do-we-have-any-XML-library-compatible-to-USB-drivers-from-the/m-p/582967#M5922</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to parse an XML file from the USB. so do we have any library compatible Kinetis&amp;nbsp;based USB drivers? As the USB API's uses the FIL pointer which is having a different structure than the normally used FILE pointer. Also, I am using FRDM-K22F board along with KSDKv2.0.&lt;/P&gt;&lt;P&gt;Thanks in advance. :-)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Vishal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Sep 2016 12:07:10 GMT</pubDate>
    <dc:creator>vishalwankar</dc:creator>
    <dc:date>2016-09-01T12:07:10Z</dc:date>
    <item>
      <title>Do we have any XML library compatible to USB drivers from the KSDKv2.0?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Do-we-have-any-XML-library-compatible-to-USB-drivers-from-the/m-p/582967#M5922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to parse an XML file from the USB. so do we have any library compatible Kinetis&amp;nbsp;based USB drivers? As the USB API's uses the FIL pointer which is having a different structure than the normally used FILE pointer. Also, I am using FRDM-K22F board along with KSDKv2.0.&lt;/P&gt;&lt;P&gt;Thanks in advance. :-)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Vishal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Sep 2016 12:07:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Do-we-have-any-XML-library-compatible-to-USB-drivers-from-the/m-p/582967#M5922</guid>
      <dc:creator>vishalwankar</dc:creator>
      <dc:date>2016-09-01T12:07:10Z</dc:date>
    </item>
    <item>
      <title>Re: Do we have any XML library compatible to USB drivers from the KSDKv2.0?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Do-we-have-any-XML-library-compatible-to-USB-drivers-from-the/m-p/582968#M5923</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Vishal,&lt;/P&gt;&lt;P&gt;As far as I know the we have not any library compatible Kinetis&amp;nbsp;based USB drivers, the Kinetis driver in SDK is low level driver instead of high level driver, we can transfer message or datas based on Kinetis USB driver in SDK.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2016 02:31:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Do-we-have-any-XML-library-compatible-to-USB-drivers-from-the/m-p/582968#M5923</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-09-02T02:31:05Z</dc:date>
    </item>
  </channel>
</rss>