<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックSDK 2.0 SPI without RX</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SDK-2-0-SPI-without-RX/m-p/558388#M5726</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use the SPI driver to transmit data. However, I do not wish to receive data.&lt;/P&gt;&lt;P&gt;Using the SDK 2.0 driver, am I required to create a RX buffer that is the same size as my TX buffer? How do I tell it otherwise?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Aug 2016 13:33:31 GMT</pubDate>
    <dc:creator>ETCTim</dc:creator>
    <dc:date>2016-08-01T13:33:31Z</dc:date>
    <item>
      <title>SDK 2.0 SPI without RX</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SDK-2-0-SPI-without-RX/m-p/558388#M5726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use the SPI driver to transmit data. However, I do not wish to receive data.&lt;/P&gt;&lt;P&gt;Using the SDK 2.0 driver, am I required to create a RX buffer that is the same size as my TX buffer? How do I tell it otherwise?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Aug 2016 13:33:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SDK-2-0-SPI-without-RX/m-p/558388#M5726</guid>
      <dc:creator>ETCTim</dc:creator>
      <dc:date>2016-08-01T13:33:31Z</dc:date>
    </item>
    <item>
      <title>Re: SDK 2.0 SPI without RX</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SDK-2-0-SPI-without-RX/m-p/558389#M5727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, it can only send not receive .&lt;/P&gt;&lt;P&gt;Please try define the receive buffer to NULL .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Aug 2016 03:45:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SDK-2-0-SPI-without-RX/m-p/558389#M5727</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-08-02T03:45:23Z</dc:date>
    </item>
  </channel>
</rss>