<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Incorrecte baudrate in FRDM-K64F flexcan example</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Incorrecte-baudrate-in-FRDM-K64F-flexcan-example/m-p/553859#M5695</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to run the flexcan_loopback example in the SDK 2.0 IAR for FRDM-K64F.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I changed the UART instance to UART4, and changed the MUX for the correct pins, and activated the clocks for PORTE.&lt;BR /&gt;Despite that, no changes from standard. But the problem is, the output baudrate is half the specified. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In BOARD_InitDebugConsole, uartClkSrcFreq is set to 120MHz. I don't know if that is correct.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas? Is it system clock that is wrong or only the uart baudrate?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Jun 2016 10:08:57 GMT</pubDate>
    <dc:creator>johanwallstrom</dc:creator>
    <dc:date>2016-06-21T10:08:57Z</dc:date>
    <item>
      <title>Incorrecte baudrate in FRDM-K64F flexcan example</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Incorrecte-baudrate-in-FRDM-K64F-flexcan-example/m-p/553859#M5695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to run the flexcan_loopback example in the SDK 2.0 IAR for FRDM-K64F.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I changed the UART instance to UART4, and changed the MUX for the correct pins, and activated the clocks for PORTE.&lt;BR /&gt;Despite that, no changes from standard. But the problem is, the output baudrate is half the specified. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In BOARD_InitDebugConsole, uartClkSrcFreq is set to 120MHz. I don't know if that is correct.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas? Is it system clock that is wrong or only the uart baudrate?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jun 2016 10:08:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Incorrecte-baudrate-in-FRDM-K64F-flexcan-example/m-p/553859#M5695</guid>
      <dc:creator>johanwallstrom</dc:creator>
      <dc:date>2016-06-21T10:08:57Z</dc:date>
    </item>
    <item>
      <title>Re: Incorrecte baudrate in FRDM-K64F flexcan example</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Incorrecte-baudrate-in-FRDM-K64F-flexcan-example/m-p/553860#M5696</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Johan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In K64's reference manual &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/ref_manual/K64P144M120SF5RM.pdf" rel="nofollow noopener noreferrer" title="http://cache.freescale.com/files/microcontrollers/doc/ref_manual/K64P144M120SF5RM.pdf" target="_blank"&gt;http://cache.freescale.com/files/microcontrollers/doc/ref_manual/K64P144M120SF5RM.pdf&lt;/A&gt; , there is a section called Clock distribution (chapter 5), in which, it specifies different clock sources for all available modules in K64. In section 5.7.10 UART clocking section, it expresses:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;" UART0 and UART1 modules operate from the core/system clock, which provides higher performance level for these modules. All other UART modules operate from the bus clock."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And as MCU is operating in PEE modue, System clock is configured to 120MHz while Bus clock is set to 60MHz. So, source clock value is the problem you are facing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can substitute the definition:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="_jivemacro_uid_14665369392342424 jive_macro_code jive_text_macro" data-renderedposition="268_8_1192_16" jivemacro_uid="_14665369392342424" modifiedtitle="true"&gt;&lt;P&gt;#define BOARD_DEBUG_UART_CLK_FREQ CLOCK_GetCoreSysClkFreq()&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;by:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code jive_text_macro _jivemacro_uid_14665369687196385" data-renderedposition="310_8_1192_16" jivemacro_uid="_14665369687196385" modifiedtitle="true"&gt;&lt;P&gt;#define BOARD_DEBUG_UART_CLK_FREQ CLOCK_GetBusClkFreq()&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then recompile the project and it should be working well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this can help you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Isaac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jun 2016 19:23:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Incorrecte-baudrate-in-FRDM-K64F-flexcan-example/m-p/553860#M5696</guid>
      <dc:creator>isaacavila</dc:creator>
      <dc:date>2016-06-21T19:23:31Z</dc:date>
    </item>
    <item>
      <title>Re: Incorrecte baudrate in FRDM-K64F flexcan example</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Incorrecte-baudrate-in-FRDM-K64F-flexcan-example/m-p/553861#M5697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;that works perfectly! &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you so much!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Johan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jun 2016 06:45:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Incorrecte-baudrate-in-FRDM-K64F-flexcan-example/m-p/553861#M5697</guid>
      <dc:creator>johanwallstrom</dc:creator>
      <dc:date>2016-06-22T06:45:48Z</dc:date>
    </item>
  </channel>
</rss>