<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KSDK2.0 USB HID Generic demo, is there a Windows demo ? in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK2-0-USB-HID-Generic-demo-is-there-a-Windows-demo/m-p/552455#M5668</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;In the KSDK for K24f and K64f devices there is demonstration code for USB HID device implementation, so I am looking on the NXP software pages for demo Windows PC application code that works with these HID demo's to verify connectivity and data transfer and then integrate that functionality into a application that can send/receive data structures holding application specific information. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I looked into the code for the new Kinetis Bootloader 2.0 that works over USB-hid to see how that is implemented &lt;/P&gt;&lt;P&gt;and noticed it uses HIDAPI - Multi-Platform library for communication with HID devices written by Alan Ott Signal 11 Software. I had previously considered using this library so can review the bootloader and flash loader code and develop based on the principles used, this approach could take considerable time.&amp;nbsp; If NXP released a simple windows demo application that works with the Generic HIS device code in KSDK2.0 that would be ideal.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the bootloader code the best point of reference for developing the Windows application code, or is there a windows demo that I have missed?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Jul 2016 05:46:22 GMT</pubDate>
    <dc:creator>chadwilliams</dc:creator>
    <dc:date>2016-07-29T05:46:22Z</dc:date>
    <item>
      <title>KSDK2.0 USB HID Generic demo, is there a Windows demo ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK2-0-USB-HID-Generic-demo-is-there-a-Windows-demo/m-p/552455#M5668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;In the KSDK for K24f and K64f devices there is demonstration code for USB HID device implementation, so I am looking on the NXP software pages for demo Windows PC application code that works with these HID demo's to verify connectivity and data transfer and then integrate that functionality into a application that can send/receive data structures holding application specific information. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I looked into the code for the new Kinetis Bootloader 2.0 that works over USB-hid to see how that is implemented &lt;/P&gt;&lt;P&gt;and noticed it uses HIDAPI - Multi-Platform library for communication with HID devices written by Alan Ott Signal 11 Software. I had previously considered using this library so can review the bootloader and flash loader code and develop based on the principles used, this approach could take considerable time.&amp;nbsp; If NXP released a simple windows demo application that works with the Generic HIS device code in KSDK2.0 that would be ideal.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the bootloader code the best point of reference for developing the Windows application code, or is there a windows demo that I have missed?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jul 2016 05:46:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK2-0-USB-HID-Generic-demo-is-there-a-Windows-demo/m-p/552455#M5668</guid>
      <dc:creator>chadwilliams</dc:creator>
      <dc:date>2016-07-29T05:46:22Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK2.0 USB HID Generic demo, is there a Windows demo ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK2-0-USB-HID-Generic-demo-is-there-a-Windows-demo/m-p/552456#M5669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chad,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately there is no such windows demo - or I haven´t heard about it yet.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Iva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Aug 2016 13:48:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK2-0-USB-HID-Generic-demo-is-there-a-Windows-demo/m-p/552456#M5669</guid>
      <dc:creator>ivadorazinova</dc:creator>
      <dc:date>2016-08-18T13:48:55Z</dc:date>
    </item>
  </channel>
</rss>