<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックTWR-K70F120M kit - does the demo use the TSI (Touch Sense Input) module, or is it running custom code for touch sense? I can't find the project on the website, so I can't check the code myself.</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/TWR-K70F120M-kit-does-the-demo-use-the-TSI-Touch-Sense-Input/m-p/549749#M5629</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've experienced some buggy behavior using the TWR-K70 touch sense buttons. I'd like to confirm that the kit is actually running the nxp TSI module code, or if it is custom. THe quick start guide says "download the demonstration labs at freescale.com/TWR-K70F120M", but of course there are no such labs there (AFAIK). Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Jul 2016 19:59:25 GMT</pubDate>
    <dc:creator>arthurroberts</dc:creator>
    <dc:date>2016-07-28T19:59:25Z</dc:date>
    <item>
      <title>TWR-K70F120M kit - does the demo use the TSI (Touch Sense Input) module, or is it running custom code for touch sense? I can't find the project on the website, so I can't check the code myself.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/TWR-K70F120M-kit-does-the-demo-use-the-TSI-Touch-Sense-Input/m-p/549749#M5629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've experienced some buggy behavior using the TWR-K70 touch sense buttons. I'd like to confirm that the kit is actually running the nxp TSI module code, or if it is custom. THe quick start guide says "download the demonstration labs at freescale.com/TWR-K70F120M", but of course there are no such labs there (AFAIK). Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 19:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/TWR-K70F120M-kit-does-the-demo-use-the-TSI-Touch-Sense-Input/m-p/549749#M5629</guid>
      <dc:creator>arthurroberts</dc:creator>
      <dc:date>2016-07-28T19:59:25Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K70F120M kit - does the demo use the TSI (Touch Sense Input) module, or is it running custom code for touch sense? I can't find the project on the website, so I can't check the code myself.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/TWR-K70F120M-kit-does-the-demo-use-the-TSI-Touch-Sense-Input/m-p/549750#M5630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arthur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please go to &lt;A href="http://www.nxp.com/products/software-and-tools/hardware-development-tools/tower-development-boards/mcu-and-processor-modules/kinetis-modules/kinetis-k70-120-mhz-tower-system-module:TWR-K70F120M?fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.nxp.com/products/software-and-tools/hardware-development-tools/tower-development-boards/mcu-and-processor-modules/kinetis-modules/kinetis-k70-120-mhz-tower-system-module:TWR-K70F120M?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;TWR-K70F120M|Tower System Board|Kinetis MCUs|NXP&lt;/A&gt; and download demonstration labs here&lt;/P&gt;&lt;H3&gt;&lt;A class="dtmAssetClick" data-dtmassettype="Download" data-dtmname="Kinetis 120MHz bare metal sample code" href="http://www.nxp.com/webapp/sps/download/license.jsp?colCode=KINETIS_120MHZ_SC&amp;amp;location=null&amp;amp;Parent_nodeId=1322538641013716882290&amp;amp;Parent_pageType=product" target="_blank"&gt;Kinetis 120MHz bare metal sample code&lt;/A&gt;&lt;SPAN class="small-rev"&gt; &lt;/SPAN&gt;&lt;/H3&gt;&lt;P&gt;&lt;SPAN class="small-rev"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="small-rev"&gt;there are some sample codes, for example TSI demo lowpower which is located under&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="small-rev"&gt; &amp;lt;KINETIS_120MHZ_SC\KINETIS_120MHZ_SC_path&amp;gt;\build\&amp;lt;iar/cw&amp;gt;\TSI_demo_lowpower&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="small-rev"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="small-rev"&gt;I hope this helps you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="small-rev"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="small-rev"&gt;Iva&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Aug 2016 14:54:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/TWR-K70F120M-kit-does-the-demo-use-the-TSI-Touch-Sense-Input/m-p/549750#M5630</guid>
      <dc:creator>ivadorazinova</dc:creator>
      <dc:date>2016-08-01T14:54:46Z</dc:date>
    </item>
  </channel>
</rss>