<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックRe: SDK 2.0 I2C driver is not properly detecting stop events when master is reading data</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SDK-2-0-I2C-driver-is-not-properly-detecting-stop-events-when/m-p/533198#M5538</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sorry, but I don't think you have to remove the ifdef I2C_HAS_STOP_DETECT and force the kI2C_SlaveCompletionEvent, because the i2c slave interrupt handler sets this event when STOP flag is set, please kindly refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37343i18069A977C825108/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and kI2C_StopDetectFlag is checked in I2C_SlaveGetStatusFlags().&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Jul 2016 03:51:21 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2016-07-26T03:51:21Z</dc:date>
    <item>
      <title>SDK 2.0 I2C driver is not properly detecting stop events when master is reading data</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SDK-2-0-I2C-driver-is-not-properly-detecting-stop-events-when/m-p/533197#M5537</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I am using the SDK 2.0 I2C driver with FreeRTOS on a KL16. I am setting up as an I2C slave. I am finding that the driver is not properly detecting stop events when the master is reading data from the slave. Instead the driver continues to send data to the D register and eventually returns an NAK event.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Using an I2C sniffer I can see that the bus did, in fact, send a stop and moves on to communicating to the next device on the bus. For now my solution has been to remove the ifdef I2C_HAS_STOP_DETECT and force the kI2C_SlaveCompletionEvent when I know the entire packet has been read by the master. But I would rather it did not work this way.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The code is nearly identical to the freeRTOS I2C example.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jul 2016 17:43:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SDK-2-0-I2C-driver-is-not-properly-detecting-stop-events-when/m-p/533197#M5537</guid>
      <dc:creator>davidfindlay</dc:creator>
      <dc:date>2016-07-22T17:43:04Z</dc:date>
    </item>
    <item>
      <title>Re: SDK 2.0 I2C driver is not properly detecting stop events when master is reading data</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SDK-2-0-I2C-driver-is-not-properly-detecting-stop-events-when/m-p/533198#M5538</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sorry, but I don't think you have to remove the ifdef I2C_HAS_STOP_DETECT and force the kI2C_SlaveCompletionEvent, because the i2c slave interrupt handler sets this event when STOP flag is set, please kindly refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37343i18069A977C825108/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and kI2C_StopDetectFlag is checked in I2C_SlaveGetStatusFlags().&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jul 2016 03:51:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SDK-2-0-I2C-driver-is-not-properly-detecting-stop-events-when/m-p/533198#M5538</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2016-07-26T03:51:21Z</dc:date>
    </item>
  </channel>
</rss>