<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックRe: Information on building required KSDK libraries.</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355791#M539</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First, to answer your question, I'm using KDS 2.0.0with KSDK 1.1.0 on a &lt;/P&gt;&lt;P&gt;Windows 7 system. The KDS and KSDK are both installed to C:\Freescale. &lt;/P&gt;&lt;P&gt;My project is located at C:\Projects\Rebuild.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I did this morning is build up a new project from scratch. I used &lt;/P&gt;&lt;P&gt;PE to load all the components needed. Once I had the same structure as &lt;/P&gt;&lt;P&gt;my original project, I generated the code and compiled. Since that was &lt;/P&gt;&lt;P&gt;clean, I copied over the source files from the other project and &lt;/P&gt;&lt;P&gt;recompiled. That was also clean&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At that point, I did not have the I2C component added. So, I added it &lt;/P&gt;&lt;P&gt;in, regenerated the code and compiled. Thankfully, I got the same error, &lt;/P&gt;&lt;P&gt;but this time the project settings were as I expected them to be. So &lt;/P&gt;&lt;P&gt;that eliminated that possible problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Separately, I generated a short project that just had MQX and the I2C. &lt;/P&gt;&lt;P&gt;Since that compiled cleanly, I think it can eliminate the I2C as being &lt;/P&gt;&lt;P&gt;the source of the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The attached file is the new project (Rebuild) that shows this problem. &lt;/P&gt;&lt;P&gt;After you unzip it and import it into a project, if you just use PE to &lt;/P&gt;&lt;P&gt;generate the code and compile, you should see the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm sort of second guessing it, but it looks as though the string being &lt;/P&gt;&lt;P&gt;passed as the command line to the compiler might exceed the maximum &lt;/P&gt;&lt;P&gt;length allowed by Windows.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know if you find anything (particularly a solution!) or need more &lt;/P&gt;&lt;P&gt;information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Mar 2015 14:59:35 GMT</pubDate>
    <dc:creator>davepfaltzgraff</dc:creator>
    <dc:date>2015-03-04T14:59:35Z</dc:date>
    <item>
      <title>Information on building required KSDK libraries.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355787#M535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on a KSDK project using PE. When I add fsl_i2c and try to compile, the linker is unable to find:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;C:/Freescale/KS_2.0.0/eclipse//../toolchain/arm-none-eabi/lib/m4/fp/v4-sp-d16/libc.a&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It would be nice if there was a single placed that listed which libraries could be found where, but I haven't stumbled on it yet.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2015 20:15:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355787#M535</guid>
      <dc:creator>davepfaltzgraff</dc:creator>
      <dc:date>2015-03-03T20:15:47Z</dc:date>
    </item>
    <item>
      <title>Re: Information on building required KSDK libraries.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355788#M536</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There's something else going on here that doesn't make sense to me. I repeated the process and got the same error but this time for &lt;STRONG&gt;libm.a&lt;/STRONG&gt;. I have checked and both are in the Project=&amp;gt;Properties=&amp;gt;C/C++ Build=&amp;gt;Settings=&amp;gt;Cross ARM C++ Linker=&amp;gt;Miscellaneous panel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, any suggestions welcome!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2015 20:48:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355788#M536</guid>
      <dc:creator>davepfaltzgraff</dc:creator>
      <dc:date>2015-03-03T20:48:28Z</dc:date>
    </item>
    <item>
      <title>Re: Information on building required KSDK libraries.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355789#M537</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David ,&lt;/P&gt;&lt;P&gt;Could you upload your project ?&lt;/P&gt;&lt;P&gt;And what's the version of your KSDK ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 02:19:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355789#M537</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-03-04T02:19:23Z</dc:date>
    </item>
    <item>
      <title>Re: Information on building required KSDK libraries.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355790#M538</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working through some changes that were (inadvertently) made in the Project=&amp;gt;Properties. If I can make sense of them, I'll let you know. If not, I'll be glad to upload the project to see what you can find. I should know tomorrow.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 02:40:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355790#M538</guid>
      <dc:creator>davepfaltzgraff</dc:creator>
      <dc:date>2015-03-04T02:40:11Z</dc:date>
    </item>
    <item>
      <title>Re: Information on building required KSDK libraries.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355791#M539</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First, to answer your question, I'm using KDS 2.0.0with KSDK 1.1.0 on a &lt;/P&gt;&lt;P&gt;Windows 7 system. The KDS and KSDK are both installed to C:\Freescale. &lt;/P&gt;&lt;P&gt;My project is located at C:\Projects\Rebuild.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I did this morning is build up a new project from scratch. I used &lt;/P&gt;&lt;P&gt;PE to load all the components needed. Once I had the same structure as &lt;/P&gt;&lt;P&gt;my original project, I generated the code and compiled. Since that was &lt;/P&gt;&lt;P&gt;clean, I copied over the source files from the other project and &lt;/P&gt;&lt;P&gt;recompiled. That was also clean&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At that point, I did not have the I2C component added. So, I added it &lt;/P&gt;&lt;P&gt;in, regenerated the code and compiled. Thankfully, I got the same error, &lt;/P&gt;&lt;P&gt;but this time the project settings were as I expected them to be. So &lt;/P&gt;&lt;P&gt;that eliminated that possible problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Separately, I generated a short project that just had MQX and the I2C. &lt;/P&gt;&lt;P&gt;Since that compiled cleanly, I think it can eliminate the I2C as being &lt;/P&gt;&lt;P&gt;the source of the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The attached file is the new project (Rebuild) that shows this problem. &lt;/P&gt;&lt;P&gt;After you unzip it and import it into a project, if you just use PE to &lt;/P&gt;&lt;P&gt;generate the code and compile, you should see the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm sort of second guessing it, but it looks as though the string being &lt;/P&gt;&lt;P&gt;passed as the command line to the compiler might exceed the maximum &lt;/P&gt;&lt;P&gt;length allowed by Windows.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know if you find anything (particularly a solution!) or need more &lt;/P&gt;&lt;P&gt;information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 14:59:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355791#M539</guid>
      <dc:creator>davepfaltzgraff</dc:creator>
      <dc:date>2015-03-04T14:59:35Z</dc:date>
    </item>
    <item>
      <title>Re: Information on building required KSDK libraries.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355792#M540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have test and check your project ,while it still have error when build.&lt;/P&gt;&lt;P&gt;So i refer to your component create a new project , and i have not cofigure the PE component detail,&lt;/P&gt;&lt;P&gt;while it have no error when build, so i send to your , and please test on it .&lt;/P&gt;&lt;P&gt;If it have not error,&amp;nbsp; i think you can configure on it .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Mar 2015 14:35:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355792#M540</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-03-07T14:35:36Z</dc:date>
    </item>
    <item>
      <title>Re: Information on building required KSDK libraries.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355793#M541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you want me to test your solution, you need to forward it to me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, it is important to me to have the PE involved in the design process.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Mar 2015 14:45:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355793#M541</guid>
      <dc:creator>davepfaltzgraff</dc:creator>
      <dc:date>2015-03-07T14:45:05Z</dc:date>
    </item>
    <item>
      <title>Re: Information on building required KSDK libraries.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355794#M542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The basic problem is the maximum line limitation found in Windows. For the correct solution see &lt;A href="https://community.nxp.com/message/487685"&gt;Re: Re: KSDK Linker Error - Command line too long&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 08 Mar 2015 15:42:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Information-on-building-required-KSDK-libraries/m-p/355794#M542</guid>
      <dc:creator>davepfaltzgraff</dc:creator>
      <dc:date>2015-03-08T15:42:06Z</dc:date>
    </item>
  </channel>
</rss>