<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PEx  clockMan1 not generating proper code for BLPI mode. in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/PEx-clockMan1-not-generating-proper-code-for-BLPI-mode/m-p/512167#M5289</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Jorge, I was able to get into the VLPR mode, but I think there is another issue with PE.&lt;/P&gt;&lt;P&gt;I can not change clock modes when running.&lt;/P&gt;&lt;P&gt;kClockManagerErrorOutOfRange ALWAYS fails here in fsl_clock_manager.c when debugging:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Clock configuration index is out of range. */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (targetConfigIndex &amp;gt;= g_clockState.clockConfigNum)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return kClockManagerErrorOutOfRange;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;This always fails because targetConfigurationIndex is either 0 or 1 and clockConfigNum is ALWAYS zero .&lt;/P&gt;&lt;P&gt;Here is what I think is the bug: PE does not correctly "identify" the number of user clock configurations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my case I know I have 2, and PE defines them in the generated code clockMan1.h file as:&lt;/P&gt;&lt;P&gt;/*! @brief Count of user configuration structures */&lt;/P&gt;&lt;P&gt; #define FSL_CLOCK_MANAGER_CONFIG_CNT 2U&lt;/P&gt;&lt;P&gt;Problem is: FSL_CLOCK_MANAGER_CONFIG_CNT is not used (or found) anywhere else in the project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All project references to the number of user clock configurations is clockConfigNum.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have attached a simple test project that "attempts" to change between 2 different run modes: both are FEI run. Only difference is config0 is 50 mhz and config 1 is 20 mhz (the basic default).&lt;/P&gt;&lt;P&gt;I know the configurations are OK, because if I set them as the default in PE, they work fine (just will not change in debug run)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help here would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, I can't see where I can attach my file, so I put it on my FTP here: &lt;A href="http://www.h-itt.com/beta/TEST.zip" title="http://www.h-itt.com/beta/TEST.zip"&gt;http://www.h-itt.com/beta/TEST.zip&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Apr 2016 22:12:32 GMT</pubDate>
    <dc:creator>randenewberry</dc:creator>
    <dc:date>2016-04-26T22:12:32Z</dc:date>
    <item>
      <title>PEx  clockMan1 not generating proper code for BLPI mode.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/PEx-clockMan1-not-generating-proper-code-for-BLPI-mode/m-p/512165#M5287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using KDS 3.2,&amp;nbsp; KSDK 1.3.0, PE with an MK02FN64VLH10 in 64 pin package with a custom PCBA .&lt;/P&gt;&lt;P&gt;I want to set up clocks for BLPI mode to get in the VLPR mode. Here are the PE selections (note it is BLPI mode)&lt;/P&gt;&lt;P&gt;Here are the PE selections (note it is BLPI mode)...The clocks out look correct to enter the VLPR mode, correct??.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121227iDD10BD8658ED457A/image-size/large?v=v2&amp;amp;px=999" title="144945_144945.png" alt="144945_144945.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26311i62054202D769A056/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;..&lt;/P&gt;&lt;P&gt;Problem is the PE generated code shows the selected mode as:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121228i4DAA60E14B565EC0/image-size/large?v=v2&amp;amp;px=999" title="144946_144946.png" alt="144946_144946.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26354iD2B6A4657FD1300E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PEE mode is not on the PE MCG mode selection list. &lt;/P&gt;&lt;P&gt;Searching the project for kMcgModePEE, All references to it are greyed (between #if&amp;nbsp; ....and ..&amp;nbsp; #endif) except in the enum for _mcg_modes.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Rande.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Mar 2016 20:03:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/PEx-clockMan1-not-generating-proper-code-for-BLPI-mode/m-p/512165#M5287</guid>
      <dc:creator>randenewberry</dc:creator>
      <dc:date>2016-03-29T20:03:39Z</dc:date>
    </item>
    <item>
      <title>Re: PEx  clockMan1 not generating proper code for BLPI mode.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/PEx-clockMan1-not-generating-proper-code-for-BLPI-mode/m-p/512166#M5288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rande Newberry:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I reproduced your settings and this must be a Processor Expert bug. I will report this to PEx team, sorry for the confusion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Notice however that those structures are generated for run-time clock configuration changes, but the MCU should still be initialized in BLPI mode. The file &lt;STRONG&gt;system_MK02F12810.h&lt;/STRONG&gt; has the clock initialization macros, and you should see something like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27680iDBB18EFDD18F8FD6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case you need to change the clocks at run-time then the structure will indeed be wrong. As workaround you can change it to BLPI:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27776i36F54D4A86115E45/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And disable code generation for the &lt;STRONG&gt;fsl_clock_manager&lt;/STRONG&gt; component (right click on the component to open context menu):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27848iAB8CC08009CDC9E2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Apr 2016 20:29:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/PEx-clockMan1-not-generating-proper-code-for-BLPI-mode/m-p/512166#M5288</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-04-04T20:29:02Z</dc:date>
    </item>
    <item>
      <title>Re: PEx  clockMan1 not generating proper code for BLPI mode.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/PEx-clockMan1-not-generating-proper-code-for-BLPI-mode/m-p/512167#M5289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Jorge, I was able to get into the VLPR mode, but I think there is another issue with PE.&lt;/P&gt;&lt;P&gt;I can not change clock modes when running.&lt;/P&gt;&lt;P&gt;kClockManagerErrorOutOfRange ALWAYS fails here in fsl_clock_manager.c when debugging:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Clock configuration index is out of range. */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (targetConfigIndex &amp;gt;= g_clockState.clockConfigNum)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return kClockManagerErrorOutOfRange;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;This always fails because targetConfigurationIndex is either 0 or 1 and clockConfigNum is ALWAYS zero .&lt;/P&gt;&lt;P&gt;Here is what I think is the bug: PE does not correctly "identify" the number of user clock configurations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my case I know I have 2, and PE defines them in the generated code clockMan1.h file as:&lt;/P&gt;&lt;P&gt;/*! @brief Count of user configuration structures */&lt;/P&gt;&lt;P&gt; #define FSL_CLOCK_MANAGER_CONFIG_CNT 2U&lt;/P&gt;&lt;P&gt;Problem is: FSL_CLOCK_MANAGER_CONFIG_CNT is not used (or found) anywhere else in the project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All project references to the number of user clock configurations is clockConfigNum.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have attached a simple test project that "attempts" to change between 2 different run modes: both are FEI run. Only difference is config0 is 50 mhz and config 1 is 20 mhz (the basic default).&lt;/P&gt;&lt;P&gt;I know the configurations are OK, because if I set them as the default in PE, they work fine (just will not change in debug run)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help here would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, I can't see where I can attach my file, so I put it on my FTP here: &lt;A href="http://www.h-itt.com/beta/TEST.zip" title="http://www.h-itt.com/beta/TEST.zip"&gt;http://www.h-itt.com/beta/TEST.zip&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 22:12:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/PEx-clockMan1-not-generating-proper-code-for-BLPI-mode/m-p/512167#M5289</guid>
      <dc:creator>randenewberry</dc:creator>
      <dc:date>2016-04-26T22:12:32Z</dc:date>
    </item>
    <item>
      <title>Re: PEx  clockMan1 not generating proper code for BLPI mode.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/PEx-clockMan1-not-generating-proper-code-for-BLPI-mode/m-p/512168#M5290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rande:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Before switching clock configurations you need to call &lt;STRONG&gt;CLOCK_SYS_Init()&lt;/STRONG&gt;, which actually asks for the number of configurations in the second parameter:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;IMG alt="pastedImage_1.png" src="https://community.nxp.com/t5/image/serverpage/image-id/35525i36FB9005036D4918/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So in your case this would be something like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="plain" __jive_macro_name="code" class="jive_macro_code jive_text_macro _jivemacro_uid_14617145474991896" data-renderedposition="354.5_8_1155_64" jivemacro_uid="_14617145474991896" modifiedtitle="true"&gt;&lt;P&gt;CLOCK_SYS_Init(g_clockManConfigsArr,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FSL_CLOCK_MANAGER_CONFIG_CNT,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; g_clockManCallbacksArr,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FSL_CLOCK_MANAGER_CALLBACK_CNT);&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 13:29:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/PEx-clockMan1-not-generating-proper-code-for-BLPI-mode/m-p/512168#M5290</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2020-11-02T13:29:34Z</dc:date>
    </item>
    <item>
      <title>Re: PEx  clockMan1 not generating proper code for BLPI mode.</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/PEx-clockMan1-not-generating-proper-code-for-BLPI-mode/m-p/512169#M5291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;When it seems to work something breaks. &lt;/P&gt;&lt;P&gt;I don't think changing the name in the PE generated code from FEI to BLIP is a complete run time solution.&lt;/P&gt;&lt;P&gt;Does NXP post PE's recent known issues / workarounds / fixes-Updates?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Clock switching works except when trying to set the BLPI mode:&lt;/P&gt;&lt;P&gt;The program gets in a continuous loop where the matrixIdx = 7 and matricIdxTarget = 1&lt;/P&gt;&lt;P&gt;And always goes to the matrix: case MCG_MATRIX_FBI:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52252i95F52E19D376B08C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have found that in BLPI mode, power is significantly reduced, and I do not need to use a VLPR mode.&lt;/P&gt;&lt;P&gt;problem is the BLPI mode seems to have a problem.&lt;/P&gt;&lt;P&gt;Is it possible to use the FBI mode, fast (4meg) clock and get the same clocks out as the BLPI mode, then go into the VLPR mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice would be greatly appreciated!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 20:35:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/PEx-clockMan1-not-generating-proper-code-for-BLPI-mode/m-p/512169#M5291</guid>
      <dc:creator>randenewberry</dc:creator>
      <dc:date>2016-04-27T20:35:20Z</dc:date>
    </item>
  </channel>
</rss>