<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Re:  How to modify the interrupt vectors, using FRDM K64, sdk 2.0 with freertos ?</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-modify-the-interrupt-vectors-using-FRDM-K64-sdk-2-0-with/m-p/510086#M5227</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Raul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here's a simple example that will read the SW2 input and then change the color and frequency of the LED flash. This example builds off of the FrerRTOS hello world example that is shipped with SDK 2.0. You should be able to replace the freertos_hello.c file, build, and download to your target board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The key points to enable the SW interrupt functionality can be round in the init_sw2() function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This function will:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;enable the clock for the SW2 port&lt;/LI&gt;&lt;LI&gt;setup the pin mux as GPIO&lt;/LI&gt;&lt;LI&gt;enable the port and system interrupts&lt;/LI&gt;&lt;LI&gt;set the GPIO as an input.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once all of these steps are complete, the only step left is to add the IRQ handler to override the default weak implementation in the startup file. Don't forget to clear the interrupt before leaving your interrupt function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 06 Mar 2016 16:31:47 GMT</pubDate>
    <dc:creator>Jmart</dc:creator>
    <dc:date>2016-03-06T16:31:47Z</dc:date>
    <item>
      <title>How to modify the interrupt vectors, using FRDM K64, sdk 2.0 with freertos ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-modify-the-interrupt-vectors-using-FRDM-K64-sdk-2-0-with/m-p/510085#M5226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you have some examples using SW buttons in FRDMK64 with interrupts, SDK2.0 and freertos ? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 Mar 2016 13:09:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-modify-the-interrupt-vectors-using-FRDM-K64-sdk-2-0-with/m-p/510085#M5226</guid>
      <dc:creator>RaAolCortAcsMat</dc:creator>
      <dc:date>2016-03-06T13:09:38Z</dc:date>
    </item>
    <item>
      <title>Re:  How to modify the interrupt vectors, using FRDM K64, sdk 2.0 with freertos ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-modify-the-interrupt-vectors-using-FRDM-K64-sdk-2-0-with/m-p/510086#M5227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Raul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here's a simple example that will read the SW2 input and then change the color and frequency of the LED flash. This example builds off of the FrerRTOS hello world example that is shipped with SDK 2.0. You should be able to replace the freertos_hello.c file, build, and download to your target board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The key points to enable the SW interrupt functionality can be round in the init_sw2() function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This function will:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;enable the clock for the SW2 port&lt;/LI&gt;&lt;LI&gt;setup the pin mux as GPIO&lt;/LI&gt;&lt;LI&gt;enable the port and system interrupts&lt;/LI&gt;&lt;LI&gt;set the GPIO as an input.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once all of these steps are complete, the only step left is to add the IRQ handler to override the default weak implementation in the startup file. Don't forget to clear the interrupt before leaving your interrupt function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 Mar 2016 16:31:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-modify-the-interrupt-vectors-using-FRDM-K64-sdk-2-0-with/m-p/510086#M5227</guid>
      <dc:creator>Jmart</dc:creator>
      <dc:date>2016-03-06T16:31:47Z</dc:date>
    </item>
    <item>
      <title>Re:  How to modify the interrupt vectors, using FRDM K64, sdk 2.0 with freertos ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-modify-the-interrupt-vectors-using-FRDM-K64-sdk-2-0-with/m-p/510087#M5228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jason&lt;/P&gt;&lt;P&gt;I was missing &lt;/P&gt;&lt;UL&gt;&lt;LI&gt;setup the pin mux as GPIO&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Raul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Mar 2016 02:57:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/How-to-modify-the-interrupt-vectors-using-FRDM-K64-sdk-2-0-with/m-p/510087#M5228</guid>
      <dc:creator>RaAolCortAcsMat</dc:creator>
      <dc:date>2016-03-07T02:57:16Z</dc:date>
    </item>
  </channel>
</rss>