<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Does anyone have an example using one ADC to measure 3 different signals at the same time with sdk 2.0 and frdm k64f? in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503715#M4911</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Diego,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sorry, what I said previously is not totally correct. If you use Ping-Pong mode of SAR ADC, because there is only one ADC converter for each ADC module, the instant of Ping ADC sampling can not happen at the same time as the instant of Pong ADC sampling, the delay should be GREATER than one ADC conversion time, otherwise, there is error.&lt;/P&gt;&lt;P&gt;I copy part of ADC example code for Ping-Pong mode for K40, hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 08:52:49 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2016-06-16T08:52:49Z</dc:date>
    <item>
      <title>Does anyone have an example using one ADC to measure 3 different signals at the same time with sdk 2.0 and frdm k64f?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503712#M4908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.!&lt;/P&gt;&lt;P&gt;I am using the FRDM k64F and KSDK 2.0. &lt;/P&gt;&lt;P&gt;I need to measure 3 different signals with an ADC and 3 different singals with the other one, but I don't know how to do it.&lt;/P&gt;&lt;P&gt;Can anybody help me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 May 2016 16:27:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503712#M4908</guid>
      <dc:creator>diegovalerio</dc:creator>
      <dc:date>2016-05-27T16:27:14Z</dc:date>
    </item>
    <item>
      <title>Re: Does anyone have an example using one ADC to measure 3 different signals at the same time with sdk 2.0 and frdm k64f?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503713#M4909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Diego,&lt;/P&gt;&lt;P&gt;I think that the K64F supports to sample 3 different signals at the same time, this is the solution. As you know that the K64F has one PDB module and two ADC modules(ADC0 and ADC1), each ADC module support Ping-Pong operation for example, the Ping is controlled by ADC0_SC1A, the Pong is controlled by ADC0_SC1B, if you want to sample 3 different signals, you have to use two ADC modules at the same time. For example, this is the channels:&lt;/P&gt;&lt;P&gt;ADC0_SEx&lt;/P&gt;&lt;P&gt;ADC0_SEy&lt;/P&gt;&lt;P&gt;ADC1_SEz&lt;/P&gt;&lt;P&gt;ADC1_SEw(this can be a dummy channels)&lt;/P&gt;&lt;P&gt;The PDB Channel0 delay0 control the instant of sampling ADC0_SEx, the PDB Channel0 delay1 control the instant of sampling ADC0_SEy; the PDB Channel1 delay0 control the instant of sampling ADC1_SEz, the PDB Channel1 delay1 control the instant of sampling ADC1_SEw. If you set the PDBCH0DLY0=PDBCH0DLY1=PDBCH1DLY0=PDBCH1DLY1, all the four samples will be acquired at the same time.&lt;/P&gt;&lt;P&gt;I suggest you use software triggering mode for the PDB by setting the SWTRIG bit in PDBx_SC, in the case, external triggering source is not required. the ADC sampling cycle is controlled only&amp;nbsp; by the PDBx_MOD register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to sample another 3 different signals, you can change the channels of both ADC modules in the ISR of ADC, in this way, you can get 6 different samples in two ADC sampling cycles in interleaved mode, but I do not know if it can meet your requirements. If it do not meet your requirement, I think you can consider the Kinetis processor which the ADC supports scan mode for example KV58.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 May 2016 06:17:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503713#M4909</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-05-30T06:17:19Z</dc:date>
    </item>
    <item>
      <title>Re: Does anyone have an example using one ADC to measure 3 different signals at the same time with sdk 2.0 and frdm k64f?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503714#M4910</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiangjun Rong.&lt;/P&gt;&lt;P&gt;I kinda understand the point, but I can´t make it real in a program.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to measure a three phase signal with the FRDM K64F, that's why I need to measure three signals at the time.&lt;/P&gt;&lt;P&gt;By chance, do you have an example using the different channels of the ADC and how does the 'ping-pong' work?&lt;/P&gt;&lt;P&gt;It would be so helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:04:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503714#M4910</guid>
      <dc:creator>diegovalerio</dc:creator>
      <dc:date>2016-06-15T17:04:22Z</dc:date>
    </item>
    <item>
      <title>Re: Does anyone have an example using one ADC to measure 3 different signals at the same time with sdk 2.0 and frdm k64f?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503715#M4911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Diego,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sorry, what I said previously is not totally correct. If you use Ping-Pong mode of SAR ADC, because there is only one ADC converter for each ADC module, the instant of Ping ADC sampling can not happen at the same time as the instant of Pong ADC sampling, the delay should be GREATER than one ADC conversion time, otherwise, there is error.&lt;/P&gt;&lt;P&gt;I copy part of ADC example code for Ping-Pong mode for K40, hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 08:52:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503715#M4911</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-06-16T08:52:49Z</dc:date>
    </item>
    <item>
      <title>Re: Does anyone have an example using one ADC to measure 3 different signals at the same time with sdk 2.0 and frdm k64f?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503716#M4912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is the ADC example code, you can refer to it.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 08:55:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503716#M4912</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-06-16T08:55:15Z</dc:date>
    </item>
    <item>
      <title>Re: Does anyone have an example using one ADC to measure 3 different signals at the same time with sdk 2.0 and frdm k64f?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503717#M4913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiangjun.&lt;/P&gt;&lt;P&gt;Thanks for the explanation, but I can´t see the example code you send.&lt;/P&gt;&lt;P&gt;Could you send it to me one more time, if possible?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Diego.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 16:08:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503717#M4913</guid>
      <dc:creator>diegovalerio</dc:creator>
      <dc:date>2016-06-16T16:08:30Z</dc:date>
    </item>
    <item>
      <title>Re: Does anyone have an example using one ADC to measure 3 different signals at the same time with sdk 2.0 and frdm k64f?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503718#M4914</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I paste the code here:&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;/*&lt;/P&gt;&lt;P&gt; * main implementation: use this 'C' sample to create your own application&lt;/P&gt;&lt;P&gt; *&lt;/P&gt;&lt;P&gt; */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define PE_MCUINIT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#include &amp;lt;stdio.h&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#include "derivative.h" /* include peripheral declarations */&lt;/P&gt;&lt;P&gt;#define SOFTWARE_TRIGGER 0&lt;/P&gt;&lt;P&gt;#define PIT_TRIGGER 0&lt;/P&gt;&lt;P&gt;#define PDB_TRIGGER 1&lt;/P&gt;&lt;P&gt;void MCU_init(void); /* Device initialization function declaration */&lt;/P&gt;&lt;P&gt;void ADC_ISR(void);&lt;/P&gt;&lt;P&gt;unsigned int sample[10];&lt;/P&gt;&lt;P&gt;//ADC1_DM1 is connected to adjustable resistor, so the code can be used to &lt;/P&gt;&lt;P&gt;//test the output of the adjustable resistor&lt;/P&gt;&lt;P&gt;int main(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; int counter = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCU_init(); /* call device initialization */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //toggle LED E1 by toggling PCT7 pin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //set the PCT7 as GPIO output pin mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SCGC5=SIM_SCGC5|0x3E00; //enable port A/B/C/D/E clock &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm(nop);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORTC_PCR7=0x100; //PTC7 in GPIO mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOC_PDDR=0x80; //PTC direction register, PTC7 is in output mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; NVICIP58=0x0F; //set ADC0 interrupt priority&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; NVICICPR1|=1&amp;lt;&amp;lt;26;&amp;nbsp;&amp;nbsp; //clear the pending register of interrupt source of ADC(57)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; NVICISER1|=1&amp;lt;&amp;lt;26;&amp;nbsp; //set the interrupt source of ADC0, 57%32=25&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;#if&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SOFTWARE_TRIGGER &lt;/P&gt;&lt;P&gt;//Conclusion:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_ISR(void) can be entered&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //enable ADC0 clock, FTM1 and FTM0 clock, PIT clock, PDB clock&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SCGC6|=0x0BC00000; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SCGC3|=0x08000000; //enable ADC1 clock &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //ADICLK=00 Bus Clock, MODE=01 12 bits conversion &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //ADLSMP=0 short sample time&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //ADIV 00 divide ratio is 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_CFG1=0x04; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_CFG2=0x00;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_SC2=0x00; //software triggered, &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_SC3=0x00; //one conversion&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //initiate ADC conversion by software triggering&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_SC1A=0x54; //interrupt enable and select ADC1_DM1 channel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm(cpsie i); //interrupt enable&lt;/P&gt;&lt;P&gt;#endif&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;#if&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PIT1_TRIGGER&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //enable ADC0 clock, FTM1 and FTM0 clock, PIT clock, PDB clock&lt;/P&gt;&lt;P&gt;//Conclusion:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_ISR(void)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; can be entered&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SCGC6|=0x0BC00000; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SCGC3|=0x08000000; //enable ADC1 clock &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //ADICLK=00 Bus Clock, MODE=01 12 bits conversion &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //ADLSMP=0 short sample time&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //ADIV 00 divide ratio is 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //PIT module configuration&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PIT_MCR = 0x00;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PIT_LDVAL1 = 0x003FFFFF; // setup timer so that the LED have enough time to flash&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //select PIT1 trigger via SIM_SOP7&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SOPT7=0x8500; //PIT1 trigger&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_CFG1=0x04; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_CFG2=0x00;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_SC2=0x40; //hardware triggered, &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_SC3=0x00; //one conversion&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //initiate ADC conversion by software triggering&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_SC1A=0x54; //interrupt enable and select ADC1_DM1 channel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PIT_TCTRL1 |= 0x01; // start Timer 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm(cpsie i); //interrupt enable&lt;/P&gt;&lt;P&gt;#endif&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;#if&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PDB_TRIGGER&lt;/P&gt;&lt;P&gt;//software trigger PDB, PDB triggers ADC&lt;/P&gt;&lt;P&gt;//enable ADC0 clock, FTM1 and FTM0 clock, PIT clock, PDB clock&lt;/P&gt;&lt;P&gt;//Conclusion:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_ISR(void)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; can be entered&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SCGC6|=0x0BC00000; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SCGC3|=0x08000000; //enable ADC1 clock &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //ADICLK=00 Bus Clock, MODE=01 12 bits conversion &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //ADLSMP=0 short sample time&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //ADIV 00 divide ratio is 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //PDB module configuration&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PDB0_CH0S=0x0000;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PDB0_SC=0x00F80; //PDB enable, PDB interrupt enable&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PDB0_MOD=0x8000;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PDB0_IDLY=0x00;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PDB0_CH0C1=0x0303; //Enable CH0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PDB0_CH0DLY0=0x1000;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PDB0_CH0DLY1=0x5000;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PDB0_SC|=0x02; //write the register&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PDB0_SC|=0x01; //write the register&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //select PIT1 trigger via SIM_SOP7&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SIM_SOPT7=0x00; //PDB0 trigger ADC1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_CFG1=0x04; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_CFG2=0x00;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_SC2=0x40; //hardware triggered, &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_SC3=0x00; //one conversion&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //initiate ADC conversion by software triggering&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_SC1A=0x54; //interrupt enable and select ADC1_DM1 channel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_SC1B=0x53; //interrupt enable and select ADC1_DM0 channel&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PDB0_SC|=0x10000; //start trigger&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm(cpsie i); //interrupt enable&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //The ADC_ISR() can not be entered &lt;/P&gt;&lt;P&gt;#endif&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; for(;;) {&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; counter++;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return 0;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;#pragma interrupt on&lt;/P&gt;&lt;P&gt;void ADC_ISR(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //LED indicator&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOC_PTOR=0x80;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; sample[0]=ADC1_RA;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm(nop);&lt;/P&gt;&lt;P&gt;#if&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SOFTWARE_TRIGGER&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC1_SC1A=0x54; //software triggering interrupt enable&lt;/P&gt;&lt;P&gt;#endif&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#pragma interrupt on&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 00:03:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Does-anyone-have-an-example-using-one-ADC-to-measure-3-different/m-p/503718#M4914</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-06-17T00:03:59Z</dc:date>
    </item>
  </channel>
</rss>