<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPI Driver Not working Arm M0+ MKL15Z128VFT4 in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SPI-Driver-Not-working-Arm-M0-MKL15Z128VFT4/m-p/486883#M4304</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jonathan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your question, it seems that there is problem for the following function, pls check.&lt;/P&gt;&lt;P&gt;SPI_DRV_MasterInit(*m_instance, &amp;amp;SPI_COM1_MasterState);&lt;/P&gt;&lt;P&gt;SPI_DRV_MasterConfigureBus(*m_instance, &amp;amp;SPI_COM1_MasterConfig0, &amp;amp;SPI_COM1_calculatedBaudRate);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not know what you define the m_instance, if you define it as:&lt;/P&gt;&lt;P&gt;#define m_instance 1 //if you use SPI1&lt;/P&gt;&lt;P&gt;#define m_instance 0 //if you use SPI0&lt;/P&gt;&lt;P&gt;#define m_instance 2 //if you use SPI2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the case, you should omit the * when you call the API function.&lt;/P&gt;&lt;P&gt;SPI_DRV_MasterInit(m_instance, &amp;amp;SPI_COM1_MasterState);&lt;/P&gt;&lt;P&gt;SPI_DRV_MasterConfigureBus(m_instance, &amp;amp;SPI_COM1_MasterConfig0, &amp;amp;SPI_COM1_calculatedBaudRate);&lt;/P&gt;&lt;P&gt;Hope it can help.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Apr 2016 03:57:50 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2016-04-07T03:57:50Z</dc:date>
    <item>
      <title>SPI Driver Not working Arm M0+ MKL15Z128VFT4</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SPI-Driver-Not-working-Arm-M0-MKL15Z128VFT4/m-p/486882#M4303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm in the process of debugging a SPI peripheral I'm using with the ARM M0+ uC MKL15Z128VFT4. The OS is BareMetal and the SysTick is at 1ms. The clock speed for the SPI peripheral is 23.405714 kHz. I keep running into an issue where an exception is thrown when the hit the SPI_HAL_SetIntMode(base, kSpiRxFullAndModfInt) and then the debugger jumps to DefaultISR. I have the instruction set in Thumb mode and the debug level at Default -g. Also I do initialize the peripheral driver before this with:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class="j-rte-table"&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD style=""&gt;&lt;/TD&gt;&lt;TD style=""&gt;//Install interrupt handler for SPI comm&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; OSA_InstallIntHandler(SPI0_IRQn, SPI_COM1_IRQHandler);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Initialize SPI to Master control&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(SPI_DRV_MasterInit(*m_instance, &amp;amp;SPI_COM1_MasterState) == kStatus_SPI_Success)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;DIV class="j-rte-table"&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD style=""&gt;&lt;/TD&gt;&lt;TD style=""&gt;//Configure the SPI bus&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD style=""&gt;&lt;/TD&gt;&lt;TD style=""&gt;SPI_DRV_MasterConfigureBus(*m_instance, &amp;amp;SPI_COM1_MasterConfig0, &amp;amp;SPI_COM1_calculatedBaudRate);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD style=""&gt;&lt;/TD&gt;&lt;TD style=""&gt;return true;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return false;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So I can't imagine it's the proper initialization of the peripheral that's the cause of this exception being thrown, but I won't rule it out. Any pointers/ideas to help solve this would be much appreciated. BTW, if I manually step through the code with the debugger, the exception isn't thrown, since the debugger is controlling the execution. I've seen this issue arise in the past with the SysTick timer, or the debugger symbol file not being aligned. I'm not sure.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Apr 2016 14:46:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SPI-Driver-Not-working-Arm-M0-MKL15Z128VFT4/m-p/486882#M4303</guid>
      <dc:creator>jonathan_guinta</dc:creator>
      <dc:date>2016-04-06T14:46:26Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Driver Not working Arm M0+ MKL15Z128VFT4</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SPI-Driver-Not-working-Arm-M0-MKL15Z128VFT4/m-p/486883#M4304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jonathan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your question, it seems that there is problem for the following function, pls check.&lt;/P&gt;&lt;P&gt;SPI_DRV_MasterInit(*m_instance, &amp;amp;SPI_COM1_MasterState);&lt;/P&gt;&lt;P&gt;SPI_DRV_MasterConfigureBus(*m_instance, &amp;amp;SPI_COM1_MasterConfig0, &amp;amp;SPI_COM1_calculatedBaudRate);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not know what you define the m_instance, if you define it as:&lt;/P&gt;&lt;P&gt;#define m_instance 1 //if you use SPI1&lt;/P&gt;&lt;P&gt;#define m_instance 0 //if you use SPI0&lt;/P&gt;&lt;P&gt;#define m_instance 2 //if you use SPI2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the case, you should omit the * when you call the API function.&lt;/P&gt;&lt;P&gt;SPI_DRV_MasterInit(m_instance, &amp;amp;SPI_COM1_MasterState);&lt;/P&gt;&lt;P&gt;SPI_DRV_MasterConfigureBus(m_instance, &amp;amp;SPI_COM1_MasterConfig0, &amp;amp;SPI_COM1_calculatedBaudRate);&lt;/P&gt;&lt;P&gt;Hope it can help.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Apr 2016 03:57:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/SPI-Driver-Not-working-Arm-M0-MKL15Z128VFT4/m-p/486883#M4304</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-04-07T03:57:50Z</dc:date>
    </item>
  </channel>
</rss>