<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Switching between Run mode and High Speed Run mode in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486008#M4268</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using IRC48MCLK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I made a change to the KSDK that seems to fix the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;background:&lt;/P&gt;&lt;P&gt;I use CLOCK_SYS_SetConfiguration() to change the clocks when changing the power mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;after calling CLOCK_SYS_SetConfiguration USB stops sending. &lt;/P&gt;&lt;P&gt;I isolated the cause of the USB failure to CLOCK_SYS_SetMcgMode()&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Although I am in PLL Engaged External(PEE)Mode in both the old and new configuration&lt;/P&gt;&lt;P&gt;it first switches to PLL Bypassed External(PBE) Mode then back to PEE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think there is a mistake in mcgModeMatrix[8][8]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If old is PEE and new is PEE it goes to PBE&lt;/P&gt;&lt;P&gt;I changed it to stay in PEE and USB rides through the clock change&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the code, can you tell me if this is correct&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56027i76849829CCFFBEA2/image-size/large?v=v2&amp;amp;px=999" title="fsl_clock_manager-snip.png" alt="fsl_clock_manager-snip.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Jan 2016 21:21:34 GMT</pubDate>
    <dc:creator>joebirch</dc:creator>
    <dc:date>2016-01-22T21:21:34Z</dc:date>
    <item>
      <title>Switching between Run mode and High Speed Run mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486002#M4262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Normally I am in High Speed Run mode but to program flash I have to switch to normal Run mode.&lt;/P&gt;&lt;P&gt;First is this correct? and second what is the proper way to switch modes during run time?&lt;/P&gt;&lt;P&gt;I prefer not to have to reboot.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the MK22FN512 with KDS3.0 and KSDK 1.3. Currently using the FRDM-K22 eval board&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 21:10:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486002#M4262</guid>
      <dc:creator>joebirch</dc:creator>
      <dc:date>2016-01-12T21:10:24Z</dc:date>
    </item>
    <item>
      <title>Re: Switching between Run mode and High Speed Run mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486003#M4263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Joe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Firstly, you are right, erasing/programming flash should be in normal RUM mode, erasing/programming flash in High Speed RUN mode is NOT allowed. This is the transition sequence from High speed RUN mode to normal run mode:&lt;/P&gt;&lt;P&gt;The K22 is running in High Speed RUN mode mode now.&lt;/P&gt;&lt;P&gt;1)change the FLL or PLL setting so that the core/system clock is in 80MHz or less, Bus clock frequency is 50M or less, and Flash clock is in 25mhz or less.&lt;/P&gt;&lt;P&gt;2)set the RUNM bit as 00 in binary so that the chip runs in normal mode.&lt;/P&gt;&lt;P&gt;3)polling the SMC_PMSTAT whether the chip is in Normak RUN mode&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I copy the part from RM.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;14.4.3.3 High Speed Run (HSRUN) mode&lt;/P&gt;&lt;P&gt;In HSRUN mode, the on-chip voltage regulator remains in a run regulation state, but with&lt;/P&gt;&lt;P&gt;a slightly elevated voltage output. In this state, the MCU is able to operate at a faster&lt;/P&gt;&lt;P&gt;frequency compared to normal RUN mode. See Power Management chapter for&lt;/P&gt;&lt;P&gt;maximum allowable frequencies.&lt;/P&gt;&lt;P&gt;While in this mode, the following restrictions must be adhered to:&lt;/P&gt;&lt;P&gt;• The maximum allowable change in frequency of the system, bus, flash or core clocks&lt;/P&gt;&lt;P&gt;is restricted to x2.&lt;/P&gt;&lt;P&gt;• Before exiting HSRUN mode, clock frequencies should be reduced back down to&lt;/P&gt;&lt;P&gt;those acceptable in RUN mode.&lt;/P&gt;&lt;P&gt;• Stop mode entry is not supported from HSRUN.&lt;/P&gt;&lt;P&gt;• Modifications to clock gating control bits are prohibited.&lt;/P&gt;&lt;P&gt;• Flash programming/erasing is not allowed.&lt;/P&gt;&lt;P&gt;To enter HSRUN mode, set RUNM=HSRUN. Before increasing clock frequencies, the&lt;/P&gt;&lt;P&gt;PMSTAT register should be polled to determine when the system has completed entry&lt;/P&gt;&lt;P&gt;into HSRUN mode. To reenter normal RUN mode, clear RUNM. Any reset will also&lt;/P&gt;&lt;P&gt;clear RUNM and cause the system to exit to normal RUN mode after the MCU exits its&lt;/P&gt;&lt;P&gt;reset flow.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jan 2016 06:22:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486003#M4263</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-01-14T06:22:13Z</dc:date>
    </item>
    <item>
      <title>Re: Switching between Run mode and High Speed Run mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486004#M4264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Thank you for the info. changing from hsrun to normal run does allow me to erase and program flash&lt;/P&gt;&lt;P&gt;but when I change the clock speed the uart and usb connections stop functioning.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I have to reinitialize these. Or can I change my clocking configuration so they are not affected by switching power modes?&lt;/P&gt;&lt;P&gt;I don't really understand the clocking settings. I am just using examples I found in KSDK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I start in hsrun mode and made 2 functions: goHighSpeedRunMode(), goNormalRunMode() to go back and forth during run time&lt;/P&gt;&lt;P&gt;See attached for these functions and the initialization code&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help is appreciated&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2016 21:17:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486004#M4264</guid>
      <dc:creator>joebirch</dc:creator>
      <dc:date>2016-01-15T21:17:00Z</dc:date>
    </item>
    <item>
      <title>Re: Switching between Run mode and High Speed Run mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486005#M4265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Joe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Firstly, if you change the RUN mode from High Speed Run mode to Normal Run mode, the bus clock will change accordingly, the UART driving clock will change if you use Bus clock as driving clock source of UART.&lt;/P&gt;&lt;P&gt;After you change the mode from HSRUN mode to Normal Run mode, you have to call the following function to change the baudrate based on New bus clock frequency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; uint32_t uartSourceClock = CLOCK_SYS_GetUartFreq(UART0_IDX);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; LPUART_Type * base = g_uartBase[UART0_IDX];&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; LPUART_HAL_SetBaudRate(base, uartSourceClock, BaudRate);&lt;/P&gt;&lt;P&gt;Regarding the USB,&amp;nbsp; I suppose that the USB uses dedicated IRC48M clock, which is Not effected by the bus clock.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 07:31:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486005#M4265</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-01-18T07:31:05Z</dc:date>
    </item>
    <item>
      <title>Re: Switching between Run mode and High Speed Run mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486006#M4266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was able to correct the uart issue by deinitializing the uart before the run mode change and re-initializing after.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the USB still does not survive the change.&lt;/P&gt;&lt;P&gt;You are right I am using IRC48M clock for USB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe it is because I use CLOCK_SYS_SetConfiguration() to change the clock before going to Normal run mode?&lt;/P&gt;&lt;P&gt;Here is the code&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CLOCK_SYS_SetConfiguration(&amp;amp;g_defaultClockConfigRun);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; smc_power_mode_config_t powerModeConfig = {.powerModeName = kPowerModeRun, };&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SMC_HAL_SetMode(SMC, &amp;amp;powerModeConfig);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can you advise on a better way?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 20:02:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486006#M4266</guid>
      <dc:creator>joebirch</dc:creator>
      <dc:date>2016-01-18T20:02:19Z</dc:date>
    </item>
    <item>
      <title>Re: Switching between Run mode and High Speed Run mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486007#M4267</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the USB clock diagram for K22. If you use IRC48MCLK source, I do not think there is any problem after you change the system/core clock. But if you use MCGPLL clock as the system/core clock, after you change the frequency, there is issue. Pls check the SIM_SOPT2[PLLFLLSEL] and determine the USB clock source. Not that the USB must use 48MHz clock with low jitter.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54508i436AE97D5B0398C7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jan 2016 06:27:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486007#M4267</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-01-21T06:27:55Z</dc:date>
    </item>
    <item>
      <title>Re: Switching between Run mode and High Speed Run mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486008#M4268</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using IRC48MCLK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I made a change to the KSDK that seems to fix the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;background:&lt;/P&gt;&lt;P&gt;I use CLOCK_SYS_SetConfiguration() to change the clocks when changing the power mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;after calling CLOCK_SYS_SetConfiguration USB stops sending. &lt;/P&gt;&lt;P&gt;I isolated the cause of the USB failure to CLOCK_SYS_SetMcgMode()&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Although I am in PLL Engaged External(PEE)Mode in both the old and new configuration&lt;/P&gt;&lt;P&gt;it first switches to PLL Bypassed External(PBE) Mode then back to PEE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think there is a mistake in mcgModeMatrix[8][8]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If old is PEE and new is PEE it goes to PBE&lt;/P&gt;&lt;P&gt;I changed it to stay in PEE and USB rides through the clock change&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the code, can you tell me if this is correct&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56027i76849829CCFFBEA2/image-size/large?v=v2&amp;amp;px=999" title="fsl_clock_manager-snip.png" alt="fsl_clock_manager-snip.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jan 2016 21:21:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Switching-between-Run-mode-and-High-Speed-Run-mode/m-p/486008#M4268</guid>
      <dc:creator>joebirch</dc:creator>
      <dc:date>2016-01-22T21:21:34Z</dc:date>
    </item>
  </channel>
</rss>