<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Re: Convert non-KSDK project to KSDK</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Convert-non-KSDK-project-to-KSDK/m-p/483535#M4185</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kevin Penn:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately there is not a direct migration path from the legacy Processor Expert to a project using KSDK drivers.&lt;/P&gt;&lt;P&gt;The best and cleanest approach is to start with a base project and replicate the application using the new drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- With the &lt;STRONG&gt;Kinetis SDK Project Generator&lt;/STRONG&gt; you can create a new project or clone one of the existing KSDK example projects:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-328990"&gt;New Kinetis SDK Project Generator v2 is available! &lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- If using KDS then you can use the &lt;STRONG&gt;Kinetis SDK v2.x Project Wizard&lt;/STRONG&gt;:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329662"&gt;Using Kinetis Design Studio v3.x with Kinetis SDK v2.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Mar 2016 02:05:51 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2016-03-18T02:05:51Z</dc:date>
    <item>
      <title>Convert non-KSDK project to KSDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Convert-non-KSDK-project-to-KSDK/m-p/483534#M4184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've been developing a project for a while using the non-KSDK version of the MK21FN1M0VLL12 processor in processor expert to setup hardware.&amp;nbsp; I'm working on implementing support for a micro SD card and would like to use the KSDK version now as there is better support for the micro SD.&amp;nbsp; Is it possible to convert a project setup initially without the KSDK to a project that uses the KSDK?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Mar 2016 15:53:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Convert-non-KSDK-project-to-KSDK/m-p/483534#M4184</guid>
      <dc:creator>kevinpenn92</dc:creator>
      <dc:date>2016-03-16T15:53:25Z</dc:date>
    </item>
    <item>
      <title>Re: Convert non-KSDK project to KSDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Convert-non-KSDK-project-to-KSDK/m-p/483535#M4185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kevin Penn:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately there is not a direct migration path from the legacy Processor Expert to a project using KSDK drivers.&lt;/P&gt;&lt;P&gt;The best and cleanest approach is to start with a base project and replicate the application using the new drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- With the &lt;STRONG&gt;Kinetis SDK Project Generator&lt;/STRONG&gt; you can create a new project or clone one of the existing KSDK example projects:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-328990"&gt;New Kinetis SDK Project Generator v2 is available! &lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- If using KDS then you can use the &lt;STRONG&gt;Kinetis SDK v2.x Project Wizard&lt;/STRONG&gt;:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329662"&gt;Using Kinetis Design Studio v3.x with Kinetis SDK v2.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Mar 2016 02:05:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Convert-non-KSDK-project-to-KSDK/m-p/483535#M4185</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-03-18T02:05:51Z</dc:date>
    </item>
  </channel>
</rss>