<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックFRDM-K64F - Using ADC in Hardware Trigger Mode</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K64F-Using-ADC-in-Hardware-Trigger-Mode/m-p/480097#M4104</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I try to configure the ADC (ADC1)&amp;nbsp; in hardware trigger mode using a PDB channel as the ADC trigger.&lt;/P&gt;&lt;P&gt;Which PDB trigger Input source should I use ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any examples in KSDK 2.0 for such a thing ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Nadine&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 May 2016 15:58:36 GMT</pubDate>
    <dc:creator>nadine</dc:creator>
    <dc:date>2016-05-17T15:58:36Z</dc:date>
    <item>
      <title>FRDM-K64F - Using ADC in Hardware Trigger Mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K64F-Using-ADC-in-Hardware-Trigger-Mode/m-p/480097#M4104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I try to configure the ADC (ADC1)&amp;nbsp; in hardware trigger mode using a PDB channel as the ADC trigger.&lt;/P&gt;&lt;P&gt;Which PDB trigger Input source should I use ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any examples in KSDK 2.0 for such a thing ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Nadine&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 May 2016 15:58:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K64F-Using-ADC-in-Hardware-Trigger-Mode/m-p/480097#M4104</guid>
      <dc:creator>nadine</dc:creator>
      <dc:date>2016-05-17T15:58:36Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F - Using ADC in Hardware Trigger Mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K64F-Using-ADC-in-Hardware-Trigger-Mode/m-p/480098#M4105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nadine,&lt;/P&gt;&lt;P&gt;Please look at following example to see if it helps.&lt;/P&gt;&lt;P&gt;C:\NXP\KSDK_v2\SDK_2.0_FRDM-K64F_KDS\boards\frdmk64f\driver_examples\pdb\adc16_trigger &lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 May 2016 16:15:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K64F-Using-ADC-in-Hardware-Trigger-Mode/m-p/480098#M4105</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2016-05-17T16:15:20Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F - Using ADC in Hardware Trigger Mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K64F-Using-ADC-in-Hardware-Trigger-Mode/m-p/480099#M4106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nadine,&lt;/P&gt;&lt;P&gt;You can refer that example.&lt;/P&gt;&lt;P&gt;The PDB trigger Input source can be found at "Table 3-57. PDB Input Trigger Options" in &lt;A href="http://cache.nxp.com/files/microcontrollers/doc/ref_manual/K64P144M120SF5RM.pdf?fpsp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;K64P144M120SF5RM&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="PDB Input Trigger Options.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22530i759210F3C7D671D4/image-size/large?v=v2&amp;amp;px=999" role="button" title="PDB Input Trigger Options.jpg" alt="PDB Input Trigger Options.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;You can try to change the PDB trigger Input source.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="trigger input source for the PDB.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22181iA89CE1855DF0EE4A/image-size/large?v=v2&amp;amp;px=999" role="button" title="trigger input source for the PDB.jpg" alt="trigger input source for the PDB.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 May 2016 08:43:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K64F-Using-ADC-in-Hardware-Trigger-Mode/m-p/480099#M4106</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2016-05-18T08:43:22Z</dc:date>
    </item>
  </channel>
</rss>