<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GPIO output with frdm-kl43z and processor expert in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/GPIO-output-with-frdm-kl43z-and-processor-expert/m-p/474531#M3910</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I realized that the pins are outputting 3 V, but they are not outputting enough current to power my air compressor.&lt;/P&gt;&lt;P&gt;Is there anyway to draw more current from the kl43z pins?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Jan 2016 00:52:18 GMT</pubDate>
    <dc:creator>christopherira</dc:creator>
    <dc:date>2016-01-29T00:52:18Z</dc:date>
    <item>
      <title>GPIO output with frdm-kl43z and processor expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/GPIO-output-with-frdm-kl43z-and-processor-expert/m-p/474530#M3909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using the frdm-kl43z board and trying to control a simple output with processor expert.&lt;/P&gt;&lt;P&gt;I am able to do so with the on board LEDs, but when trying to output a voltage with the pins, I can't toggle an output.&lt;/P&gt;&lt;P&gt;I've configured several pins in processor expert but get nothing out.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;these are the configurations of LEDs and J2_17:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121029iA188170822E03E38/image-size/large?v=v2&amp;amp;px=999" title="133749_133749.png" alt="133749_133749.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33822iDF3B3E06AFA5A963/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I've also tried an output logic of 1 and various combinations of slew rate and drive strength.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is my code to control a simple toggle of the output with the on board buttons.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121030iA6ECF43613409248/image-size/large?v=v2&amp;amp;px=999" title="133748_133748.png" alt="133748_133748.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6653iF2C68675BC569455/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It works fine with the LEDs but not with the Pins.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jan 2016 22:59:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/GPIO-output-with-frdm-kl43z-and-processor-expert/m-p/474530#M3909</guid>
      <dc:creator>christopherira</dc:creator>
      <dc:date>2016-01-28T22:59:31Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO output with frdm-kl43z and processor expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/GPIO-output-with-frdm-kl43z-and-processor-expert/m-p/474531#M3910</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I realized that the pins are outputting 3 V, but they are not outputting enough current to power my air compressor.&lt;/P&gt;&lt;P&gt;Is there anyway to draw more current from the kl43z pins?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jan 2016 00:52:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/GPIO-output-with-frdm-kl43z-and-processor-expert/m-p/474531#M3910</guid>
      <dc:creator>christopherira</dc:creator>
      <dc:date>2016-01-29T00:52:18Z</dc:date>
    </item>
  </channel>
</rss>