<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックRe: KSDK code exit for MK22FN1M0VLH12</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-code-exit-for-MK22FN1M0VLH12/m-p/349434#M381</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was having no trouble with KDS/KDSK in terms of compiling and now it's being touchy, running less and less consistently now to a point where I can't get my application on to the chip, and if I open terminal I'm seeing the last program that was loaded onto it running. I tried unplugging, holding reset while plugging back in and reloading OPENSDA 2.1 multiple times, and while the board automatically resets and appears as the J-Link under COM Ports, it won't load code. It won't even load a file with just while(1) or for(;;) and no code, no includes other than things like studio.h, etc...it will however load example projects. I don't understand this inconsistency - I had this working for almost a month and in the last 24 hours it started to do this. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this what you are getting? &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47402iFAF9BCD90EE0A5F8/image-size/large?v=v2&amp;amp;px=999" title="20141120_KDS_TerminationSS.png" alt="20141120_KDS_TerminationSS.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Not sure if this will help at all because you don't say anything about Freedom, but there are a few links already started related KDS/K22, and the KDS platform/debugging in general that may help you:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101792"&gt;FRDM-K22F: Debugging with P&amp;amp;amp;E OpenSDAv2.1 Firmware&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/426304"&gt;Re: First impression with KDS 1.1.0 Can't Debug FRDM-K64F with OpenOCD/CMSIS-DAP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-100733"&gt;Using FRDM-K64F with P&amp;amp;amp;E and Segger OpenSDAv2 Firmware&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Nov 2014 17:31:11 GMT</pubDate>
    <dc:creator>bosleymusic_com</dc:creator>
    <dc:date>2014-11-20T17:31:11Z</dc:date>
    <item>
      <title>KSDK code exit for MK22FN1M0VLH12</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-code-exit-for-MK22FN1M0VLH12/m-p/349433#M380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am using MK22FN1M0VLH12,Installed KDS and KSDK. I tried to run hello_world program from KSDK,it is compiled and loaded successfully but while running program exited from program.I found KSDK for K22- 512MB.How to use KSDK programs for K22-1MB?what all I need to change?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Nov 2014 12:20:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-code-exit-for-MK22FN1M0VLH12/m-p/349433#M380</guid>
      <dc:creator>vanajagujjala</dc:creator>
      <dc:date>2014-11-18T12:20:19Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK code exit for MK22FN1M0VLH12</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-code-exit-for-MK22FN1M0VLH12/m-p/349434#M381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was having no trouble with KDS/KDSK in terms of compiling and now it's being touchy, running less and less consistently now to a point where I can't get my application on to the chip, and if I open terminal I'm seeing the last program that was loaded onto it running. I tried unplugging, holding reset while plugging back in and reloading OPENSDA 2.1 multiple times, and while the board automatically resets and appears as the J-Link under COM Ports, it won't load code. It won't even load a file with just while(1) or for(;;) and no code, no includes other than things like studio.h, etc...it will however load example projects. I don't understand this inconsistency - I had this working for almost a month and in the last 24 hours it started to do this. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this what you are getting? &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47402iFAF9BCD90EE0A5F8/image-size/large?v=v2&amp;amp;px=999" title="20141120_KDS_TerminationSS.png" alt="20141120_KDS_TerminationSS.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Not sure if this will help at all because you don't say anything about Freedom, but there are a few links already started related KDS/K22, and the KDS platform/debugging in general that may help you:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101792"&gt;FRDM-K22F: Debugging with P&amp;amp;amp;E OpenSDAv2.1 Firmware&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/426304"&gt;Re: First impression with KDS 1.1.0 Can't Debug FRDM-K64F with OpenOCD/CMSIS-DAP&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-100733"&gt;Using FRDM-K64F with P&amp;amp;amp;E and Segger OpenSDAv2 Firmware&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Nov 2014 17:31:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-code-exit-for-MK22FN1M0VLH12/m-p/349434#M381</guid>
      <dc:creator>bosleymusic_com</dc:creator>
      <dc:date>2014-11-20T17:31:11Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK code exit for MK22FN1M0VLH12</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-code-exit-for-MK22FN1M0VLH12/m-p/349435#M382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could it be that bug in GDB?&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2014/10/11/failed-to-debug-with-gdb-breakpoints-or-expressions-on-non-existing-locations/" title="http://mcuoneclipse.com/2014/10/11/failed-to-debug-with-gdb-breakpoints-or-expressions-on-non-existing-locations/"&gt;http://mcuoneclipse.com/2014/10/11/failed-to-debug-with-gdb-breakpoints-or-expressions-on-non-existing-locations/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Clear all breakpoints and watchpoints/expressions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Nov 2014 17:35:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-code-exit-for-MK22FN1M0VLH12/m-p/349435#M382</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2014-11-20T17:35:14Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK code exit for MK22FN1M0VLH12</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-code-exit-for-MK22FN1M0VLH12/m-p/349436#M383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just tried clearing all breakpoints - noticed that there were two BP's on the same line of code as well - and that appears to be exactly what it is...I hope. I'm back to running so I'll keep this in mind, and thank you for the quick response. Now if I could only get SAI to work properly, I'd be really happy.:smileysilly:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Nov 2014 17:43:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/KSDK-code-exit-for-MK22FN1M0VLH12/m-p/349436#M383</guid>
      <dc:creator>bosleymusic_com</dc:creator>
      <dc:date>2014-11-20T17:43:13Z</dc:date>
    </item>
  </channel>
</rss>