<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic void FLEXCAN_DRV_IRQHandler (uint8_t instance) in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/void-FLEXCAN-DRV-IRQHandler-uint8-t-instance/m-p/470702#M3770</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wants to use CAN interrupt . Is there any example code for this? I am using FRDM64 Board.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kinetis SDK v.1.3 API Reference Manual.pdf don't have much information about it.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Rishi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jan 2016 04:18:10 GMT</pubDate>
    <dc:creator>Anonymous</dc:creator>
    <dc:date>2016-01-06T04:18:10Z</dc:date>
    <item>
      <title>void FLEXCAN_DRV_IRQHandler (uint8_t instance)</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/void-FLEXCAN-DRV-IRQHandler-uint8-t-instance/m-p/470702#M3770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everyone,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wants to use CAN interrupt . Is there any example code for this? I am using FRDM64 Board.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kinetis SDK v.1.3 API Reference Manual.pdf don't have much information about it.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Rishi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jan 2016 04:18:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/void-FLEXCAN-DRV-IRQHandler-uint8-t-instance/m-p/470702#M3770</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2016-01-06T04:18:10Z</dc:date>
    </item>
    <item>
      <title>Re: void FLEXCAN_DRV_IRQHandler (uint8_t instance)</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/void-FLEXCAN-DRV-IRQHandler-uint8-t-instance/m-p/470703#M3771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rishi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please take a look at example for FlexCAN, the project is located under&lt;/P&gt;&lt;P&gt;&amp;lt;SDK_Install&amp;gt;/examples/&amp;lt;board&amp;gt;/driver_examples/flexcan/&amp;lt;use-case&amp;gt;/&amp;lt;toolchain&amp;gt;&lt;/P&gt;&lt;P&gt;there are two examples - FlexCAN Loopback and FlexCAN Network and because these examples are done for TWR-K64F120M, TWR-K60D100M, TWR-K65F180M, TWR-K21F120M and TWR-KV11Z75M, is needed to do some modifications for your board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case of FRDM-K64F, please connect &lt;STRONG&gt;TJA1050&lt;/STRONG&gt; according to &lt;A href="http://cache.nxp.com/files/microcontrollers/hardware_tools/schematics/TWR-SER-SCH.pdf" rel="nofollow noopener noreferrer noopener noreferrer" target="_blank" title="http://cache.nxp.com/files/microcontrollers/hardware_tools/schematics/TWR-SER-SCH.pdf"&gt;TWR-SER Schematic&lt;/A&gt; to PTB18 and PTB19 and it should works.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="TJA1050.png"&gt;&lt;IMG alt="TJA1050.png" src="https://community.nxp.com/t5/image/serverpage/image-id/52103i574AAD8367301618/image-size/large?v=v2&amp;amp;px=999" title="TJA1050.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="schematic.png"&gt;&lt;IMG alt="schematic.png" src="https://community.nxp.com/t5/image/serverpage/image-id/52030i9767E825A2AD7231/image-size/large?v=v2&amp;amp;px=999" title="schematic.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;More description for each flexcan functions you can get in fsl_flexcan_driver.h, located under C:\Freescale\KSDK_1.3.0\platform\drivers\inc&lt;/P&gt;&lt;PRE __default_attr="c#" __jive_macro_name="code" class="jive_macro_code jive_text_macro _jivemacro_uid_14520935472165105" data-renderedposition="686_8_1231_208" jivemacro_uid="_14520935472165105" modifiedtitle="true"&gt;&lt;P&gt;void FLEXCAN_DRV_IRQHandler(uint8_t instance);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*!&lt;/P&gt;&lt;P&gt; * @brief Returns whether the previous FLEXCAN transmit has finished.&lt;/P&gt;&lt;P&gt; *&lt;/P&gt;&lt;P&gt; * When performing an async transmit, call this function to ascertain the state of the&lt;/P&gt;&lt;P&gt; * current transmission: in progress (or busy) or complete (success).&lt;/P&gt;&lt;P&gt; *&lt;/P&gt;&lt;P&gt; * @param instance The FLEXCAN module base address.&lt;/P&gt;&lt;P&gt; * @return The transmit status.&lt;/P&gt;&lt;P&gt; * @retval kStatus_FLEXCAN_Success The transmit has completed successfully.&lt;/P&gt;&lt;P&gt; * @retval kStatus_FLEXCAN_TxBusy The transmit is still in progress.&lt;/P&gt;&lt;P&gt; */&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Iva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 13:25:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/void-FLEXCAN-DRV-IRQHandler-uint8-t-instance/m-p/470703#M3771</guid>
      <dc:creator>ivadorazinova</dc:creator>
      <dc:date>2020-11-02T13:25:08Z</dc:date>
    </item>
  </channel>
</rss>