<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックRe: DSPI abnormal timing between frames</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/DSPI-abnormal-timing-between-frames/m-p/469295#M3721</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Peter,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your question, for the K66, the PTE0 is multiplexed with the other peripherals as following:&lt;/P&gt;&lt;P&gt;Pin assignment:PTE0, ADC1_SE4a,SPI1_PCS1, UART1_TX, SDHC0_D1, TRACE_CLKOUT,I2C1_SDA RTC_CLKOUT.&lt;/P&gt;&lt;P&gt;From your code, it seems that you set the PTE0 pin as GPIO output and toggle it in software. If you use the pin PTE0 as SPI1_PCS1, you should not set the PTE0 as GPIO by setting the MUX bits of PORTE_PCR0 as ALT1, you should set the MUX bits of PORTE_PCR0 as ALT2 so that the SPI1 module can drive the PTE2 automatically.&lt;/P&gt;&lt;P&gt;Of course, you are right that the PDT/DT bits in SPIx_CTARn determine the interval between two SPI transfer. If you do not call the SDK function and write the SPIx_PUSHR register directly, I think the interval between two transfer will be very short which is based on the DT/PTD mechanism. I have checked your code, I think the code is okay, but the SDK is a high level function, the DSPI_DRV_MasterTransfer() function just put the data to an internal buffer, the code efficiency is low, which leads to the interval is long. If you require the speed of SPI, I suggest you write register directly without calling SDK function.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Dec 2015 07:47:16 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2015-12-09T07:47:16Z</dc:date>
    <item>
      <title>DSPI abnormal timing between frames</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/DSPI-abnormal-timing-between-frames/m-p/469294#M3720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on a custom board equipped with K66 MCU(120MHz, and 60MHz bus clock), serial Flash, and other peripherals. The purpose of serial Flash is just for data storage. I have successfully read the device JEDEC ID through DSPI bus 1 (20MHz baud). However, based on the scope observation, the delay between 8-bit frames are too long (approximately&amp;nbsp; 3.2us). Please refer to the following scope screenshot, &lt;/P&gt;&lt;P&gt;Yellow signal: PCS0 on DSPI1,&lt;/P&gt;&lt;P&gt;Green signal: CLK,&lt;/P&gt;&lt;P&gt;Blue signal: SOUT, and&lt;/P&gt;&lt;P&gt;Pink signal: SIN.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="113649_113649.png"&gt;&lt;IMG alt="113649_113649.png" src="https://community.nxp.com/t5/image/serverpage/image-id/120867iAE8F889D02AF4104/image-size/large?v=v2&amp;amp;px=999" title="113649_113649.png" /&gt;&lt;/SPAN&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;IMG alt="pastedImage_0.png" src="https://community.nxp.com/t5/image/serverpage/image-id/58302iD9281592FFB35B4A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I would like to have minimum delay between transfer by setting delay with DSPI_HAL_SetDelay() function. Based on the calculation,&lt;/P&gt;&lt;P&gt;PCSSCK=0, CSSCk=0 --&amp;gt; tcsc=(1/60M)*1*2=33.3ns&lt;/P&gt;&lt;P&gt;PASS=0, ASC=0, tasc=(1/60M)*1*2=33.3ns&lt;/P&gt;&lt;P&gt;PDT=0, DT=0, tdt=(1/60M)*1*2=33.3ns&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="113650_113650.jpg"&gt;&lt;IMG alt="113650_113650.jpg" src="https://community.nxp.com/t5/image/serverpage/image-id/120868i0D3C642D2A6C4136/image-size/large?v=v2&amp;amp;px=999" title="113650_113650.jpg" /&gt;&lt;/SPAN&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_21.jpg"&gt;&lt;IMG alt="pastedImage_21.jpg" src="https://community.nxp.com/t5/image/serverpage/image-id/58320iF8D5DDF103707704/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_21.jpg" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have verified the register has been correct set to zero before calling transfer. Based on the reference manual, the delay between transfer should be tasc+tcsc or maybe even none. However, I have 3.2us between transfer. This is too much away from specification. I wonder if any thing wrong in my code. Please let me know if you have idea or recommendation. Thank you very much.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The following are source code for my test:&lt;/P&gt;&lt;PRE class="c++" name="code"&gt;int main(void) { &amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t&amp;nbsp;&amp;nbsp;&amp;nbsp; int32utmp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; /* Write your code here */ &amp;nbsp;&amp;nbsp;&amp;nbsp; // Init hardware &amp;nbsp;&amp;nbsp;&amp;nbsp; hardware_init(); &amp;nbsp;&amp;nbsp;&amp;nbsp; dbg_uart_init();&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; PRINTF("\r\n\nRunning SPI_Test example.");&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; // Configure SPI pins &amp;nbsp;&amp;nbsp;&amp;nbsp; configure_spi_pins(BOARD_ETHSW_SERFLASH_SPI_INSTANCE);&amp;nbsp;&amp;nbsp;&amp;nbsp; //configure SPI1 &amp;nbsp;&amp;nbsp;&amp;nbsp; gpio_Init();&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; int32utmp = W25Q128FV_ReadID(); &amp;nbsp;&amp;nbsp;&amp;nbsp; if (int32utmp == 0xEF4018)&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("\nW25Q128FV is detected.");&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; /* This for loop should be replaced. By default this loop allows a single stepping. */ &amp;nbsp;&amp;nbsp;&amp;nbsp; for (;;) { &amp;nbsp;&amp;nbsp;&amp;nbsp; } &amp;nbsp;&amp;nbsp;&amp;nbsp; /* Never leave main */ &amp;nbsp;&amp;nbsp;&amp;nbsp; return 0; }&lt;/PRE&gt;&lt;DIV style="display:none;"&gt; &lt;/DIV&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE class="c++" name="code"&gt;uint32_t W25Q128FV_ReadID(void) { &amp;nbsp;&amp;nbsp;&amp;nbsp; uint8_t&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; send_buf[5]; &amp;nbsp;&amp;nbsp;&amp;nbsp; uint8_t&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; recv_buf[5]; &amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; result;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOE_PSOR |= 0x00000001; &amp;nbsp;&amp;nbsp;&amp;nbsp; result = dspicomm_w25qxf_init(DSPI_W25QxFV_INSTANCE, TRANSFER_HIGH_BAUDRATE); &amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOE_PCOR |= 0x00000001; &amp;nbsp;&amp;nbsp;&amp;nbsp; if (result != kStatus_DSPI_Success)&amp;nbsp;&amp;nbsp;&amp;nbsp; return (-1);&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; send_buf[0] = JEDEC_ID; &amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOE_PSOR |= 0x00000001; &amp;nbsp;&amp;nbsp;&amp;nbsp; result = dspicomm_read(DSPI_W25QxFV_INSTANCE, send_buf, 1, recv_buf, 3); &amp;nbsp;&amp;nbsp;&amp;nbsp; GPIOE_PCOR |= 0x00000001; &amp;nbsp;&amp;nbsp;&amp;nbsp; dspicomm_close(DSPI_W25QxFV_INSTANCE);&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; result = (uint32_t)(recv_buf[1] &amp;lt;&amp;lt; 16);&amp;nbsp;&amp;nbsp;&amp;nbsp; // Manuf ID&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : Winbond&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0xEF &amp;nbsp;&amp;nbsp;&amp;nbsp; result |= recv_buf[2] &amp;lt;&amp;lt; 8;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Memory Type&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : SPI Serial Flash&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0x40 &amp;nbsp;&amp;nbsp;&amp;nbsp; result |= recv_buf[3];&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Memory Size&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : W25Q128FV&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = 0x18&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; return result; }&lt;/PRE&gt;&lt;DIV style="display:none;"&gt; &lt;/DIV&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE class="c++" name="code"&gt;int8_t dspicomm_w25qxf_init(uint32_t instance, uint32_t speed) { &amp;nbsp;&amp;nbsp;&amp;nbsp; dspi_status_t dspiResult; &amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t calculatedBaudRate; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; w25Q128FV_masterUserConfig.isChipSelectContinuous = true; &amp;nbsp;&amp;nbsp;&amp;nbsp; w25Q128FV_masterUserConfig.isSckContinuous&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = false; &amp;nbsp;&amp;nbsp;&amp;nbsp; w25Q128FV_masterUserConfig.pcsPolarity&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = kDspiPcs_ActiveLow; &amp;nbsp;&amp;nbsp;&amp;nbsp; w25Q128FV_masterUserConfig.whichCtar&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = kDspiCtar0; &amp;nbsp;&amp;nbsp;&amp;nbsp; w25Q128FV_masterUserConfig.whichPcs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = kDspiPcs0;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; // Initialize master driver. &amp;nbsp;&amp;nbsp;&amp;nbsp; dspiResult = DSPI_DRV_MasterInit(instance, &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;amp;w25Q128FV_masterState, &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;amp;w25Q128FV_masterUserConfig); &amp;nbsp;&amp;nbsp;&amp;nbsp; if (dspiResult != kStatus_DSPI_Success) &amp;nbsp;&amp;nbsp;&amp;nbsp; { &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PRINTF("\r\nERROR: Can not initialize SPI master driver!"); &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return -1; &amp;nbsp;&amp;nbsp;&amp;nbsp; }&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; // Setup the configuration. &amp;nbsp;&amp;nbsp;&amp;nbsp; w25Q128FV_masterDevice.dataBusConfig.bitsPerFrame = 8; &amp;nbsp;&amp;nbsp;&amp;nbsp; w25Q128FV_masterDevice.dataBusConfig.clkPhase&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = kDspiClockPhase_FirstEdge; &amp;nbsp;&amp;nbsp;&amp;nbsp; w25Q128FV_masterDevice.dataBusConfig.clkPolarity&amp;nbsp; = kDspiClockPolarity_ActiveHigh; &amp;nbsp;&amp;nbsp;&amp;nbsp; w25Q128FV_masterDevice.dataBusConfig.direction&amp;nbsp;&amp;nbsp;&amp;nbsp; = kDspiMsbFirst; &amp;nbsp;&amp;nbsp;&amp;nbsp; w25Q128FV_masterDevice.bitsPerSec = speed; //&amp;nbsp;&amp;nbsp;&amp;nbsp; dspiResult = DSPI_DRV_MasterConfigureBus(instance, //&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;amp;w25Q128FV_masterDevice, //&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;amp;calculatedBaudRate); //&amp;nbsp;&amp;nbsp;&amp;nbsp; if (dspiResult != kStatus_DSPI_Success) //&amp;nbsp;&amp;nbsp;&amp;nbsp; { //&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("\r\nERROR: failure in configuration SPI bus!"); //&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return -1; //&amp;nbsp;&amp;nbsp;&amp;nbsp; }&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; // The original DSPI_DRV_MasterConfigureBus() routine takes about 30us to complete. &amp;nbsp;&amp;nbsp;&amp;nbsp; // The following initialization takes only about 2.5us &amp;nbsp;&amp;nbsp;&amp;nbsp; dspi_master_state_t * dspiState = (dspi_master_state_t *)g_dspiStatePtr[instance]; &amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_Type *base = g_dspiBase[instance];&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_BWR_CTAR_DBR(base, dspiState-&amp;gt;whichCtar, 0x01);&amp;nbsp;&amp;nbsp;&amp;nbsp; //DBR = 1 &amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_BWR_CTAR_PBR(base, dspiState-&amp;gt;whichCtar, 0x01);&amp;nbsp;&amp;nbsp;&amp;nbsp; //PBR = 1 &amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_BWR_CTAR_BR(base, dspiState-&amp;gt;whichCtar, 0x00);&amp;nbsp;&amp;nbsp;&amp;nbsp; //BR = 0, Baud = (fp/PBR)*[(1+DBR)/BR] = (60M/3)*[(1+1)/2] = 20MHz&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_BWR_CTAR_FMSZ(base, dspiState-&amp;gt;whichCtar, (w25Q128FV_masterDevice.dataBusConfig.bitsPerFrame - 1)); &amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_BWR_CTAR_CPOL(base, dspiState-&amp;gt;whichCtar, w25Q128FV_masterDevice.dataBusConfig.clkPolarity); &amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_BWR_CTAR_CPHA(base, dspiState-&amp;gt;whichCtar, w25Q128FV_masterDevice.dataBusConfig.clkPhase); &amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_BWR_CTAR_LSBFE(base, dspiState-&amp;gt;whichCtar, w25Q128FV_masterDevice.dataBusConfig.direction);&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; DSPI_HAL_SetDelay(base, dspiState-&amp;gt;whichCtar, 0x00, 0x00, kDspiPcsToSck);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //PCSSCK=0, CSSCK=0, Tcsc=(1/60M)*1*2=32ns &amp;nbsp;&amp;nbsp;&amp;nbsp; DSPI_HAL_SetDelay(base, dspiState-&amp;gt;whichCtar, 0x00, 0x00, kDspiLastSckToPcs);&amp;nbsp;&amp;nbsp;&amp;nbsp; //PASC=0, ASC=0, Tasc=(1/60M)*1*2=32ns &amp;nbsp;&amp;nbsp;&amp;nbsp; DSPI_HAL_SetDelay(base, dspiState-&amp;gt;whichCtar, 0x00, 0x00, kDspiAfterTransfer);&amp;nbsp;&amp;nbsp;&amp;nbsp; //PDT=0, DT=0, Tdt=(1/60M)*1*2=32ns&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; return (kStatus_DSPI_Success); }&amp;nbsp; int8_t dspicomm_close(uint32_t instance) { &amp;nbsp;&amp;nbsp;&amp;nbsp; dspi_status_t dspiResult;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; dspiResult = DSPI_DRV_MasterDeinit(instance); &amp;nbsp;&amp;nbsp;&amp;nbsp; if (dspiResult != kStatus_DSPI_Success) &amp;nbsp;&amp;nbsp;&amp;nbsp; { &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PRINTF("\r\nERROR: failure in configuration SPI bus!"); &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return -1; &amp;nbsp;&amp;nbsp;&amp;nbsp; }&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; return (kStatus_DSPI_Success); }&amp;nbsp; int32_t dspicomm_write(uint32_t instance, uint8_t *data, uint32_t size) { &amp;nbsp;&amp;nbsp;&amp;nbsp; dspi_status_t&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; dspiResult; &amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; wordsTransfer = 0;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; // Send the data. &amp;nbsp;&amp;nbsp;&amp;nbsp; dspiResult = DSPI_DRV_MasterTransfer(instance, &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NULL, &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; data, &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NULL, &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; size); &amp;nbsp;&amp;nbsp;&amp;nbsp; if (dspiResult != kStatus_DSPI_Success) &amp;nbsp;&amp;nbsp;&amp;nbsp; { &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PRINTF("\r\nERROR: Write data transfer error!"); &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return (-1); &amp;nbsp;&amp;nbsp;&amp;nbsp; } &amp;nbsp;&amp;nbsp;&amp;nbsp; // Wait until the transfer is complete. &amp;nbsp;&amp;nbsp;&amp;nbsp; while (DSPI_DRV_MasterGetTransferStatus(instance, &amp;amp;wordsTransfer) == kStatus_DSPI_Busy) &amp;nbsp;&amp;nbsp;&amp;nbsp; {}&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; return size; }&amp;nbsp; int32_t dspicomm_read(uint32_t instance, uint8_t *txData, uint32_t txSize, uint8_t *rxData, uint32_t rxSize) { &amp;nbsp;&amp;nbsp;&amp;nbsp; dspi_status_t&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; dspiResult; &amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; wordsTransfer = 0;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; // Send the data. &amp;nbsp;&amp;nbsp;&amp;nbsp; dspiResult = DSPI_DRV_MasterTransfer(instance, &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NULL, &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; txData, &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; rxData, &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; txSize+rxSize); &amp;nbsp;&amp;nbsp;&amp;nbsp; if (dspiResult != kStatus_DSPI_Success) &amp;nbsp;&amp;nbsp;&amp;nbsp; { &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PRINTF("\r\nERROR: Read data transfer error!"); &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return (-1); &amp;nbsp;&amp;nbsp;&amp;nbsp; } &amp;nbsp;&amp;nbsp;&amp;nbsp; // Wait until the transfer is complete. &amp;nbsp;&amp;nbsp;&amp;nbsp; while (DSPI_DRV_MasterGetTransferStatus(instance, &amp;amp;wordsTransfer) == kStatus_DSPI_Busy) &amp;nbsp;&amp;nbsp;&amp;nbsp; {}&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; return rxSize; }&lt;/PRE&gt;&lt;DIV style="display:none;"&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 13:24:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/DSPI-abnormal-timing-between-frames/m-p/469294#M3720</guid>
      <dc:creator>petershih</dc:creator>
      <dc:date>2020-11-02T13:24:56Z</dc:date>
    </item>
    <item>
      <title>Re: DSPI abnormal timing between frames</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/DSPI-abnormal-timing-between-frames/m-p/469295#M3721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Peter,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your question, for the K66, the PTE0 is multiplexed with the other peripherals as following:&lt;/P&gt;&lt;P&gt;Pin assignment:PTE0, ADC1_SE4a,SPI1_PCS1, UART1_TX, SDHC0_D1, TRACE_CLKOUT,I2C1_SDA RTC_CLKOUT.&lt;/P&gt;&lt;P&gt;From your code, it seems that you set the PTE0 pin as GPIO output and toggle it in software. If you use the pin PTE0 as SPI1_PCS1, you should not set the PTE0 as GPIO by setting the MUX bits of PORTE_PCR0 as ALT1, you should set the MUX bits of PORTE_PCR0 as ALT2 so that the SPI1 module can drive the PTE2 automatically.&lt;/P&gt;&lt;P&gt;Of course, you are right that the PDT/DT bits in SPIx_CTARn determine the interval between two SPI transfer. If you do not call the SDK function and write the SPIx_PUSHR register directly, I think the interval between two transfer will be very short which is based on the DT/PTD mechanism. I have checked your code, I think the code is okay, but the SDK is a high level function, the DSPI_DRV_MasterTransfer() function just put the data to an internal buffer, the code efficiency is low, which leads to the interval is long. If you require the speed of SPI, I suggest you write register directly without calling SDK function.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Dec 2015 07:47:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/DSPI-abnormal-timing-between-frames/m-p/469295#M3721</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2015-12-09T07:47:16Z</dc:date>
    </item>
    <item>
      <title>Re: DSPI abnormal timing between frames</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/DSPI-abnormal-timing-between-frames/m-p/469296#M3722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiangjun:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks your feedback!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PTE0 is used as GPIO for output to scope for debug purpose, not for SPI1. I have no problem with SPI1 signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based on your feedback, I have tried to send data by writing to PUSHR register without calling KSDK, it gives me the best situation 760ns between transfer, which is much better than before. I think it will be OK for my system.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60075iBE4D230770E4BA0A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried to implement based on eDMA in KSDK, it gives me pretty good 67ns between transfer. However, the initialization takes 45us to complete. I will assume it will be good for large quantity of data transfer, not for 4 bytes data transfer. &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/60105iEFB22A6CD48A9DA4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks your help. &lt;/P&gt;&lt;P&gt;Peter Shih&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Dec 2015 21:54:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/DSPI-abnormal-timing-between-frames/m-p/469296#M3722</guid>
      <dc:creator>petershih</dc:creator>
      <dc:date>2015-12-09T21:54:59Z</dc:date>
    </item>
  </channel>
</rss>