<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Re: Which RTOS is recommended to be used with K65?</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Which-RTOS-is-recommended-to-be-used-with-K65/m-p/466904#M3627</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for fast response,&lt;/P&gt;&lt;P&gt;I initially considered to use MQX but I run into the following:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/383145"&gt;Is NXP abandoning MQX?&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Feb 2016 13:59:13 GMT</pubDate>
    <dc:creator>goranigic</dc:creator>
    <dc:date>2016-02-19T13:59:13Z</dc:date>
    <item>
      <title>Which RTOS is recommended to be used with K65?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Which-RTOS-is-recommended-to-be-used-with-K65/m-p/466902#M3625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have K65 processor available, with 64MB of SDRAM, I also need to support SD-CARD, and USB host and USB device (two ports).&lt;/P&gt;&lt;P&gt;Which RTOS should I use.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2016 00:53:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Which-RTOS-is-recommended-to-be-used-with-K65/m-p/466902#M3625</guid>
      <dc:creator>goranigic</dc:creator>
      <dc:date>2016-02-19T00:53:30Z</dc:date>
    </item>
    <item>
      <title>Re: Which RTOS is recommended to be used with K65?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Which-RTOS-is-recommended-to-be-used-with-K65/m-p/466903#M3626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We recommend MQX, the NXP MQX &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;RTOS&lt;/STRONG&gt;&lt;/SPAN&gt; is intended for Kinetis, Vybrid, ColdFire and Freescale PowerPC Microcontrollers. The release consists of &lt;/P&gt;&lt;P&gt;• MQX real time kernel and system components &lt;/P&gt;&lt;P&gt;• TCP/IP networking stack (RTCS) &lt;/P&gt;&lt;P&gt;• FAT file system (MFS) &lt;/P&gt;&lt;P&gt;• NAND flash file system (FFS) &lt;/P&gt;&lt;P&gt;• USB Host and Device stacks &lt;/P&gt;&lt;P&gt;• Platform and Board support packages &lt;/P&gt;&lt;P&gt;• I/O drivers. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For SD card, MQX contains &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;SD&lt;/STRONG&gt;&lt;/SPAN&gt; &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;Card&lt;/STRONG&gt;&lt;/SPAN&gt; I/O Driver and (E)SDHC I/O Driver drivers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2016 07:05:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Which-RTOS-is-recommended-to-be-used-with-K65/m-p/466903#M3626</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-02-19T07:05:39Z</dc:date>
    </item>
    <item>
      <title>Re: Which RTOS is recommended to be used with K65?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Which-RTOS-is-recommended-to-be-used-with-K65/m-p/466904#M3627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for fast response,&lt;/P&gt;&lt;P&gt;I initially considered to use MQX but I run into the following:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/383145"&gt;Is NXP abandoning MQX?&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Feb 2016 13:59:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Which-RTOS-is-recommended-to-be-used-with-K65/m-p/466904#M3627</guid>
      <dc:creator>goranigic</dc:creator>
      <dc:date>2016-02-19T13:59:13Z</dc:date>
    </item>
    <item>
      <title>Re: Which RTOS is recommended to be used with K65?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Which-RTOS-is-recommended-to-be-used-with-K65/m-p/466905#M3628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After some digging, I found today that NXP is not abandoning MQX, instead they are moving away from making it available free for use on their processors to a licensing/support fee system much like many other RTOSes out there.&amp;nbsp; Lookup MQX v5 on the NXP site for the details.&amp;nbsp; For their older processors, you can continue to use MQX 4.x and older for free, for newer processors, such as the K65, K66, you cannot unless you port it yourself.&amp;nbsp; There is still support for a free version of it using the KSDK and KDS, but, the documentation is somewhat lacking in my experience so far.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Apr 2016 21:23:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Which-RTOS-is-recommended-to-be-used-with-K65/m-p/466905#M3628</guid>
      <dc:creator>RichardR</dc:creator>
      <dc:date>2016-04-28T21:23:21Z</dc:date>
    </item>
  </channel>
</rss>