<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Re: FRDM-K22F 16-bit ADC output format in differential mode</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K22F-16-bit-ADC-output-format-in-differential-mode/m-p/452231#M3135</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;The differential ADC will measure the &lt;STRONG&gt;voltage difference&lt;/STRONG&gt; between two pins, DADPx and DADMx, no matter if one input is different to Vcc/2.&lt;/P&gt;&lt;P style="text-align: justify;"&gt;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;In this case the DADPx is acting as the ‘sign bit’. If DADPx voltage is larger than DADMx, sign bit doesn't be set; otherwise, if DADPx voltage is smaller than DADMx, sign bit is set. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;I hope this information will be useful for you. In case you still have questions, please let me know. I will be glad to help.&lt;/P&gt;&lt;P style="text-align: justify;"&gt;Have a great day. :smileyhappy:&lt;/P&gt;&lt;P style="text-align: justify;"&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Sep 2015 16:11:56 GMT</pubDate>
    <dc:creator>david_diaz</dc:creator>
    <dc:date>2015-09-02T16:11:56Z</dc:date>
    <item>
      <title>FRDM-K22F 16-bit ADC output format in differential mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K22F-16-bit-ADC-output-format-in-differential-mode/m-p/452230#M3134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the 16-bit ADC on a FRDM-K22F board to measure a differential signal. If the ADC references are 0V and Vcc, and the DADM0 pin is tied to Vcc/2, then I would expect the result of any conversion would fall between -32768 (0x1000) and 32767(0x7FFF). If Vcc is 3.3V, this is what I would expect with the voltage per bit being about 50uV/bit.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If, however, the DADM0 is tied to a voltage other than Vcc/2, what can I expect of the differential voltage is greater than Vcc/2. For example, if DADM0 = 0.8V and DADP0 is greater than 2.4V (0.8V + Vcc/2), what can I expect after the conversion? Will it just top out at the maximum of 0x7FFF, or will the result be indeterminant?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Aug 2015 17:36:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K22F-16-bit-ADC-output-format-in-differential-mode/m-p/452230#M3134</guid>
      <dc:creator>davepfaltzgraff</dc:creator>
      <dc:date>2015-08-19T17:36:49Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K22F 16-bit ADC output format in differential mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K22F-16-bit-ADC-output-format-in-differential-mode/m-p/452231#M3135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;The differential ADC will measure the &lt;STRONG&gt;voltage difference&lt;/STRONG&gt; between two pins, DADPx and DADMx, no matter if one input is different to Vcc/2.&lt;/P&gt;&lt;P style="text-align: justify;"&gt;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;In this case the DADPx is acting as the ‘sign bit’. If DADPx voltage is larger than DADMx, sign bit doesn't be set; otherwise, if DADPx voltage is smaller than DADMx, sign bit is set. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="text-align: justify;"&gt;I hope this information will be useful for you. In case you still have questions, please let me know. I will be glad to help.&lt;/P&gt;&lt;P style="text-align: justify;"&gt;Have a great day. :smileyhappy:&lt;/P&gt;&lt;P style="text-align: justify;"&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 16:11:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K22F-16-bit-ADC-output-format-in-differential-mode/m-p/452231#M3135</guid>
      <dc:creator>david_diaz</dc:creator>
      <dc:date>2015-09-02T16:11:56Z</dc:date>
    </item>
  </channel>
</rss>