<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Re: No KSDK for new project although vers. 1.2.0 is installed and KSDK_PATH set</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444068#M2905</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the answers, but the problem is that i have a board with an MK60DN256ZVLL10 which shold work in a product in a few months.&lt;/P&gt;&lt;P&gt;So what can i do?&lt;/P&gt;&lt;P&gt;Is there a way to use KDS without KSDK?&lt;/P&gt;&lt;P&gt;I tried that but without KSDK i have no components, so nearly nothing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And what are the alternatives to KDS, for the MK60DN256ZVLL10?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Jun 2015 14:58:45 GMT</pubDate>
    <dc:creator>rolffreitag</dc:creator>
    <dc:date>2015-06-30T14:58:45Z</dc:date>
    <item>
      <title>No KSDK for new project although vers. 1.2.0 is installed and KSDK_PATH set</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444065#M2902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I installed KSDK 1.2.0, KDS 3.0.0, PE 10.4 and JLink V500, installed the KSDK a second time in KDS via help/install (because the &lt;/P&gt;&lt;P&gt;"installation program" is only a self-extracting archive) and then a third time the same way and now it can't be installed a fourth time because it is already installed:&lt;span class="lia-inline-image-display-wrapper" image-alt="45298_45298.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120434iB0C41C00AE8F1AED/image-size/large?v=v2&amp;amp;px=999" role="button" title="45298_45298.png" alt="45298_45298.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ksdk1.2.0installed_2015-06-30.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61055i62BBC8B1E82CCB73/image-size/large?v=v2&amp;amp;px=999" role="button" title="ksdk1.2.0installed_2015-06-30.png" alt="ksdk1.2.0installed_2015-06-30.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So now it is fully installed.&lt;/P&gt;&lt;P&gt;I also set the environment variable KSDK_PATH, but i still don't have a KSDK when i start a new Kinetis project for a processor (MK60DN256ZVLL10):&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="45299_45299.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120435i1C2A0A0AF05CFF5D/image-size/large?v=v2&amp;amp;px=999" role="button" title="45299_45299.png" alt="45299_45299.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="no_ksdk_2015-06-30.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61057i9366A720EDC1AB73/image-size/large?v=v2&amp;amp;px=999" role="button" title="no_ksdk_2015-06-30.png" alt="no_ksdk_2015-06-30.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This results in strange errors like my code in the loop in main.c gets deleted and when i am using PE, and many components are shown but not availible, e. g. for gpio1:fsl_gpio i get the error "is not installed in this version of ProcessorExpert".&lt;/P&gt;&lt;P&gt;And without PE i can use no component, so i can use nothing; even LED blinking is not possible!&lt;/P&gt;&lt;P&gt;How can i start a new project with KSDK?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2015 08:59:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444065#M2902</guid>
      <dc:creator>rolffreitag</dc:creator>
      <dc:date>2015-06-30T08:59:00Z</dc:date>
    </item>
    <item>
      <title>Re: No KSDK for new project although vers. 1.2.0 is installed and KSDK_PATH set</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444066#M2903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The SDK supported devices are listed in&lt;/P&gt;&lt;P&gt;C:\Freescale\KSDK_1.2.0\ksdk_manifest.xml&lt;/P&gt;&lt;P&gt;And there I see that the variant without the 'Z' is supported by the SDK, but not the one with the 'Z'&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61078iD53C7C7CD7767CA1/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2015 14:45:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444066#M2903</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-06-30T14:45:24Z</dc:date>
    </item>
    <item>
      <title>Re: No KSDK for new project although vers. 1.2.0 is installed and KSDK_PATH set</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444067#M2904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rolf,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes - it is right, because MK60DN256ZVLL10 is actually no supported by current KSDK 1.2.&lt;/P&gt;&lt;P&gt;So what can I recommend you it use to supported devices. These devices you find at &lt;A href="http://cache.freescale.com/files/soft_dev_tools/doc/support_info/KSDK120RN.pdf?fpsp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" title="http://cache.freescale.com/files/soft_dev_tools/doc/support_info/KSDK120RN.pdf?fpsp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;Release Note&lt;/A&gt;​&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you,&lt;/P&gt;&lt;P&gt;Iva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2015 14:51:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444067#M2904</guid>
      <dc:creator>ivadorazinova</dc:creator>
      <dc:date>2015-06-30T14:51:04Z</dc:date>
    </item>
    <item>
      <title>Re: No KSDK for new project although vers. 1.2.0 is installed and KSDK_PATH set</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444068#M2905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the answers, but the problem is that i have a board with an MK60DN256ZVLL10 which shold work in a product in a few months.&lt;/P&gt;&lt;P&gt;So what can i do?&lt;/P&gt;&lt;P&gt;Is there a way to use KDS without KSDK?&lt;/P&gt;&lt;P&gt;I tried that but without KSDK i have no components, so nearly nothing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And what are the alternatives to KDS, for the MK60DN256ZVLL10?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2015 14:58:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444068#M2905</guid>
      <dc:creator>rolffreitag</dc:creator>
      <dc:date>2015-06-30T14:58:45Z</dc:date>
    </item>
    <item>
      <title>Re: No KSDK for new project although vers. 1.2.0 is installed and KSDK_PATH set</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444069#M2906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rolf,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sure, you can create new project in KDS without KSDK.&lt;/P&gt;&lt;P&gt;Just&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="k60.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61049i8E969256949A8A3C/image-size/large?v=v2&amp;amp;px=999" role="button" title="k60.png" alt="k60.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="k60_.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61080i308B9C37D56A4065/image-size/large?v=v2&amp;amp;px=999" role="button" title="k60_.png" alt="k60_.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;or if you want to work with KSDK, you can follow the steps in the attached guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Iva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2015 15:03:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444069#M2906</guid>
      <dc:creator>ivadorazinova</dc:creator>
      <dc:date>2015-06-30T15:03:23Z</dc:date>
    </item>
    <item>
      <title>Re: No KSDK for new project although vers. 1.2.0 is installed and KSDK_PATH set</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444070#M2907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the answer, but can the platform library for KDS build the same way as for IAR, as described in the migration guide?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How much work (mandays) is necessary for such a migration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And does this give me the components, e. g. for the GPIO pins for LED toggling?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2015 15:19:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444070#M2907</guid>
      <dc:creator>rolffreitag</dc:creator>
      <dc:date>2015-06-30T15:19:36Z</dc:date>
    </item>
    <item>
      <title>Re: No KSDK for new project although vers. 1.2.0 is installed and KSDK_PATH set</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444071#M2908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rolf,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, it is the same procedure for KDS.&lt;/P&gt;&lt;P&gt;It can take few days, not whole week.&lt;/P&gt;&lt;P&gt;Yes, it will be the same support like for supported devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Iva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2015 18:39:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444071#M2908</guid>
      <dc:creator>ivadorazinova</dc:creator>
      <dc:date>2015-07-01T18:39:02Z</dc:date>
    </item>
    <item>
      <title>Re: No KSDK for new project although vers. 1.2.0 is installed and KSDK_PATH set</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444072#M2909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, i do migrate due to the migration guide, but i found that the K60D10 files, device specific files and platform files, are already there. So this part is finished fast.&lt;/P&gt;&lt;P&gt;Now i want to check the options at "Build the Platform Library" (page 12), but i can't find the displayed menues. Under project properties there is no "Category" and e. g. no "Assembler". I searched both strings via the "Quick Access" box and the properties search box but got only empty results.&lt;/P&gt;&lt;P&gt;Where can i find the options?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jul 2015 10:15:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444072#M2909</guid>
      <dc:creator>rolffreitag</dc:creator>
      <dc:date>2015-07-02T10:15:56Z</dc:date>
    </item>
    <item>
      <title>Re: No KSDK for new project although vers. 1.2.0 is installed and KSDK_PATH set</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444073#M2910</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I followed the instructions in the migration guide and found out that for MK60DN256ZVLL10 i have to choose MK60DN256VLL10 because they differ only in the DIE mask version. &lt;/P&gt;&lt;P&gt;But for all projects with this processor there is no support for PE and KDS, even in the example projects in the KSDK 1.2! So there is something still missing which is not mentioned in the guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Therefore i tried the other way, creating a project with the board twrk60d100 and switching the processor to type MK60DN256VLL10. This works; i can compile and debug with the Segger USB adapter and have the project with KDS and PE!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2015 06:52:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444073#M2910</guid>
      <dc:creator>rolffreitag</dc:creator>
      <dc:date>2015-07-08T06:52:45Z</dc:date>
    </item>
    <item>
      <title>Re: No KSDK for new project although vers. 1.2.0 is installed and KSDK_PATH set</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444074#M2911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rolf, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I´m very sorry for my late response, but I see your&lt;A href="https://community.nxp.com/thread/359136"&gt;post&lt;/A&gt; and the answer (with mask revision) from my colleague.&lt;/P&gt;&lt;P&gt;Please, is it now your issue solved or still occurs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please, let me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Iva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jul 2015 12:59:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444074#M2911</guid>
      <dc:creator>ivadorazinova</dc:creator>
      <dc:date>2015-07-17T12:59:18Z</dc:date>
    </item>
    <item>
      <title>Re: No KSDK for new project although vers. 1.2.0 is installed and KSDK_PATH set</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444075#M2912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, the mask revision problem is solved, thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jul 2015 15:29:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/No-KSDK-for-new-project-although-vers-1-2-0-is-installed-and/m-p/444075#M2912</guid>
      <dc:creator>rolffreitag</dc:creator>
      <dc:date>2015-07-17T15:29:31Z</dc:date>
    </item>
  </channel>
</rss>