<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Re: FLEXBUS_DRV functionality to setup up multiple flexbus regions</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FLEXBUS-DRV-functionality-to-setup-up-multiple-flexbus-regions/m-p/443198#M2875</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ping,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Definitely correct me if I am wrong, but I don't think some of these calls are supported in KSDK 1.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example FB should be Flexbus. FB_HAL_WriteBaseAddr should be Flexbus_HAL_WriteAddr, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Oct 2015 16:52:22 GMT</pubDate>
    <dc:creator>davidtietz</dc:creator>
    <dc:date>2015-10-05T16:52:22Z</dc:date>
    <item>
      <title>FLEXBUS_DRV functionality to setup up multiple flexbus regions</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FLEXBUS-DRV-functionality-to-setup-up-multiple-flexbus-regions/m-p/443196#M2873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Maybe I'm missing it somewhere, but there doesn't seem to be a clean way to set up multiple regions of the flexbus using the flexbus driver directly. Setting up the first region is simple enough using FLEXBUS_DRV_Init() but you can't call it a second time to set up another region because it calls FLEXBUS_HAL_Init() which clears out all of the flexbus registers, thus clobbering the settings for the first region. I know I can access the appropriate registers directly, or call FLEXBUS_HAL_Configure(), but isn't the point of the abstraction layers and ultimately the driver to make it so the user doesn't have to have intimate knowledge of the lower layers? &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My suggestion would be that FLEXBUS_DRV_Init() does what it does now, minus the call to FLEXBUS_HAL_Configure(). A new function should be added, something like FLEXBUS_DRV_AddRegion( const flexbus_user_config_t* userConfigPtr ) that allows you to set up different parameters for different chip selects without having to muck with registers directly or having to reference g_fbBase[] for the sake of having a pointer to pass to FLEXBUS_HAL_Configure(). &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyone else run into this, or am I missing something?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Sep 2015 19:48:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FLEXBUS-DRV-functionality-to-setup-up-multiple-flexbus-regions/m-p/443196#M2873</guid>
      <dc:creator>yorknh</dc:creator>
      <dc:date>2015-09-11T19:48:47Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXBUS_DRV functionality to setup up multiple flexbus regions</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FLEXBUS-DRV-functionality-to-setup-up-multiple-flexbus-regions/m-p/443197#M2874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Larry,&lt;/P&gt;&lt;P&gt;Yes, it's unavailable to configure additional region by using some specific functions that from the KSDK 1.2.0.&lt;/P&gt;&lt;P&gt;Below is an example of setup flow, and you can follow the flow to setup other regions of the FlexBus.&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="_jivemacro_uid_14423827406086845 jive_macro_code jive_text_macro" data-renderedposition="70_8_1232_515" jivemacro_uid="_14423827406086845" modifiedtitle="true"&gt;&lt;/PRE&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;#define FLEX_BASE_ADDRESS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;0x6000&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;#define SRAM_BASE_ADDRESS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;0x8000&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;#define FLEX_ADRESS_MASK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;0x000f&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;#define MRAM_CHIP_SELECTION&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;2&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;#define LCD_CHIP_SELECTION&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;0&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void lcd_flexbus_init(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;configure_flexbus_pins(0);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;CLOCK_HAL_SetDivider(SIM_BASE,kClockDividerOutdiv3,3);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;SIM_HAL_SetFlexbusSecurityLevelMode(SIM_BASE,kSimFbslLevel3);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;SIM_HAL_EnableFlexbusClock(SIM_BASE,0);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;FB_HAL_SetChipSelectValidCmd(FB_BASE,LCD_CHIP_SELECTION,1);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;FB_HAL_WriteBaseAddr(FB_BASE,LCD_CHIP_SELECTION,FLEX_BASE_ADDRESS);&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;FB_HAL_SetByteLaneShift(FB_BASE,LCD_CHIP_SELECTION,kFlexbus_shifted);&amp;nbsp; &lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;FB_HAL_SetAutoAcknowledgeCmd(FB_BASE,LCD_CHIP_SELECTION,1);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;FB_HAL_SetPortSize(FB_BASE,LCD_CHIP_SELECTION,kFlexbus_2bytes);&amp;nbsp; &lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;FB_HAL_SetByteModeCmd(FB_BASE,MRAM_CHIP_SELECTION,1);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;FB_HAL_SetMultiplexControlGroup2(FB_BASE,kFlexbus_multiplex_group2_FB_BE_31_24);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;FB_HAL_SetMultiplexControlGroup3(FB_BASE,kFlexbus_multiplex_group3_FB_BE_23_16);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;FB_HAL_SetMultiplexControlGroup4(FB_BASE,kFlexbus_multiplex_group4_FB_CS2);&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Sep 2015 05:52:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FLEXBUS-DRV-functionality-to-setup-up-multiple-flexbus-regions/m-p/443197#M2874</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-09-16T05:52:50Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXBUS_DRV functionality to setup up multiple flexbus regions</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FLEXBUS-DRV-functionality-to-setup-up-multiple-flexbus-regions/m-p/443198#M2875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ping,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Definitely correct me if I am wrong, but I don't think some of these calls are supported in KSDK 1.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example FB should be Flexbus. FB_HAL_WriteBaseAddr should be Flexbus_HAL_WriteAddr, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Oct 2015 16:52:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FLEXBUS-DRV-functionality-to-setup-up-multiple-flexbus-regions/m-p/443198#M2875</guid>
      <dc:creator>davidtietz</dc:creator>
      <dc:date>2015-10-05T16:52:22Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXBUS_DRV functionality to setup up multiple flexbus regions</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FLEXBUS-DRV-functionality-to-setup-up-multiple-flexbus-regions/m-p/443199#M2876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;Thanks for your feedback.&lt;/P&gt;&lt;P&gt;In the KSDK 1.2, it should use the Flexbus_HAL_WriteAddr instead of the FB_HAL_WriteBaseAddr.&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Ping&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Oct 2015 07:29:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FLEXBUS-DRV-functionality-to-setup-up-multiple-flexbus-regions/m-p/443199#M2876</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-10-08T07:29:49Z</dc:date>
    </item>
  </channel>
</rss>