<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Re: adc dma pdb</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/adc-dma-pdb/m-p/434980#M2657</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am curious if you have clear the DMA CH1 related interrupt request and Done Flag.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Aug 2015 07:23:20 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2015-08-13T07:23:20Z</dc:date>
    <item>
      <title>adc dma pdb</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/adc-dma-pdb/m-p/434979#M2656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello everybody,&lt;/P&gt;&lt;P&gt;I'm using KV31F256 microcontroller and KSDK 1.2 on IAR Embedded workbench.&lt;/P&gt;&lt;P&gt;Here is my problem i configured dma channel 0 on pdb request and in this transfer i configured ADC0 SC1A register throw a buffer i created so&amp;nbsp; it can generate a soft trigger to begin adc0 conversion.&lt;/P&gt;&lt;P&gt;In the other hand i configured dma channel 1 on ADC0 COCO request to transfer data from ADC0 RA to a buffer i created.&lt;/P&gt;&lt;P&gt;So regarding to this configuration i expected to have one conversion after each PDB request.&lt;/P&gt;&lt;P&gt;To check this i configured a dma channel1 interrupt and i set then reset a pin to see a pulse at the oscilloscope each time a conversion is complete.&lt;/P&gt;&lt;P&gt;here is my problem i got a continuous train of pulses that are not synchronized with the pdb request so i checked the adc0 and it is not configured in continuous mode so i didn't understand why i didn't have the desired behavior.&lt;/P&gt;&lt;P&gt;Can anyone help me please.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2015 21:09:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/adc-dma-pdb/m-p/434979#M2656</guid>
      <dc:creator>benelghali</dc:creator>
      <dc:date>2015-08-12T21:09:04Z</dc:date>
    </item>
    <item>
      <title>Re: adc dma pdb</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/adc-dma-pdb/m-p/434980#M2657</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am curious if you have clear the DMA CH1 related interrupt request and Done Flag.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2015 07:23:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/adc-dma-pdb/m-p/434980#M2657</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-08-13T07:23:20Z</dc:date>
    </item>
  </channel>
</rss>