<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Flash Demo Swap Feature</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Flash-Demo-Swap-Feature/m-p/431662#M2580</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the demonstration of the flash swap feature in the Demo Flash application, the implementation seems to be a hybrid of calls to PFlashSwapCtl and a call to PFlashSwap which utilizes the SwapCallback function.&amp;nbsp; The documentation states in section 10.5 "Note: Callback functions are not currently supported during flash erase or program operations".&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone explain why this demo is not a single call to PFlashSwap with calls to erase a programming functions implemented in the callback function?&amp;nbsp; This seems to be the intention of the API author.&amp;nbsp; (see Standard Software Driver (SSD) for C90TFS/FTFx Manual). &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, does the note mean that the PFlashSwap function does not support erase or program operations OR does it mean the the DEMO does not support erase and program operations in the call back?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Nov 2015 19:07:52 GMT</pubDate>
    <dc:creator>tomtalkington</dc:creator>
    <dc:date>2015-11-20T19:07:52Z</dc:date>
    <item>
      <title>Flash Demo Swap Feature</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Flash-Demo-Swap-Feature/m-p/431662#M2580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the demonstration of the flash swap feature in the Demo Flash application, the implementation seems to be a hybrid of calls to PFlashSwapCtl and a call to PFlashSwap which utilizes the SwapCallback function.&amp;nbsp; The documentation states in section 10.5 "Note: Callback functions are not currently supported during flash erase or program operations".&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone explain why this demo is not a single call to PFlashSwap with calls to erase a programming functions implemented in the callback function?&amp;nbsp; This seems to be the intention of the API author.&amp;nbsp; (see Standard Software Driver (SSD) for C90TFS/FTFx Manual). &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, does the note mean that the PFlashSwap function does not support erase or program operations OR does it mean the the DEMO does not support erase and program operations in the call back?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2015 19:07:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Flash-Demo-Swap-Feature/m-p/431662#M2580</guid>
      <dc:creator>tomtalkington</dc:creator>
      <dc:date>2015-11-20T19:07:52Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Demo Swap Feature</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Flash-Demo-Swap-Feature/m-p/431663#M2581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tom Talkington:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the delayed response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you mean the KSDK flash demo, I think the demo project calls the &lt;STRONG&gt;PFlashSwapCtl&lt;/STRONG&gt; to be compatible with the rest of the application, since the demo uses some other features of the flash driver. But yes you should be able to simply call the &lt;STRONG&gt;PFlashSwap&lt;/STRONG&gt; API and implement all the erasing and programming in the callbacks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding the note, I did not find it, can you point me to the exact document? Erasing and programming are fully supported in the &lt;STRONG&gt;PFlashSwap&lt;/STRONG&gt; callbacks, in fact this is done in the Flash Demo.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 29 Nov 2015 23:01:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Flash-Demo-Swap-Feature/m-p/431663#M2581</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-11-29T23:01:09Z</dc:date>
    </item>
  </channel>
</rss>