<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic DSPI DMA slave on K64 in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/DSPI-DMA-slave-on-K64/m-p/429600#M2474</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is on &lt;STRONG&gt;FRDM-K64&lt;/STRONG&gt; board.&lt;/P&gt;&lt;P&gt;I needed to implement sort of SPI passthrough, so I've used SPI0 for master reads from a peripheral and SPI1 in slave mode to provide data to the external host. For performance reasons I need DMA on both SPI0 and SPI1. However what I found out is that when I call DSPI_DRV_EdmaSlaveTransfer (blocking or non-blocking) and provide say 160 bytes to be transferred, what comes over the wire is 1st byte, followed by the 2nd byte repeated through the rest of the packet. E.g.&lt;/P&gt;&lt;P&gt;0, 1, 2, 3, 4....&lt;/P&gt;&lt;P&gt;will come across as &lt;/P&gt;&lt;P&gt;0, 1, 1, 1, 1, 1...&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;During the same transfer the data comes across just fine in the other direction. So to summarize - on SPI1/2 in DMA slave mode MISO fails but MOSI works. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This happens only in DMA mode and only on SPI1 and SPI2. Of course SPI1 and 2 are special on K64 in the sense that they use shared DMA channel for tx/rx. Is there any fix or workaround for this? The issue can be easily replicated by taking DSPI DMA slave sample from the SDK and modifying it to use SPI1 instead of the SPI0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Nov 2015 19:39:12 GMT</pubDate>
    <dc:creator>alexfeinman</dc:creator>
    <dc:date>2015-11-20T19:39:12Z</dc:date>
    <item>
      <title>DSPI DMA slave on K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/DSPI-DMA-slave-on-K64/m-p/429600#M2474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is on &lt;STRONG&gt;FRDM-K64&lt;/STRONG&gt; board.&lt;/P&gt;&lt;P&gt;I needed to implement sort of SPI passthrough, so I've used SPI0 for master reads from a peripheral and SPI1 in slave mode to provide data to the external host. For performance reasons I need DMA on both SPI0 and SPI1. However what I found out is that when I call DSPI_DRV_EdmaSlaveTransfer (blocking or non-blocking) and provide say 160 bytes to be transferred, what comes over the wire is 1st byte, followed by the 2nd byte repeated through the rest of the packet. E.g.&lt;/P&gt;&lt;P&gt;0, 1, 2, 3, 4....&lt;/P&gt;&lt;P&gt;will come across as &lt;/P&gt;&lt;P&gt;0, 1, 1, 1, 1, 1...&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;During the same transfer the data comes across just fine in the other direction. So to summarize - on SPI1/2 in DMA slave mode MISO fails but MOSI works. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This happens only in DMA mode and only on SPI1 and SPI2. Of course SPI1 and 2 are special on K64 in the sense that they use shared DMA channel for tx/rx. Is there any fix or workaround for this? The issue can be easily replicated by taking DSPI DMA slave sample from the SDK and modifying it to use SPI1 instead of the SPI0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2015 19:39:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/DSPI-DMA-slave-on-K64/m-p/429600#M2474</guid>
      <dc:creator>alexfeinman</dc:creator>
      <dc:date>2015-11-20T19:39:12Z</dc:date>
    </item>
    <item>
      <title>Re: DSPI DMA slave on K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/DSPI-DMA-slave-on-K64/m-p/429601#M2475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alex,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recreated the scenario and I got the same issue, by debugging I saw that the DMA TCDs are fulfilled Ok so I don't know where the problem is. If I found this as an issue I will report it to the development team. In the meantime, I will be working to solve the problem or to find a workaround.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have any discovering on this please don't hesitate on share it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Earl Ramírez.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 18:01:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/DSPI-DMA-slave-on-K64/m-p/429601#M2475</guid>
      <dc:creator>EarlOrlando</dc:creator>
      <dc:date>2015-12-08T18:01:40Z</dc:date>
    </item>
    <item>
      <title>Re: DSPI DMA slave on K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/DSPI-DMA-slave-on-K64/m-p/429602#M2476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello again Alex,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached you will find a workaround to this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Replace the file &lt;STRONG&gt;fsl_dspi_edma_slave_driver.c&lt;/STRONG&gt; which is located at &lt;STRONG&gt;C:\Freescale\KSDK_1.3.0\platform\drivers\src\dspi&lt;/STRONG&gt; with the attached version, and then rebuild the platform library (&lt;STRONG&gt;C:\Freescale\KSDK_1.3.0\lib\ksdk_platform_lib\kds\K64F12&lt;/STRONG&gt;).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There was a step out of order when configuring the eDMA TX channel that caused the issue. You can locate the changes by searching for the "FIX" comments in the file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Earl.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: Calibri; font-size: 11.0pt; color: #c55a11;"&gt;&lt;SPAN style="font-weight: bold;"&gt;/* If this post answers your question please click the Correct Answer button. */&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jan 2016 23:55:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/DSPI-DMA-slave-on-K64/m-p/429602#M2476</guid>
      <dc:creator>EarlOrlando</dc:creator>
      <dc:date>2016-01-07T23:55:28Z</dc:date>
    </item>
  </channel>
</rss>