<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックRe: FTM interrupt using KDS SDK</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FTM-interrupt-using-KDS-SDK/m-p/428062#M2387</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason,&lt;/P&gt;&lt;P&gt;Attach KDS_3.0 + KSDK_1.3 new project that uses PE for FRDM-K64F.&lt;/P&gt;&lt;P&gt;The project has a bunch of example stuff (using FTM's for PWM, GPIO, multiple tasks) to it but I setup flexTimer3:fsl_ftm component as a timer.&amp;nbsp; The overflow ISR is in Event.c and the start/stop/read timer code is in os_tasks.c Task1_task();&lt;/P&gt;&lt;P&gt;Two locations in the Task1_task() are provided for the test but only enable one #define at a time.&amp;nbsp; The first will return counter result with FTM3 no ever having overflowed.&lt;/P&gt;&lt;P&gt;The second location uses the FTM3 and returns variable timer result as it is dependent on user input.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Nov 2015 15:40:22 GMT</pubDate>
    <dc:creator>DavidS</dc:creator>
    <dc:date>2015-11-23T15:40:22Z</dc:date>
    <item>
      <title>FTM interrupt using KDS SDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FTM-interrupt-using-KDS-SDK/m-p/428061#M2386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&amp;nbsp; I'm using a K64 processor with KDS, and using MQX and Processor Expert via the SDK.&amp;nbsp; I setup a simple FTM timer with an interrupt, but when I run the code using the debugger I never hit the interrupt handler.&amp;nbsp; Has anyone been able to get this to work and if so, could you share your project and/or a screenshot of how you setup your FTM timer component please?&amp;nbsp; Thank you in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Nov 2015 17:53:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FTM-interrupt-using-KDS-SDK/m-p/428061#M2386</guid>
      <dc:creator>jasonpionke</dc:creator>
      <dc:date>2015-11-19T17:53:44Z</dc:date>
    </item>
    <item>
      <title>Re: FTM interrupt using KDS SDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FTM-interrupt-using-KDS-SDK/m-p/428062#M2387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason,&lt;/P&gt;&lt;P&gt;Attach KDS_3.0 + KSDK_1.3 new project that uses PE for FRDM-K64F.&lt;/P&gt;&lt;P&gt;The project has a bunch of example stuff (using FTM's for PWM, GPIO, multiple tasks) to it but I setup flexTimer3:fsl_ftm component as a timer.&amp;nbsp; The overflow ISR is in Event.c and the start/stop/read timer code is in os_tasks.c Task1_task();&lt;/P&gt;&lt;P&gt;Two locations in the Task1_task() are provided for the test but only enable one #define at a time.&amp;nbsp; The first will return counter result with FTM3 no ever having overflowed.&lt;/P&gt;&lt;P&gt;The second location uses the FTM3 and returns variable timer result as it is dependent on user input.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Nov 2015 15:40:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FTM-interrupt-using-KDS-SDK/m-p/428062#M2387</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2015-11-23T15:40:22Z</dc:date>
    </item>
  </channel>
</rss>