<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックWrite bytes to sending by uart</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Write-bytes-to-sending-by-uart/m-p/425002#M2311</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody, i am playing with a thermal printer and the kinetis FRDM _k64f , i send text by UART to the printer succesfuly but if i want change the printer settings i need to send not a char or a string , i need to send or writr a byte to the UART , i have been doing in arduino using write.byte but oviously in c it doesn´t work in the same way . Some one have any idea to send an hexadecimal byte ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Sep 2015 17:04:12 GMT</pubDate>
    <dc:creator>marceladuenas</dc:creator>
    <dc:date>2015-09-03T17:04:12Z</dc:date>
    <item>
      <title>Write bytes to sending by uart</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Write-bytes-to-sending-by-uart/m-p/425002#M2311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody, i am playing with a thermal printer and the kinetis FRDM _k64f , i send text by UART to the printer succesfuly but if i want change the printer settings i need to send not a char or a string , i need to send or writr a byte to the UART , i have been doing in arduino using write.byte but oviously in c it doesn´t work in the same way . Some one have any idea to send an hexadecimal byte ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 17:04:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Write-bytes-to-sending-by-uart/m-p/425002#M2311</guid>
      <dc:creator>marceladuenas</dc:creator>
      <dc:date>2015-09-03T17:04:12Z</dc:date>
    </item>
    <item>
      <title>Re: Write bytes to sending by uart</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Write-bytes-to-sending-by-uart/m-p/425003#M2312</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marcela,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may use UART_DRV_SendDataBlocking() or UART_DRV_SendData() to send the raw data out via UART. Please refer to C:\Freescale\KSDK_1.2.0\examples\frdmk64f\driver_examples\uart for more details.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Freescale Technical Support&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 Sep 2015 05:58:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Write-bytes-to-sending-by-uart/m-p/425003#M2312</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2015-09-06T05:58:15Z</dc:date>
    </item>
  </channel>
</rss>