<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development KitのトピックExample of adc16 with hardware trigger</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Example-of-adc16-with-hardware-trigger/m-p/423392#M2240</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like like to use a hardware input to trigger an ADC conversion. As I understand the manual, this could be either through the PDB or directly with the ADHWT input, but I'm not able to make the full connection.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My design has a front end with a peak detector that gives a rising edge when the peak is found. I know I could use that edge as an interrupt to generate a software trigger and achieve the same result. But, if possible, I'd like the hardware to initiate that process and thus save the interrupt latency time.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there an example that would show me the way?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Aug 2015 19:21:15 GMT</pubDate>
    <dc:creator>davepfaltzgraff</dc:creator>
    <dc:date>2015-08-07T19:21:15Z</dc:date>
    <item>
      <title>Example of adc16 with hardware trigger</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Example-of-adc16-with-hardware-trigger/m-p/423392#M2240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like like to use a hardware input to trigger an ADC conversion. As I understand the manual, this could be either through the PDB or directly with the ADHWT input, but I'm not able to make the full connection.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My design has a front end with a peak detector that gives a rising edge when the peak is found. I know I could use that edge as an interrupt to generate a software trigger and achieve the same result. But, if possible, I'd like the hardware to initiate that process and thus save the interrupt latency time.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there an example that would show me the way?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2015 19:21:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Example-of-adc16-with-hardware-trigger/m-p/423392#M2240</guid>
      <dc:creator>davepfaltzgraff</dc:creator>
      <dc:date>2015-08-07T19:21:15Z</dc:date>
    </item>
    <item>
      <title>Re: Example of adc16 with hardware trigger</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Example-of-adc16-with-hardware-trigger/m-p/423393#M2241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which chip do you use ?&lt;/P&gt;&lt;P&gt;For example the frdmk64, you can find the adc_hw_trigger demo here :&lt;/P&gt;&lt;P&gt;...\Freescale\KSDK_1.2.0\examples\frdmk64f\demo_apps , under it , there have the PDB trigger ADC demo code .&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52164i4E2C3FEAA5B3D09F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2015 01:52:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Example-of-adc16-with-hardware-trigger/m-p/423393#M2241</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-08-10T01:52:17Z</dc:date>
    </item>
    <item>
      <title>Re: Example of adc16 with hardware trigger</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Example-of-adc16-with-hardware-trigger/m-p/423394#M2242</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the pointer. I am using the FRDM-K22F and see that there a corresponding example there. I'll look into it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dave&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2015 13:19:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Example-of-adc16-with-hardware-trigger/m-p/423394#M2242</guid>
      <dc:creator>davepfaltzgraff</dc:creator>
      <dc:date>2015-08-10T13:19:14Z</dc:date>
    </item>
  </channel>
</rss>