<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Windows 7 unable to find COM driver for USB-KW24D512 using example SMAC Connectivity Test</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Windows-7-unable-to-find-COM-driver-for-USB-KW24D512-using/m-p/415823#M1999</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a USB-KW24D512, using it on a Windows 7 64-bit and I have programmed it with the example SMAC Connectivity Test(USB-KW24D512_SMAC_Connectivity Test.srec) which I should be able to connect through a COM port.&amp;nbsp; I'm getting a issue where Windows is unable to load the correct driver, using Update Drivers and manually selecting the path to search, ( C:\Program Files (x86)\Freescale\Drivers\ ), it is not finding it.&amp;nbsp; There is a installer in the C:\Program Files (x86)\Freescale\Drivers\USB-KW24D512 directory, dpinst64.exe, which I have successfully installed.&amp;nbsp; But Windows 7's device manager is still showing it as drivers for this device are NOT installed for the FREESCALE VIRTUAL COM.&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Device: USB-KW24D512&lt;/P&gt;&lt;P&gt;OS: Windows 7 Enterprise 64-bit&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you need more information, let me know.&amp;nbsp; How do I fix this?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Sep 2015 18:08:10 GMT</pubDate>
    <dc:creator>davidguinn</dc:creator>
    <dc:date>2015-09-01T18:08:10Z</dc:date>
    <item>
      <title>Windows 7 unable to find COM driver for USB-KW24D512 using example SMAC Connectivity Test</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Windows-7-unable-to-find-COM-driver-for-USB-KW24D512-using/m-p/415823#M1999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a USB-KW24D512, using it on a Windows 7 64-bit and I have programmed it with the example SMAC Connectivity Test(USB-KW24D512_SMAC_Connectivity Test.srec) which I should be able to connect through a COM port.&amp;nbsp; I'm getting a issue where Windows is unable to load the correct driver, using Update Drivers and manually selecting the path to search, ( C:\Program Files (x86)\Freescale\Drivers\ ), it is not finding it.&amp;nbsp; There is a installer in the C:\Program Files (x86)\Freescale\Drivers\USB-KW24D512 directory, dpinst64.exe, which I have successfully installed.&amp;nbsp; But Windows 7's device manager is still showing it as drivers for this device are NOT installed for the FREESCALE VIRTUAL COM.&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Device: USB-KW24D512&lt;/P&gt;&lt;P&gt;OS: Windows 7 Enterprise 64-bit&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you need more information, let me know.&amp;nbsp; How do I fix this?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Sep 2015 18:08:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Windows-7-unable-to-find-COM-driver-for-USB-KW24D512-using/m-p/415823#M1999</guid>
      <dc:creator>davidguinn</dc:creator>
      <dc:date>2015-09-01T18:08:10Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 7 unable to find COM driver for USB-KW24D512 using example SMAC Connectivity Test</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Windows-7-unable-to-find-COM-driver-for-USB-KW24D512-using/m-p/415824#M2000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figured out the issue, it appears the drivers included with the BeeKit installer ( C:\Program Files (x86)\Freescale\Drivers\USB-KW24D512 ) are a older version and Windows 7 doesn't accept them.&amp;nbsp; If you download the &lt;A class="dtmAssetClick" data-dtmassettype="Download" data-dtmname="USB-KW24D512 Board Support Package" href="http://cache.freescale.com/files/32bit/software/board_support_packages/USBKW24D512-BSP.zip" style="color: #017bba;" target="_blank"&gt;USB-KW24D512 Board Support Package&lt;/A&gt;​ and Browse to the Drivers directory where it is installed and point it at the Drivers directory, it will instsall correctly and then work as expected.&amp;nbsp; I was then able to connect the HyperTerminal to it and get the Connectivity Test menu and interact with it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The BeeKit installed "fsl_ucwnt.inf"&lt;/P&gt;&lt;P&gt;The Support Package installed "fsl_ucwxp.inf"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Sep 2015 19:06:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Windows-7-unable-to-find-COM-driver-for-USB-KW24D512-using/m-p/415824#M2000</guid>
      <dc:creator>davidguinn</dc:creator>
      <dc:date>2015-09-01T19:06:45Z</dc:date>
    </item>
  </channel>
</rss>