<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Re: Keep chip select asserted during multiple DSPI_DRV_MasterTransferBlocking calls?</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Keep-chip-select-asserted-during-multiple-DSPI-DRV/m-p/412174#M1897</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, concatenating buffers will work but I'm not a fan of (1) allocating memory and (2) spending operations on copying chunks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I could modify the master driver as you suggest, but again not a fan because as you guys provide updates to the SDK, I have to remember to go in and change your API.&lt;/P&gt;&lt;P&gt;So perhaps this can be seen as a feature request to support a last_transaction flag in the API.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a side, I think this is a regression in the API as looking at old code (MQX 4.2 era), the spi_memory.c would call fflush(spifd) at the end of the multi-block transfer to deassert the Chip Select.&amp;nbsp; (But perhaps internally, the fwrites were allocating memory!)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Raj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Oct 2015 23:27:17 GMT</pubDate>
    <dc:creator>rajbatra</dc:creator>
    <dc:date>2015-10-05T23:27:17Z</dc:date>
    <item>
      <title>Keep chip select asserted during multiple DSPI_DRV_MasterTransferBlocking calls?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Keep-chip-select-asserted-during-multiple-DSPI-DRV/m-p/412172#M1895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Communicating with some flash that requires the read/write command and data to under a single chip select.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Either controlling the CS myself, or allocating a chunk of memory where I concatenate the two buffers seem inelegant. &lt;/P&gt;&lt;P&gt;I'd like to just call DSPI_DRV_MasterTransferBlocking twice (perhaps a flag that says additional transactions coming). Any way to do this?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Or is there a better API command I should be using?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm on a K64F using latest KSDK &amp;amp; MQX.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Sep 2015 18:06:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Keep-chip-select-asserted-during-multiple-DSPI-DRV/m-p/412172#M1895</guid>
      <dc:creator>rajbatra</dc:creator>
      <dc:date>2015-09-25T18:06:15Z</dc:date>
    </item>
    <item>
      <title>Re: Keep chip select asserted during multiple DSPI_DRV_MasterTransferBlocking calls?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Keep-chip-select-asserted-during-multiple-DSPI-DRV/m-p/412173#M1896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Raj Batra:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The master driver configuration structure &lt;STRONG&gt;dspi_master_state_t&lt;/STRONG&gt; has a field called &lt;STRONG&gt;isChipSelectContinuous&lt;/STRONG&gt;. I guess this should work with only 1 call to &lt;STRONG&gt;DSP_DRV_MasterTransferBlocking&lt;/STRONG&gt;, by concatenating buffers as you mentioned. Have you tried that option?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If that does not fit your requirement then you would need to modify the SPI Master driver and rebuild the KSDK platform library, or use the GPIO driver to control the Chip Select pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Oct 2015 00:52:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Keep-chip-select-asserted-during-multiple-DSPI-DRV/m-p/412173#M1896</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-10-02T00:52:56Z</dc:date>
    </item>
    <item>
      <title>Re: Keep chip select asserted during multiple DSPI_DRV_MasterTransferBlocking calls?</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Keep-chip-select-asserted-during-multiple-DSPI-DRV/m-p/412174#M1897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, concatenating buffers will work but I'm not a fan of (1) allocating memory and (2) spending operations on copying chunks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I could modify the master driver as you suggest, but again not a fan because as you guys provide updates to the SDK, I have to remember to go in and change your API.&lt;/P&gt;&lt;P&gt;So perhaps this can be seen as a feature request to support a last_transaction flag in the API.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a side, I think this is a regression in the API as looking at old code (MQX 4.2 era), the spi_memory.c would call fflush(spifd) at the end of the multi-block transfer to deassert the Chip Select.&amp;nbsp; (But perhaps internally, the fwrites were allocating memory!)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Raj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Oct 2015 23:27:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/Keep-chip-select-asserted-during-multiple-DSPI-DRV/m-p/412174#M1897</guid>
      <dc:creator>rajbatra</dc:creator>
      <dc:date>2015-10-05T23:27:17Z</dc:date>
    </item>
  </channel>
</rss>