<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FRDM-K64F - Any good KSDK v1.2 demo for TCP/IP  in Kinetis Software Development Kit</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K64F-Any-good-KSDK-v1-2-demo-for-TCP-IP/m-p/402431#M1556</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Devan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, sure. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;HTTP Server Demo on lwIP TCP/IP Stack&lt;/STRONG&gt; -&lt;/LI&gt;&lt;/UL&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;This is an HTTPServer set up on lwIP TCP/IP stack with bare metal SDK or different RTOSes. The user uses an Internet browser to send a request for connection. The board acts as an HTTP server and sends a Web page back to the PC.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The demo is located at &lt;EM&gt;&amp;lt;ksdk_path&amp;gt;\examples\frdmk64f\demo_apps\lwip\lwip_httpserver_demo&lt;/EM&gt; for baremetal and RTOS.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Ping Demo on lwIP TCP/IP Stack&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Ping Demo on the lwIP TCP/IP stack which uses the ICMP protocol. The application on board&lt;/P&gt;&lt;P&gt;periodically sends the ICMP echo request to a PC and processes the PC reply. Just type the "ping $board_address" in the PC command window to send an ICMP echo request to the board. The lwIP stack sends the ICMP echo reply back to the PC&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The demo is located at &lt;EM&gt;&amp;lt;ksdk_path&amp;gt;\examples\frdmk64f\demo_apps\lwip\lwip_ping_demo&lt;/EM&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;TCP Echo Demo on lwIP TCP/IP Stack &lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;TCP echo demo on the lwIP TCP/IP stack with bare metal KSDK or different RTOSes, which uses the TCP protocol and acts as an echo server. The application on board sends back the TCP packets from the PC, which can be used to test whether the TCP connection is available.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The demo is located at &lt;EM&gt;&amp;lt;ksdk_path&amp;gt;\examples\frdmk64f\demo_apps\lwip\lwip_tcpecho_demo&lt;/EM&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;UDP Echo Demo on lwIP TCP/IP Stack&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;UDP echo demo on the lwIP TCP/IP stack with bare metal KSDK or different RTOSes, which&lt;/P&gt;&lt;P&gt;uses the UDP protocol and acts as an echo server. The application on board sends back the UDP packets&lt;/P&gt;&lt;P&gt;from the PC, which can be used to test whether the UDP connection is available&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The demo is located at &lt;EM&gt;&amp;lt;ksdk_path&amp;gt;\examples\frdmk64f\demo_apps\lwip\lwip_udpecho_demo&lt;/EM&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Heating, Ventilating, and Air Conditioning on lwIP TCP/IP Stack&amp;nbsp; &lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;This is a simulation of HVAC system with web server using lwIP TCP/IP stack on different RTOSes. The user uses an Internet browser to send a request for connection, to set up HVAC system on board. The board acts as an HTTP server and sends a Web page back to the PC. The user also can directly set up desired temperature by pressing switches on board and observe LEDs status.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The demo is located at &lt;EM&gt;&amp;lt;ksdk_path&amp;gt;\examples\frdmk64f\demo_apps\web_hvac&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps&lt;/P&gt;&lt;P&gt;Iva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jul 2015 05:23:21 GMT</pubDate>
    <dc:creator>ivadorazinova</dc:creator>
    <dc:date>2015-07-13T05:23:21Z</dc:date>
    <item>
      <title>FRDM-K64F - Any good KSDK v1.2 demo for TCP/IP</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K64F-Any-good-KSDK-v1-2-demo-for-TCP-IP/m-p/402430#M1555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any good demo for TCP/IP running on FRDM-K64F board using KDS v3.0 / KSDK v1.2?&lt;/P&gt;&lt;P&gt;I am looking for a small foot-print that could boot from a smallest K6x MCU.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Devan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Jul 2015 22:13:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K64F-Any-good-KSDK-v1-2-demo-for-TCP-IP/m-p/402430#M1555</guid>
      <dc:creator>Deejay</dc:creator>
      <dc:date>2015-07-12T22:13:36Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F - Any good KSDK v1.2 demo for TCP/IP</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K64F-Any-good-KSDK-v1-2-demo-for-TCP-IP/m-p/402431#M1556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Devan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, sure. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;HTTP Server Demo on lwIP TCP/IP Stack&lt;/STRONG&gt; -&lt;/LI&gt;&lt;/UL&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;This is an HTTPServer set up on lwIP TCP/IP stack with bare metal SDK or different RTOSes. The user uses an Internet browser to send a request for connection. The board acts as an HTTP server and sends a Web page back to the PC.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The demo is located at &lt;EM&gt;&amp;lt;ksdk_path&amp;gt;\examples\frdmk64f\demo_apps\lwip\lwip_httpserver_demo&lt;/EM&gt; for baremetal and RTOS.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Ping Demo on lwIP TCP/IP Stack&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Ping Demo on the lwIP TCP/IP stack which uses the ICMP protocol. The application on board&lt;/P&gt;&lt;P&gt;periodically sends the ICMP echo request to a PC and processes the PC reply. Just type the "ping $board_address" in the PC command window to send an ICMP echo request to the board. The lwIP stack sends the ICMP echo reply back to the PC&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The demo is located at &lt;EM&gt;&amp;lt;ksdk_path&amp;gt;\examples\frdmk64f\demo_apps\lwip\lwip_ping_demo&lt;/EM&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;TCP Echo Demo on lwIP TCP/IP Stack &lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;TCP echo demo on the lwIP TCP/IP stack with bare metal KSDK or different RTOSes, which uses the TCP protocol and acts as an echo server. The application on board sends back the TCP packets from the PC, which can be used to test whether the TCP connection is available.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The demo is located at &lt;EM&gt;&amp;lt;ksdk_path&amp;gt;\examples\frdmk64f\demo_apps\lwip\lwip_tcpecho_demo&lt;/EM&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;UDP Echo Demo on lwIP TCP/IP Stack&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;UDP echo demo on the lwIP TCP/IP stack with bare metal KSDK or different RTOSes, which&lt;/P&gt;&lt;P&gt;uses the UDP protocol and acts as an echo server. The application on board sends back the UDP packets&lt;/P&gt;&lt;P&gt;from the PC, which can be used to test whether the UDP connection is available&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The demo is located at &lt;EM&gt;&amp;lt;ksdk_path&amp;gt;\examples\frdmk64f\demo_apps\lwip\lwip_udpecho_demo&lt;/EM&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Heating, Ventilating, and Air Conditioning on lwIP TCP/IP Stack&amp;nbsp; &lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;This is a simulation of HVAC system with web server using lwIP TCP/IP stack on different RTOSes. The user uses an Internet browser to send a request for connection, to set up HVAC system on board. The board acts as an HTTP server and sends a Web page back to the PC. The user also can directly set up desired temperature by pressing switches on board and observe LEDs status.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The demo is located at &lt;EM&gt;&amp;lt;ksdk_path&amp;gt;\examples\frdmk64f\demo_apps\web_hvac&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps&lt;/P&gt;&lt;P&gt;Iva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jul 2015 05:23:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K64F-Any-good-KSDK-v1-2-demo-for-TCP-IP/m-p/402431#M1556</guid>
      <dc:creator>ivadorazinova</dc:creator>
      <dc:date>2015-07-13T05:23:21Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F - Any good KSDK v1.2 demo for TCP/IP</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K64F-Any-good-KSDK-v1-2-demo-for-TCP-IP/m-p/402432#M1557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Iva,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks heaps!&lt;/P&gt;&lt;P&gt;Sure, definitely I will take a look at the suggested list of demos and will get back to you if I need more help.&lt;/P&gt;&lt;P&gt;Have a great day!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Devan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2015 06:48:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-K64F-Any-good-KSDK-v1-2-demo-for-TCP-IP/m-p/402432#M1557</guid>
      <dc:creator>Deejay</dc:creator>
      <dc:date>2015-07-14T06:48:21Z</dc:date>
    </item>
  </channel>
</rss>