<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Software Development Kit中的主题 Re: FRDM-KL25Z SPI using KSDK1.2.0 for MCP23S17</title>
    <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-KL25Z-SPI-using-KSDK1-2-0-for-MCP23S17/m-p/392143#M1179</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Nelson,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your second question, If you use the SPI module of Kl25 as master and want to transfer multiple bytes using the same function so the CS pin toggles once for all the bytes, you can not use the /SS pin of master SPI to generate the output signal to select the slave SPI automatically. I suggest you connect any GPIO pin(even the /SS pin of KL25 can be configured as GPIO output function) of Kl25 to the /SS pin of slave SPI, while the SPI of KL25 is master. Before you transfer the first byte, you can clear the GPIO, then write the first byte to SPI data register, poll the SPTEF bit in SPIx_S, if the bit is set, write the second byte, then poll the SPTEF bit in SPIx_S, ...when the required byte has transfered, set the GPIO, and have a delay. In the process, you have to set the CPHA&amp;nbsp; bit so that the MISO bit is valid by the edge of SPSCK signal.&lt;/P&gt;&lt;P&gt;Regarding your first question, pls check if there are signals for the SPSCK, MOSI,MISO and /SS, if there is issue, pls check the SPI register in the debugger of the tools. I am not clear what your issue is now.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Sep 2015 06:31:49 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2015-09-21T06:31:49Z</dc:date>
    <item>
      <title>FRDM-KL25Z SPI using KSDK1.2.0 for MCP23S17</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-KL25Z-SPI-using-KSDK1-2-0-for-MCP23S17/m-p/392141#M1177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ive been trying to understand the SPI polling technique from FRDM-KL25Z(master) with my PIC18F46K22(slave). This worked flawlessly, I could detect all the packets sent over this channel. Now I thought of using my MCP23S17(I/O Expander) with the FRDM-KL25Z. Since ive already tried sending the same instructions on PIC18F and it worked well there I was assuming it would work here as well. But there was absolutely no response from the MCP module. Just to verify ive bricked the module or not i checked with PIC18F and yet again it worked just fine. Ive attached the code its a modification of the existing SPI Looping technique in Master mode available in KSDK1.2.0 examples folder. &lt;/P&gt;&lt;P&gt;C:\Freescale\KSDK_1.2.0\examples\frdmkl25z\driver_examples\spi\spi_polling&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My code would read as follows:&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#include &amp;lt;string.h&amp;gt;&lt;/P&gt;&lt;P&gt;#include "fsl_spi_master_driver.h"&lt;/P&gt;&lt;P&gt;#include "fsl_clock_manager.h"&lt;/P&gt;&lt;P&gt;#include "fsl_debug_console.h"&lt;/P&gt;&lt;P&gt;#include "board.h"&lt;/P&gt;&lt;P&gt;#include &amp;lt;stdio.h&amp;gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;// MCP23S17 SPI Slave Device&lt;/P&gt;&lt;P&gt;#define SPI_SLAVE_ID&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x40&lt;/P&gt;&lt;P&gt;#define SPI_SLAVE_ADDR&amp;nbsp; 0x07&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // A2=0,A1=0,A0=0&lt;/P&gt;&lt;P&gt;#define SPI_SLAVE_WRITE 0x00&lt;/P&gt;&lt;P&gt;#define SPI_SLAVE_READ&amp;nbsp; 0x01&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;// MCP23S17 Registers Definition for BANK=0 (default)&lt;/P&gt;&lt;P&gt;#define IODIRA 0x00&lt;/P&gt;&lt;P&gt;#define IODIRB 0x10&lt;/P&gt;&lt;P&gt;#define IOCONA 0x0A&lt;/P&gt;&lt;P&gt;#define GPPUA&amp;nbsp; 0x06&lt;/P&gt;&lt;P&gt;#define GPPUB&amp;nbsp; 0x16&lt;/P&gt;&lt;P&gt;#define GPIOA_Exp&amp;nbsp; 0x09&lt;/P&gt;&lt;P&gt;#define GPIOB_Exp&amp;nbsp; 0x19&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/*******************************************************************************&lt;/P&gt;&lt;P&gt; * Definitions&lt;/P&gt;&lt;P&gt; ******************************************************************************/&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5;"&gt;#define SPI_MASTER_INSTANCE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (0)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*! User change define to choose SPI instance */&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5;"&gt;#define TRANSFER_SIZE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (64)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;#define TRANSFER_BAUDRATE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (500000U)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*! Transfer baudrate - 500k */&lt;/P&gt;&lt;P&gt;#define MASTER_TRANSFER_TIMEOUT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (5000U)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*! Transfer timeout of master - 5s */&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/* Setup the board as a spi master */&lt;/P&gt;&lt;P&gt;int main (void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t spiSourceClock;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_Type * spiBaseAddr = g_spiBase[SPI_MASTER_INSTANCE];;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* init the hardware, this also sets up up the SPI pins for each specific SoC */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; hardware_init();&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; OSA_Init();&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Enable clock for SPI&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CLOCK_SYS_EnableSpiClock(SPI_MASTER_INSTANCE);&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // configure the run-time state struct with the source clock value&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; spiSourceClock = CLOCK_SYS_GetSpiFreq(SPI_MASTER_INSTANCE);&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Reset the SPI module to it's default state, which includes SPI disabled&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_Init(spiBaseAddr);&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set SPI to master mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_SetMasterSlave(spiBaseAddr, kSpiMaster);&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set slave select to GPIO output mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_SetSlaveSelectOutputMode(spiBaseAddr, kSpiSlaveSelect_AsGpio); /*Change introduced by me since the data need to be sent 3bytes at a time, i.e. 1)SlaveID, 2)Register,3)value*/&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set the SPI pin mode to normal mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_SetPinMode(spiBaseAddr, kSpiPinMode_Normal);&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI0_EN;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Defined&amp;nbsp; and configured in gpio_pins.h,pin_mux.c and board.h&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_ON;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // SPI system Enable&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_Enable(spiBaseAddr);&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Configure the bus to access the provided device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_SetBaud(spiBaseAddr, TRANSFER_BAUDRATE, spiSourceClock);&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Setup format as same as slave&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_SetDataFormat(spiBaseAddr, kSpiClockPolarity_ActiveHigh, kSpiClockPhase_FirstEdge, kSpiMsbFirst);&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Disable module to clear the shift register&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_Disable(spiBaseAddr);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_Enable(spiBaseAddr);&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //IOCONA register is set to 0x88&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_OFF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, SPI_SLAVE_ID);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, IOCONA);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, 0x88); //Tried 0x80 as well for Address mode disbaled&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_ON;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //PORTA of IO-expander is set to Output mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_OFF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr,SPI_SLAVE_ID);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, IODIRA);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, 0x00);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_ON;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Set all pins of PORTA high&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_OFF;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, SPI_SLAVE_ID);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, GPIOA_Exp);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, 0xFF);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_ON;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while(1)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5;"&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/*******************************************************************************&lt;/P&gt;&lt;P&gt; * EOF&lt;/P&gt;&lt;P&gt; ******************************************************************************/&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Nelson Lobo&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338610"&gt;spi_polling-.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2015 15:46:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-KL25Z-SPI-using-KSDK1-2-0-for-MCP23S17/m-p/392141#M1177</guid>
      <dc:creator>nelsonlobo</dc:creator>
      <dc:date>2015-09-18T15:46:03Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z SPI using KSDK1.2.0 for MCP23S17</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-KL25Z-SPI-using-KSDK1-2-0-for-MCP23S17/m-p/392142#M1178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In the attachment please do the following for pin_mux.c:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTC,4u,kPortMuxAsGpio); /* PCS0 */&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTC,4u,kPortMuxAlt2); /* PCS0 */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since we will be using it as GPIO.&lt;/P&gt;&lt;P&gt;Also is there any way i could send multiple bytes using the same function so the CS pin toggles once for all the bytes, just as my case for MCP23S17.&lt;/P&gt;&lt;P&gt;If there's a better alternative to control this IO expander, Im all ears :smileywink:.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Nelson Lobo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2015 15:55:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-KL25Z-SPI-using-KSDK1-2-0-for-MCP23S17/m-p/392142#M1178</guid>
      <dc:creator>nelsonlobo</dc:creator>
      <dc:date>2015-09-18T15:55:12Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z SPI using KSDK1.2.0 for MCP23S17</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-KL25Z-SPI-using-KSDK1-2-0-for-MCP23S17/m-p/392143#M1179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Nelson,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your second question, If you use the SPI module of Kl25 as master and want to transfer multiple bytes using the same function so the CS pin toggles once for all the bytes, you can not use the /SS pin of master SPI to generate the output signal to select the slave SPI automatically. I suggest you connect any GPIO pin(even the /SS pin of KL25 can be configured as GPIO output function) of Kl25 to the /SS pin of slave SPI, while the SPI of KL25 is master. Before you transfer the first byte, you can clear the GPIO, then write the first byte to SPI data register, poll the SPTEF bit in SPIx_S, if the bit is set, write the second byte, then poll the SPTEF bit in SPIx_S, ...when the required byte has transfered, set the GPIO, and have a delay. In the process, you have to set the CPHA&amp;nbsp; bit so that the MISO bit is valid by the edge of SPSCK signal.&lt;/P&gt;&lt;P&gt;Regarding your first question, pls check if there are signals for the SPSCK, MOSI,MISO and /SS, if there is issue, pls check the SPI register in the debugger of the tools. I am not clear what your issue is now.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Sep 2015 06:31:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-KL25Z-SPI-using-KSDK1-2-0-for-MCP23S17/m-p/392143#M1179</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2015-09-21T06:31:49Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z SPI using KSDK1.2.0 for MCP23S17</title>
      <link>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-KL25Z-SPI-using-KSDK1-2-0-for-MCP23S17/m-p/392144#M1180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi xiangjun.rong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based on your comments i did use delays in the appropriate&amp;nbsp; instance and now the code works just fine.&lt;/P&gt;&lt;P&gt;Here is the code:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#include &amp;lt;string.h&amp;gt;&lt;/P&gt;&lt;P&gt;#include "fsl_spi_master_driver.h"&lt;/P&gt;&lt;P&gt;#include "fsl_clock_manager.h"&lt;/P&gt;&lt;P&gt;#include "fsl_debug_console.h"&lt;/P&gt;&lt;P&gt;#include "board.h"&lt;/P&gt;&lt;P&gt;#include &amp;lt;stdio.h&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// MCP23S17 SPI Slave Device&lt;/P&gt;&lt;P&gt;#define SPI_SLAVE_ID&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x40&lt;/P&gt;&lt;P&gt;#define SPI_SLAVE_ADDR&amp;nbsp; 0x07&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // A2=0,A1=0,A0=0&lt;/P&gt;&lt;P&gt;#define SPI_SLAVE_WRITE 0x00&lt;/P&gt;&lt;P&gt;#define SPI_SLAVE_READ&amp;nbsp; 0x01&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// MCP23S17 Registers Definition for BANK=0 (default)&lt;/P&gt;&lt;P&gt;#define IODIRA 0x00&lt;/P&gt;&lt;P&gt;#define IODIRB 0x10&lt;/P&gt;&lt;P&gt;#define IOCONA 0x0A&lt;/P&gt;&lt;P&gt;#define GPPUA&amp;nbsp; 0x06&lt;/P&gt;&lt;P&gt;#define GPPUB&amp;nbsp; 0x16&lt;/P&gt;&lt;P&gt;#define GPIOA_Exp&amp;nbsp; 0x09&lt;/P&gt;&lt;P&gt;#define GPIOB_Exp&amp;nbsp; 0x19&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*******************************************************************************&lt;/P&gt;&lt;P&gt; * Definitions&lt;/P&gt;&lt;P&gt; ******************************************************************************/&lt;/P&gt;&lt;P&gt;#define SPI_MASTER_INSTANCE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (0)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*! User change define to choose SPI instance */&lt;/P&gt;&lt;P&gt;#define TRANSFER_SIZE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (64)&lt;/P&gt;&lt;P&gt;#define TRANSFER_BAUDRATE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (1000000U)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*! Transfer baudrate - 500k */&lt;/P&gt;&lt;P&gt;#define MASTER_TRANSFER_TIMEOUT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (5000U)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*! Transfer timeout of master - 5s */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void wait_tcy(unsigned int wait);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Setup the board as a spi master */&lt;/P&gt;&lt;P&gt;int main (void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t spiSourceClock;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_Type * spiBaseAddr = g_spiBase[SPI_MASTER_INSTANCE];;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* init the hardware, this also sets up up the SPI pins for each specific SoC */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; hardware_init();&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; OSA_Init();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Enable clock for SPI&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CLOCK_SYS_EnableSpiClock(SPI_MASTER_INSTANCE);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // configure the run-time state struct with the source clock value&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; spiSourceClock = CLOCK_SYS_GetSpiFreq(SPI_MASTER_INSTANCE);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Reset the SPI module to it's default state, which includes SPI disabled&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_Init(spiBaseAddr);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set SPI to master mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_SetMasterSlave(spiBaseAddr, kSpiMaster);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set slave select to GPIO output mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_SetSlaveSelectOutputMode(spiBaseAddr, kSpiSlaveSelect_AsGpio); /*Change introduced by me since the data need to be sent 3bytes at a time, i.e. 1)SlaveID, 2)Register,3)value*/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set the SPI pin mode to normal mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_SetPinMode(spiBaseAddr, kSpiPinMode_Normal);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI0_EN;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Defined&amp;nbsp; and configured in gpio_pins.h,pin_mux.c and board.h&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_OFF;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // SPI system Enable&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_Enable(spiBaseAddr);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Configure the bus to access the provided device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_SetBaud(spiBaseAddr, TRANSFER_BAUDRATE, spiSourceClock);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Setup format as same as slave&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_SetDataFormat(spiBaseAddr, kSpiClockPolarity_ActiveHigh, kSpiClockPhase_FirstEdge, kSpiMsbFirst);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Disable module to clear the shift register&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_Disable(spiBaseAddr);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_Enable(spiBaseAddr);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //IOCONA register is set to 0x88&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_ON;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, SPI_SLAVE_ID);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, IOCONA);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, 0x88); //Tried 0x80 as well for Address mode disbaled&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; OSA_TimeDelay(1);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //wait for 1ms&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_OFF;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //PORTA of IO-expander is set to Output mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_ON;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr,SPI_SLAVE_ID);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, IODIRA);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, 0x00);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; OSA_TimeDelay(1);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //wait for 1ms&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_OFF;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Set all pins of PORTA high&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_ON;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, SPI_SLAVE_ID);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, GPIOA_Exp);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, 0x05);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; OSA_TimeDelay(1);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //wait for 1ms&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_OFF;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while(1)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Set all pins of PORTA high&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_ON;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, SPI_SLAVE_ID);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, GPIOA_Exp);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, 0x05);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; OSA_TimeDelay(1);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //wait for 1ms&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Usr_SPI_OFF;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; OSA_TimeDelay(1000);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //wait for 1sec&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Set all pins of PORTA high&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Usr_SPI_ON;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, SPI_SLAVE_ID);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, GPIOA_Exp);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; SPI_HAL_WriteDataBlocking(spiBaseAddr, 0x00);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; OSA_TimeDelay(1);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //wait for 1ms&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Usr_SPI_OFF;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; OSA_TimeDelay(1000);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //wait for 1sec&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void wait_tcy(unsigned int wait)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; do&lt;/P&gt;&lt;P&gt;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp; ;&lt;/P&gt;&lt;P&gt;&amp;nbsp; }while(--wait!=0);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*******************************************************************************&lt;/P&gt;&lt;P&gt; * EOF&lt;/P&gt;&lt;P&gt; ******************************************************************************/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did try waiting for 100 time cycles instead of 1ms which according to the datasheet should be sufficient but doesn't work always,&lt;/P&gt;&lt;P&gt;This isn't the case in PIC18f&amp;nbsp; controllers wherein you could toggle the GPIO to disable SPI immediately. Am i missing something???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Nelson Lobo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 12:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Software-Development-Kit/FRDM-KL25Z-SPI-using-KSDK1-2-0-for-MCP23S17/m-p/392144#M1180</guid>
      <dc:creator>nelsonlobo</dc:creator>
      <dc:date>2015-09-22T12:20:06Z</dc:date>
    </item>
  </channel>
</rss>