<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: KV58 S19 file</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KV58-S19-file/m-p/931092#M9972</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks. It works...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jul 2019 18:07:03 GMT</pubDate>
    <dc:creator>a8Chcx</dc:creator>
    <dc:date>2019-07-17T18:07:03Z</dc:date>
    <item>
      <title>KV58 S19 file</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KV58-S19-file/m-p/931090#M9970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using "arm-none-eabi-objcopy --srec-len=64 --srec-forceS3 -O srec "aaa.elf"&amp;nbsp; "aaa.S19"" to generate S19 file.&lt;/P&gt;&lt;P&gt;The generated S19 as follows. At the end of file, it is not 64-bit alignment...&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;...............&lt;/P&gt;&lt;P&gt;S345100301C0000000000000000006D0CF43EBFD4C3E000000000000F03F000000000000F83F000000000000304300000000000030C34300000010000020F8B500BFF8BC08BC69&lt;BR /&gt;S315100302009E467047F8B500BFF8BC08BC9E467047BB&lt;BR /&gt;S30D100302104402FF7F0100000008&lt;BR /&gt;S30910030218250402108E&lt;BR /&gt;S3091003021C01040210AE&lt;BR /&gt;S34510030220000040010080000000093D00010000000000000000000000000000000000000000000000000000000000000000000000F001031000000000000000000000000079&lt;BR /&gt;S33D1003026000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000010000020000000001D&lt;BR /&gt;S705100204C91B&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because of 64-bit alignment required for KV58, I need to generate S19 file with 64-bit alignment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you tell me how to do it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2019 15:21:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KV58-S19-file/m-p/931090#M9970</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2019-07-17T15:21:35Z</dc:date>
    </item>
    <item>
      <title>Re: KV58 S19 file</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KV58-S19-file/m-p/931091#M9971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See &lt;A class="link-titled" href="https://mcuoneclipse.com/2015/09/23/aligning-s19-records-to-64-bit-boundaries/" title="https://mcuoneclipse.com/2015/09/23/aligning-s19-records-to-64-bit-boundaries/"&gt;Aligning S19 Records to 64-bit Boundaries | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2019 16:18:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KV58-S19-file/m-p/931091#M9971</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-07-17T16:18:49Z</dc:date>
    </item>
    <item>
      <title>Re: KV58 S19 file</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KV58-S19-file/m-p/931092#M9972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks. It works...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jul 2019 18:07:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KV58-S19-file/m-p/931092#M9972</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2019-07-17T18:07:03Z</dc:date>
    </item>
  </channel>
</rss>