<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: KDS Projects in Windows 7 transfer to Windows 10</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Projects-in-Windows-7-transfer-to-Windows-10/m-p/907768#M9949</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi MI,&lt;/P&gt;&lt;P&gt;1) yes, I don't see any reason why not. But I would recommend not to use KDS 3.0.0: the 3.2.0 version is the latest, so you better use that one (if not moving up to the MCUXpresso IDE).&lt;/P&gt;&lt;P&gt;2) yes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 May 2019 18:10:45 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2019-05-28T18:10:45Z</dc:date>
    <item>
      <title>KDS Projects in Windows 7 transfer to Windows 10</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Projects-in-Windows-7-transfer-to-Windows-10/m-p/907765#M9946</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a&amp;nbsp;firmware project that's based-on Kinetis MK22FX512&amp;nbsp;MCU which was developed in Kinetis Design Studio v3.0.0 using KSDK&amp;nbsp; v1.3.0, all under Windows 7.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I took over this project to upgrade and add new features in firmware to the product also in this environment in Windows 7.&amp;nbsp;&amp;nbsp;&amp;nbsp; There will be more modifications in the future to add few more&amp;nbsp;features.&amp;nbsp;&amp;nbsp;&amp;nbsp; All the project source and built files are on a server, and not in my PC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I will be starting on a new HW/FW project based-on Kinetis MKL28Z512VLL7 inside MCUXpresso usking the SDKs that I need to develop this product.&amp;nbsp;&amp;nbsp; Currently, I have been doing a lot of trial projects in MCUXpresso under Windows 7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our IT department will move all our&amp;nbsp;PC's to Windows 10 soon, in a month or so.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to start the new product's firmware in MCUXpresso under Windows 10, with all of GIT version control source management.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I still need to support and develop for the old FW in KDS IDE&amp;nbsp;that has been worked on in Windows 7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;QUESTIONS:&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; When IT upgrades my PC to Windows 10, will downloading and installing KDS v3.0.0 and KSDK v1.3.0 still work as is?&amp;nbsp; Or do I need to make special arrangements or other application installation to make them work in Windows 10 just as how it worked in Windows 7?&lt;/P&gt;&lt;P&gt;2.&amp;nbsp; When in Windows 10, will I still be able to import those KDS projects in KDS via "Import Projects" ---&amp;gt; "From Existing Projects" etc. without any issues, such that all existing MK22 firmware can be edited, upgraded and built just as how I have done it when everything was&amp;nbsp; in Windows 7?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MI&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 May 2019 18:46:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Projects-in-Windows-7-transfer-to-Windows-10/m-p/907765#M9946</guid>
      <dc:creator>mci</dc:creator>
      <dc:date>2019-05-24T18:46:13Z</dc:date>
    </item>
    <item>
      <title>Re: KDS Projects in Windows 7 transfer to Windows 10</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Projects-in-Windows-7-transfer-to-Windows-10/m-p/907766#M9947</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have migrated years ago from Win7 to Win10 and KDS without any issues.&lt;/P&gt;&lt;P&gt;The IDE and the projects make no assumptions about Win7 or Win10.&lt;/P&gt;&lt;P&gt;So:&lt;/P&gt;&lt;P&gt;1. It still works as in Win7&lt;/P&gt;&lt;P&gt;2. You simply create a new workspace and import the projects as usual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is only one reason why I keep a Win7 machine at hand (and it is not IDE releasted): to recover OpenSDA boards (see &lt;A class="link-titled" href="https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/" title="https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/"&gt;Bricking and Recovering OpenSDA Boards in Windows 8 and 10 | MCU on Eclipse&lt;/A&gt;). It is possible to configure Win10 not to brick the OpenSDA boards, but I have found it easier to have a Win7 machine at hand, just in case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 May 2019 05:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Projects-in-Windows-7-transfer-to-Windows-10/m-p/907766#M9947</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-05-25T05:25:35Z</dc:date>
    </item>
    <item>
      <title>Re: KDS Projects in Windows 7 transfer to Windows 10</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Projects-in-Windows-7-transfer-to-Windows-10/m-p/907767#M9948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response.&amp;nbsp; It is helpful &amp;amp; provides some relief.&amp;nbsp; The old product does not use OpenSDA interface; it is a custom board embedded product.&amp;nbsp;&amp;nbsp; (Now I just need to ask someplace else about Atmel &amp;amp; AVR Studio for a different old product which was built on XP &amp;amp; later Windows 7.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Follow-up questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Will older version of&amp;nbsp;KDS v3.0.0 &amp;amp; KSDK 1.3.0 still work on Windows 10?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) If not, can I import existing project to project in the latest version&amp;nbsp;KDS v3.2.0 &amp;amp; use KSDK 1.3.0 as well?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks so much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MI&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2019 14:42:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Projects-in-Windows-7-transfer-to-Windows-10/m-p/907767#M9948</guid>
      <dc:creator>mci</dc:creator>
      <dc:date>2019-05-28T14:42:47Z</dc:date>
    </item>
    <item>
      <title>Re: KDS Projects in Windows 7 transfer to Windows 10</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Projects-in-Windows-7-transfer-to-Windows-10/m-p/907768#M9949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi MI,&lt;/P&gt;&lt;P&gt;1) yes, I don't see any reason why not. But I would recommend not to use KDS 3.0.0: the 3.2.0 version is the latest, so you better use that one (if not moving up to the MCUXpresso IDE).&lt;/P&gt;&lt;P&gt;2) yes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2019 18:10:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Projects-in-Windows-7-transfer-to-Windows-10/m-p/907768#M9949</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-05-28T18:10:45Z</dc:date>
    </item>
    <item>
      <title>Re: KDS Projects in Windows 7 transfer to Windows 10</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Projects-in-Windows-7-transfer-to-Windows-10/m-p/907769#M9950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is anyone facing windows error after updating the windows 10? Actually, I am getting &lt;A href="https://errorcode0x.com/windows-update-error-80070103/"&gt;windows error 80070103&lt;/A&gt; after the windows update.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 07:45:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/KDS-Projects-in-Windows-7-transfer-to-Windows-10/m-p/907769#M9950</guid>
      <dc:creator>charliejonshon1</dc:creator>
      <dc:date>2019-06-11T07:45:10Z</dc:date>
    </item>
  </channel>
</rss>