<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: unique SDK path for the KDS 3.0   in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776265#M9767</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jennie, thanks for the update. Yes, in fact this is I'm doing right now. Modifying the path for every OS.&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;gatson&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Feb 2018 07:16:20 GMT</pubDate>
    <dc:creator>gschelotto</dc:creator>
    <dc:date>2018-02-12T07:16:20Z</dc:date>
    <item>
      <title>unique SDK path for the KDS 3.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776259#M9761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to set an unique SDK path in the project properties. The problem is I share the project with Windows/Linux developers. Under Linux I have to set the path as shown&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Screenshot from 2018-01-10 15-54-54.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38iEB231318A344F5E4/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2018-01-10 15-54-54.png" alt="Screenshot from 2018-01-10 15-54-54.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;while under Windows I have to set the C:/Freescale/KSDK_1.3.0 path.&lt;/P&gt;&lt;P&gt;How can I manage this drawback? I've tried to set a ${variable path} with no success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;gaston&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jan 2018 16:15:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776259#M9761</guid>
      <dc:creator>gschelotto</dc:creator>
      <dc:date>2018-01-10T16:15:41Z</dc:date>
    </item>
    <item>
      <title>Re: unique SDK path for the KDS 3.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776260#M9762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gaston.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We can use build variable in SDK path setting, for example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/7705i5C9030CC8C91DFCA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make sure KSDK_PATH is defined in Build Variables&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/7789i11164BA7367EB000/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just tested above on my side, the code run normally with these settings. &lt;/P&gt;&lt;P&gt;Please check if this can also work for you.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jan 2018 10:44:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776260#M9762</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2018-01-15T10:44:01Z</dc:date>
    </item>
    <item>
      <title>Re: unique SDK path for the KDS 3.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776261#M9763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is the KSDK_PATH defined in Build Variables is related to the project Properties. If the project of your example above&amp;nbsp; (with KSDK_PATH set as C:\Freescale\KSDK_1.3.0) is open in a Linux environment it wont work.&lt;/P&gt;&lt;P&gt;An idea is to set the SDK path in Window-&amp;gt;Preferences. But where? how?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;gaston&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 09:53:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776261#M9763</guid>
      <dc:creator>gschelotto</dc:creator>
      <dc:date>2018-01-17T09:53:45Z</dc:date>
    </item>
    <item>
      <title>Re: unique SDK path for the KDS 3.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776262#M9764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't think window preference can have same feature as you mentioned.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jan 2018 10:03:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776262#M9764</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2018-01-18T10:03:05Z</dc:date>
    </item>
    <item>
      <title>Re: unique SDK path for the KDS 3.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776263#M9765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jennie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case It wont be possible to open (without path conflicts) the same project on Windows/Linux indistinctly. Could you confirm there is no workaround to solve it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;gaston&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jan 2018 10:58:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776263#M9765</guid>
      <dc:creator>gschelotto</dc:creator>
      <dc:date>2018-01-18T10:58:17Z</dc:date>
    </item>
    <item>
      <title>Re: unique SDK path for the KDS 3.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776264#M9766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;gaston.&lt;/P&gt;&lt;P&gt;I don't think there is automated conversion option for it.&lt;/P&gt;&lt;P&gt;User needs to modify path setting after porting.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jennie Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Feb 2018 08:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776264#M9766</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2018-02-11T08:47:52Z</dc:date>
    </item>
    <item>
      <title>Re: unique SDK path for the KDS 3.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776265#M9767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jennie, thanks for the update. Yes, in fact this is I'm doing right now. Modifying the path for every OS.&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;gatson&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Feb 2018 07:16:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776265#M9767</guid>
      <dc:creator>gschelotto</dc:creator>
      <dc:date>2018-02-12T07:16:20Z</dc:date>
    </item>
    <item>
      <title>Re: unique SDK path for the KDS 3.0 </title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776266#M9768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are welcome!&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jennie.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Feb 2018 07:32:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/unique-SDK-path-for-the-KDS-3-0/m-p/776266#M9768</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2018-02-12T07:32:56Z</dc:date>
    </item>
  </channel>
</rss>