<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: How to use multiple I2C devices on the same bus with KE02 using Processor Expert?</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-to-use-multiple-I2C-devices-on-the-same-bus-with-KE02-using/m-p/764348#M9688</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, CI2Cx_SelectSlaveDevice() is used to select a different slave address.&lt;/P&gt;&lt;P&gt;Not sure why things are not working on your end, but have a look at the example code in the help for the component (&lt;A class="link-titled" href="https://mcuoneclipse.com/2012/11/12/getting-help-on-processor-expert-components/" title="https://mcuoneclipse.com/2012/11/12/getting-help-on-processor-expert-components/"&gt;Getting Help on Processor Expert Components | MCU on Eclipse&lt;/A&gt;&amp;nbsp;).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Nov 2017 21:07:56 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2017-11-09T21:07:56Z</dc:date>
    <item>
      <title>How to use multiple I2C devices on the same bus with KE02 using Processor Expert?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-to-use-multiple-I2C-devices-on-the-same-bus-with-KE02-using/m-p/764347#M9687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to use DS1307 and AT24c32 with the same I2C bus. I am using FRDM-KE02Z with Kinetis Design Studio. With KDS, there is only option of&amp;nbsp;specifying&amp;nbsp;only one I2C Slave Address.&amp;nbsp;How can I set another slave address for a second device?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have seen the method&amp;nbsp;CI2Cx_SelectSlaveDevice(), with which one can select another slave. But this does not seem to be working. I tried calling before CI2C_Init, MasterSendBlock and MasterReceiveBlock methods. Nothing seems to work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kindly advice on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Varma&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Nov 2017 13:20:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/How-to-use-multiple-I2C-devices-on-the-same-bus-with-KE02-using/m-p/764347#M9687</guid>
      <dc:creator>varma_s</dc:creator>
      <dc:date>2017-11-09T13:20:01Z</dc:date>
    </item>
    <item>
      <title>Re: How to use multiple I2C devices on the same bus with KE02 using Processor Expert?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-to-use-multiple-I2C-devices-on-the-same-bus-with-KE02-using/m-p/764348#M9688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, CI2Cx_SelectSlaveDevice() is used to select a different slave address.&lt;/P&gt;&lt;P&gt;Not sure why things are not working on your end, but have a look at the example code in the help for the component (&lt;A class="link-titled" href="https://mcuoneclipse.com/2012/11/12/getting-help-on-processor-expert-components/" title="https://mcuoneclipse.com/2012/11/12/getting-help-on-processor-expert-components/"&gt;Getting Help on Processor Expert Components | MCU on Eclipse&lt;/A&gt;&amp;nbsp;).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Nov 2017 21:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/How-to-use-multiple-I2C-devices-on-the-same-bus-with-KE02-using/m-p/764348#M9688</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-11-09T21:07:56Z</dc:date>
    </item>
  </channel>
</rss>