<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックFRDM-KL26Z - Freedom Development Board Debugging issue</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/FRDM-KL26Z-Freedom-Development-Board-Debugging-issue/m-p/761092#M9664</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Recently i bought a FRDM-KL26Z Freedom Development board. When i connected the board with mkl26z USB port with my pc, the drivers which required are installed. The RGB led ready to begin glow. RED BLUE etc at last it shows a combined color. The color will change with the motion of the board. Its works fine, and i tested the uart is working fine. Its display the value on my lap using teraterm. After that i updated the bootloader and firmware of the board,because i cant detect the port in KDS V3. Now KDS detect my board and port is also displayed. But the issue that the debugging is not completes. When i build the code (sampled code recommended in nxp - "hello world") no errors find and build complete. But when i debug it, the process stuck at about 75% completes. After that it doesnt moving what should i do? Is there is any issue with my over all work done? Or any issue with my KDS v3.&lt;/P&gt;&lt;P&gt;What is your suggestion? Any help will be appreciated.&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dileep&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 May 2018 14:23:24 GMT</pubDate>
    <dc:creator>dileeptn</dc:creator>
    <dc:date>2018-05-16T14:23:24Z</dc:date>
    <item>
      <title>FRDM-KL26Z - Freedom Development Board Debugging issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/FRDM-KL26Z-Freedom-Development-Board-Debugging-issue/m-p/761092#M9664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Recently i bought a FRDM-KL26Z Freedom Development board. When i connected the board with mkl26z USB port with my pc, the drivers which required are installed. The RGB led ready to begin glow. RED BLUE etc at last it shows a combined color. The color will change with the motion of the board. Its works fine, and i tested the uart is working fine. Its display the value on my lap using teraterm. After that i updated the bootloader and firmware of the board,because i cant detect the port in KDS V3. Now KDS detect my board and port is also displayed. But the issue that the debugging is not completes. When i build the code (sampled code recommended in nxp - "hello world") no errors find and build complete. But when i debug it, the process stuck at about 75% completes. After that it doesnt moving what should i do? Is there is any issue with my over all work done? Or any issue with my KDS v3.&lt;/P&gt;&lt;P&gt;What is your suggestion? Any help will be appreciated.&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dileep&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 May 2018 14:23:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/FRDM-KL26Z-Freedom-Development-Board-Debugging-issue/m-p/761092#M9664</guid>
      <dc:creator>dileeptn</dc:creator>
      <dc:date>2018-05-16T14:23:24Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL26Z - Freedom Development Board Debugging issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/FRDM-KL26Z-Freedom-Development-Board-Debugging-issue/m-p/761093#M9665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dileep ,&lt;/P&gt;&lt;P&gt;Please provde the below information:&lt;/P&gt;&lt;P&gt;- Which&amp;nbsp; bootloader and firmware you used ?&lt;/P&gt;&lt;P&gt;- What about your PC system ?&lt;/P&gt;&lt;P&gt;-Take a screesnshot about your Device manager&amp;nbsp; and Debug configuration of KDS when connect your board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 May 2018 02:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/FRDM-KL26Z-Freedom-Development-Board-Debugging-issue/m-p/761093#M9665</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-05-17T02:59:43Z</dc:date>
    </item>
  </channel>
</rss>