<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: fatal error: PE_low_level_init.h: No such file or directory</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743986#M9560</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I put the two pathes, and still can't work.&lt;/P&gt;&lt;P&gt;I fixed the first error, and now just the second error persist (make *** [Static_code...).&lt;/P&gt;&lt;P&gt;Code below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* ###################################################################&lt;BR /&gt;** Filename : main.c&lt;BR /&gt;** Project : testando&lt;BR /&gt;** Processor : MKL27Z64VLH4&lt;BR /&gt;** Version : Driver 01.01&lt;BR /&gt;** Compiler : GNU C Compiler&lt;BR /&gt;** Date/Time : 2018-03-11, 16:06, # CodeGen: 0&lt;BR /&gt;** Abstract :&lt;BR /&gt;** Main module.&lt;BR /&gt;** This module contains user's application code.&lt;BR /&gt;** Settings :&lt;BR /&gt;** Contents :&lt;BR /&gt;** No public methods&lt;BR /&gt;**&lt;BR /&gt;** ###################################################################*/&lt;BR /&gt;/*!&lt;BR /&gt;** @file main.c&lt;BR /&gt;** @version 01.01&lt;BR /&gt;** @brief&lt;BR /&gt;** Main module.&lt;BR /&gt;** This module contains user's application code.&lt;BR /&gt;*/ &lt;BR /&gt;/*!&lt;BR /&gt;** @addtogroup main_module main module documentation&lt;BR /&gt;** @{&lt;BR /&gt;*/ &lt;BR /&gt;/* MODULE main */&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/* Including needed modules to compile this module/procedure */&lt;BR /&gt;#include "Cpu.h"&lt;BR /&gt;#include "Events.h"&lt;BR /&gt;#include "clockMan1.h"&lt;BR /&gt;#include "pin_init.h"&lt;BR /&gt;#include "osa1.h"&lt;BR /&gt;#include "gpio1.h"&lt;BR /&gt;#if CPU_INIT_CONFIG&lt;BR /&gt; #include "Init_Config.h"&lt;BR /&gt;#endif&lt;BR /&gt;/* User includes (#include below this line is not maintained by Processor Expert) */&lt;/P&gt;&lt;P&gt;/*lint -save -e970 Disable MISRA rule (6.3) checking. */&lt;BR /&gt;int main(void)&lt;BR /&gt;/*lint -restore Enable MISRA rule (6.3) checking. */&lt;BR /&gt;{&lt;BR /&gt; /* Write your local variable definition here */&lt;/P&gt;&lt;P&gt;/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/&lt;BR /&gt; PE_low_level_init();&lt;BR /&gt; /*** End of Processor Expert internal initialization. ***/&lt;BR /&gt; int delay = 2000000;&lt;BR /&gt; /* Write your code here */&lt;BR /&gt; for(;;) {&lt;BR /&gt; GPIO_DRV_TogglePinOutput(LEDRGB_GREEN);&lt;BR /&gt; while(delay--);&lt;BR /&gt; delay = 2000000;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;/*** Don't write any code pass this line, or it will be deleted during code generation. ***/&lt;BR /&gt; /*** RTOS startup code. Macro PEX_RTOS_START is defined by the RTOS component. DON'T MODIFY THIS CODE!!! ***/&lt;BR /&gt; #ifdef PEX_RTOS_START&lt;BR /&gt; PEX_RTOS_START(); /* Startup of the selected RTOS. Macro is defined by the RTOS component. */&lt;BR /&gt; #endif&lt;BR /&gt; /*** End of RTOS startup code. ***/&lt;BR /&gt; /*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/&lt;BR /&gt; for(;;){}&lt;BR /&gt; /*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/&lt;BR /&gt;} /*** End of main routine. DO NOT MODIFY THIS TEXT!!! ***/&lt;/P&gt;&lt;P&gt;/* END main */&lt;BR /&gt;/*!&lt;BR /&gt;** @}&lt;BR /&gt;*/&lt;BR /&gt;/*&lt;BR /&gt;** ###################################################################&lt;BR /&gt;**&lt;BR /&gt;** This file was created by Processor Expert 10.5 [05.21]&lt;BR /&gt;** for the Freescale Kinetis series of microcontrollers.&lt;BR /&gt;**&lt;BR /&gt;** ###################################################################&lt;BR /&gt;*/&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Mar 2018 19:42:02 GMT</pubDate>
    <dc:creator>nícolasludwig</dc:creator>
    <dc:date>2018-03-12T19:42:02Z</dc:date>
    <item>
      <title>fatal error: PE_low_level_init.h: No such file or directory</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743984#M9558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone.&lt;/P&gt;&lt;P&gt;I'm having a problem (actually two) when&amp;nbsp;compiling my project. When I do it, I get this message that you can see on the image below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17131i331537450841DFD3/image-size/large?v=v2&amp;amp;px=999" title="error.png" alt="error.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The first error, the file exist, but it is in another path. I tried to put it in the "correct" path. The error disappear, but appears the same error with another file. I also tried to look the includes of the compiler in Properties -&amp;gt; C/C++ Build -&amp;gt; Settings, and I guess that all the paths are there. And I ALSO tried to put ALL the .h files into ".../Static_Code/System", as the error says. But the problem persist.&lt;/P&gt;&lt;P&gt;The second error, I just don't know what to do.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you help me?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Mar 2018 00:44:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743984#M9558</guid>
      <dc:creator>nícolasludwig</dc:creator>
      <dc:date>2018-03-11T00:44:20Z</dc:date>
    </item>
    <item>
      <title>Re: fatal error: PE_low_level_init.h: No such file or directory</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743985#M9559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="314952" data-username="nícolasludwig" href="https://community.nxp.com/people/nícolasludwig"&gt;Nícolas Ludwig&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;Please check the two pathes as below :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17897iA038C1B8E9F9FB79/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If still can't work, you can send it to my , I will check it on my side .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Mar 2018 03:15:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743985#M9559</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-03-12T03:15:33Z</dc:date>
    </item>
    <item>
      <title>Re: fatal error: PE_low_level_init.h: No such file or directory</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743986#M9560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I put the two pathes, and still can't work.&lt;/P&gt;&lt;P&gt;I fixed the first error, and now just the second error persist (make *** [Static_code...).&lt;/P&gt;&lt;P&gt;Code below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* ###################################################################&lt;BR /&gt;** Filename : main.c&lt;BR /&gt;** Project : testando&lt;BR /&gt;** Processor : MKL27Z64VLH4&lt;BR /&gt;** Version : Driver 01.01&lt;BR /&gt;** Compiler : GNU C Compiler&lt;BR /&gt;** Date/Time : 2018-03-11, 16:06, # CodeGen: 0&lt;BR /&gt;** Abstract :&lt;BR /&gt;** Main module.&lt;BR /&gt;** This module contains user's application code.&lt;BR /&gt;** Settings :&lt;BR /&gt;** Contents :&lt;BR /&gt;** No public methods&lt;BR /&gt;**&lt;BR /&gt;** ###################################################################*/&lt;BR /&gt;/*!&lt;BR /&gt;** @file main.c&lt;BR /&gt;** @version 01.01&lt;BR /&gt;** @brief&lt;BR /&gt;** Main module.&lt;BR /&gt;** This module contains user's application code.&lt;BR /&gt;*/ &lt;BR /&gt;/*!&lt;BR /&gt;** @addtogroup main_module main module documentation&lt;BR /&gt;** @{&lt;BR /&gt;*/ &lt;BR /&gt;/* MODULE main */&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/* Including needed modules to compile this module/procedure */&lt;BR /&gt;#include "Cpu.h"&lt;BR /&gt;#include "Events.h"&lt;BR /&gt;#include "clockMan1.h"&lt;BR /&gt;#include "pin_init.h"&lt;BR /&gt;#include "osa1.h"&lt;BR /&gt;#include "gpio1.h"&lt;BR /&gt;#if CPU_INIT_CONFIG&lt;BR /&gt; #include "Init_Config.h"&lt;BR /&gt;#endif&lt;BR /&gt;/* User includes (#include below this line is not maintained by Processor Expert) */&lt;/P&gt;&lt;P&gt;/*lint -save -e970 Disable MISRA rule (6.3) checking. */&lt;BR /&gt;int main(void)&lt;BR /&gt;/*lint -restore Enable MISRA rule (6.3) checking. */&lt;BR /&gt;{&lt;BR /&gt; /* Write your local variable definition here */&lt;/P&gt;&lt;P&gt;/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/&lt;BR /&gt; PE_low_level_init();&lt;BR /&gt; /*** End of Processor Expert internal initialization. ***/&lt;BR /&gt; int delay = 2000000;&lt;BR /&gt; /* Write your code here */&lt;BR /&gt; for(;;) {&lt;BR /&gt; GPIO_DRV_TogglePinOutput(LEDRGB_GREEN);&lt;BR /&gt; while(delay--);&lt;BR /&gt; delay = 2000000;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;/*** Don't write any code pass this line, or it will be deleted during code generation. ***/&lt;BR /&gt; /*** RTOS startup code. Macro PEX_RTOS_START is defined by the RTOS component. DON'T MODIFY THIS CODE!!! ***/&lt;BR /&gt; #ifdef PEX_RTOS_START&lt;BR /&gt; PEX_RTOS_START(); /* Startup of the selected RTOS. Macro is defined by the RTOS component. */&lt;BR /&gt; #endif&lt;BR /&gt; /*** End of RTOS startup code. ***/&lt;BR /&gt; /*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/&lt;BR /&gt; for(;;){}&lt;BR /&gt; /*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/&lt;BR /&gt;} /*** End of main routine. DO NOT MODIFY THIS TEXT!!! ***/&lt;/P&gt;&lt;P&gt;/* END main */&lt;BR /&gt;/*!&lt;BR /&gt;** @}&lt;BR /&gt;*/&lt;BR /&gt;/*&lt;BR /&gt;** ###################################################################&lt;BR /&gt;**&lt;BR /&gt;** This file was created by Processor Expert 10.5 [05.21]&lt;BR /&gt;** for the Freescale Kinetis series of microcontrollers.&lt;BR /&gt;**&lt;BR /&gt;** ###################################################################&lt;BR /&gt;*/&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Mar 2018 19:42:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743986#M9560</guid>
      <dc:creator>nícolasludwig</dc:creator>
      <dc:date>2018-03-12T19:42:02Z</dc:date>
    </item>
    <item>
      <title>Re: fatal error: PE_low_level_init.h: No such file or directory</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743987#M9561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="314952" data-username="nícolasludwig" href="https://community.nxp.com/people/nícolasludwig"&gt;Nícolas Ludwig&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Please send your project to me.&lt;/P&gt;&lt;P&gt;And what about your IDE version?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Mar 2018 09:21:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743987#M9561</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-03-14T09:21:38Z</dc:date>
    </item>
    <item>
      <title>Re: fatal error: PE_low_level_init.h: No such file or directory</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743988#M9562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello. I posted my project on Google Drive. It's a .rar file, link below:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://drive.google.com/file/d/19F4TzGJaRr_PkF4EPM4g73ahlMHJium_/view?usp=sharing" title="https://drive.google.com/file/d/19F4TzGJaRr_PkF4EPM4g73ahlMHJium_/view?usp=sharing"&gt;testando.rar - Google Drive&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My IDE version is 3.0.0. Yesterday I tried with 3.2.0 version, but without success.&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Mar 2018 15:36:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743988#M9562</guid>
      <dc:creator>nícolasludwig</dc:creator>
      <dc:date>2018-03-14T15:36:26Z</dc:date>
    </item>
    <item>
      <title>Re: fatal error: PE_low_level_init.h: No such file or directory</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743989#M9563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I build your project on my side, there is no error :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/35751i1CEFC5C5384EF339/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Mar 2018 09:45:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743989#M9563</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-03-20T09:45:24Z</dc:date>
    </item>
    <item>
      <title>Re: fatal error: PE_low_level_init.h: No such file or directory</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743990#M9564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;Yes. As I said, I build this project in another computer and it works. Just in mine computer it doesn't. Do you have any idea to fix it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Mar 2018 12:08:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743990#M9564</guid>
      <dc:creator>nícolasludwig</dc:creator>
      <dc:date>2018-03-20T12:08:34Z</dc:date>
    </item>
    <item>
      <title>Re: fatal error: PE_low_level_init.h: No such file or directory</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743991#M9565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please take a screenshot about your error on Console window.&lt;/P&gt;&lt;P&gt;Also your project is based on KSDKv1.3, have you isntall it on KDS ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2018 04:14:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743991#M9565</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-03-21T04:14:52Z</dc:date>
    </item>
    <item>
      <title>Re: fatal error: PE_low_level_init.h: No such file or directory</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743992#M9566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/nícolasludwig"&gt;nícolasludwig&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was having the same issue and I solve it changing the Project Location. It seems that KIDS can't handle some characters ("ñ" in my case). To be sure I also use a really short route.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Have a great day.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nicolás.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Oct 2018 15:10:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743992#M9566</guid>
      <dc:creator>niconico</dc:creator>
      <dc:date>2018-10-10T15:10:11Z</dc:date>
    </item>
    <item>
      <title>Re: fatal error: PE_low_level_init.h: No such file or directory</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743993#M9567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Nico.&lt;/P&gt;&lt;P&gt;Sorry for delay. I didn't try it yet but, just to be sure, where did you put your new Project Location?&lt;/P&gt;&lt;P&gt;And the characters you mean, are those of the project name, right? Or those inside the code too?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2019 12:55:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/fatal-error-PE-low-level-init-h-No-such-file-or-directory/m-p/743993#M9567</guid>
      <dc:creator>nícolasludwig</dc:creator>
      <dc:date>2019-05-15T12:55:55Z</dc:date>
    </item>
  </channel>
</rss>