<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Is it possible to run / debug without re-flashing?</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-it-possible-to-run-debug-without-re-flashing/m-p/737244#M9486</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have loaded an image into my KL27Z via the bootloader (not via JTAG / J-Link).&amp;nbsp; I'd like to run &amp;amp; step&amp;nbsp;the program using the debugger, but explicitly&amp;nbsp;&lt;STRONG&gt;don't&lt;/STRONG&gt; want to re-flash the image[*].&amp;nbsp; Is this possible with KDS_v3?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[*] The image I'm running is identical to the built image with the exception of the Bootloader Configuration Area, and I don't want to overwrite that.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Nov 2017 11:52:12 GMT</pubDate>
    <dc:creator>robertpoor</dc:creator>
    <dc:date>2017-11-01T11:52:12Z</dc:date>
    <item>
      <title>Is it possible to run / debug without re-flashing?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-it-possible-to-run-debug-without-re-flashing/m-p/737244#M9486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have loaded an image into my KL27Z via the bootloader (not via JTAG / J-Link).&amp;nbsp; I'd like to run &amp;amp; step&amp;nbsp;the program using the debugger, but explicitly&amp;nbsp;&lt;STRONG&gt;don't&lt;/STRONG&gt; want to re-flash the image[*].&amp;nbsp; Is this possible with KDS_v3?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[*] The image I'm running is identical to the built image with the exception of the Bootloader Configuration Area, and I don't want to overwrite that.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Nov 2017 11:52:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-it-possible-to-run-debug-without-re-flashing/m-p/737244#M9486</guid>
      <dc:creator>robertpoor</dc:creator>
      <dc:date>2017-11-01T11:52:12Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to run / debug without re-flashing?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-it-possible-to-run-debug-without-re-flashing/m-p/737245#M9487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robert,&lt;/P&gt;&lt;P&gt;Yes, see &lt;A class="link-titled" href="https://mcuoneclipse.com/2015/03/20/attaching-to-a-running-target-with-segger-j-link-gdb-and-eclipse/" title="https://mcuoneclipse.com/2015/03/20/attaching-to-a-running-target-with-segger-j-link-gdb-and-eclipse/"&gt;Attaching to a Running Target with Segger J-Link, GDB and Eclipse | MCU on Eclipse&lt;/A&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;It depends to some extend to the debug interface used. But basically disable download to flash and specify the symbol/debug file only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Nov 2017 17:46:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Is-it-possible-to-run-debug-without-re-flashing/m-p/737245#M9487</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-11-01T17:46:50Z</dc:date>
    </item>
  </channel>
</rss>