<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re:  internal compiler error: Segmentation fault</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731338#M9442</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried on another project and got the same result...&lt;/P&gt;&lt;P&gt;More likely, it is related to "-flto" optimization on gcc 4.8.4 because of the following error message :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;" lto-wrapper: arm-none-eabi-g++ returned 1 exit status&lt;/P&gt;&lt;P&gt;c:/fsl32/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/bin/ld.exe: lto-wrapper failed"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you confirm it and give me some workaround?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 May 2018 16:21:53 GMT</pubDate>
    <dc:creator>a8Chcx</dc:creator>
    <dc:date>2018-05-09T16:21:53Z</dc:date>
    <item>
      <title>internal compiler error: Segmentation fault</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731334#M9438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using KDS3.2 and KSDK 2.0 for K66F. The project works fine when I do not do optimization.&lt;/P&gt;&lt;P&gt;When I do -O3 optimization, I got "&amp;nbsp;internal compiler error: Segmentation fault"(See below)&amp;nbsp;when do linker...&lt;/P&gt;&lt;P&gt;Looks like there is the problem for optimization.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I anyone tell me how to fix the problem when I am using -O3 optimization?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;09:39:04 **** Incremental Build of configuration Release for project iNetVu7710_V50_FW ****&lt;/P&gt;&lt;P&gt;make -j8 all&lt;/P&gt;&lt;P&gt;Building file: ../middleware/lwip_2.0.0/src/netif/ethernet.c&lt;/P&gt;&lt;P&gt;Invoking: Cross ARM C Compiler&lt;/P&gt;&lt;P&gt;.......&lt;/P&gt;&lt;P&gt;-I../source/opentcp_inetvu/hns_client_iNetVu -I../source/opentcp_inetvu/iDirect_telnet_com -std=c99 -MMD -MP -MF"middleware/lwip_2.0.0/src/netif/ethernet.d" -MT"middleware/lwip_2.0.0/src/netif/ethernet.o" -c -o "middleware/lwip_2.0.0/src/netif/ethernet.o" "../middleware/lwip_2.0.0/src/netif/ethernet.c"&lt;/P&gt;&lt;P&gt;Finished building: ../middleware/lwip_2.0.0/src/netif/ethernet.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Building target: iNetVu7710_V50_FW.elf&lt;/P&gt;&lt;P&gt;Invoking: Cross ARM C++ Linker&lt;/P&gt;&lt;P&gt;arm-none-eabi-g++ -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O3 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -flto -g -T "../MK66FN2M0xxx18_flash.ld" -Xlinker --gc-sections -Wl,-Map,"iNetVu7710_V50_FW.map" --specs=nano.specs -specs=nosys.specs -Xlinker -z -Xlinker muldefs -o "iNetVu7710_V50_FW.elf" ./utilities/fsl_debug_console.o ./utilities/fsl_notifier.o ./utilities/fsl_sbrk.o ./utilities/fsl_shell.o ./startup/startup_MK66F18.o ./startup/system_MK66F18.o ./source/opentcp_inetvu/iDirect_telnet_com/iDirect_telnet_com.o ./source/opentcp_inetvu/http_server_iNetVu/http_srv_iNetVu.o ./source/opentcp_inetvu/hns_client_iNetVu/hns_client_iNetVu_modem.o ./source/dev_iNetVu/flash_utility/CFM_flash_inetvu.o ./source/dev_iNetVu/flash_utility/amd_flash_inetvu.o ./source/dev_iNetVu/USB_iNetVu/USB_inetvu.o ./source/dev_iNetVu/UART_iNetVu/UART_inetvu.o ./source/dev_iNetVu/PIT_iNetVu/timers_inetvu.o ./source/dev_iNetVu/LCD_iNetVu/LCD_inetvu.o ./source/dev_iNetVu/IIC_iNetVu/LLA_STiD135_v1.3.5_06082017/util/stfe_utilities.o ./source/dev_iNetVu/IIC_iNetVu/LLA_STiD135_v1.3.5_06082017/stid135_drv/stid135_drv.o ./source/dev_iNetVu/IIC_iNetVu/LLA_STiD135_v1.3.5_06082017/stid135_drv/stid135_init.o ./source/dev_iNetVu/IIC_iNetVu/LLA_STiD135_v1.3.5_06082017/lnb/lnb_drv.o ./source/dev_iNetVu/IIC_iNetVu/LLA_STiD135_v1.3.5_06082017/lnb/lnbh26_init.o ./source/dev_iNetVu/IIC_iNetVu/LLA_STiD135_v1.3.5_06082017/chip/chip.o ./source/dev_iNetVu/IIC_iNetVu/LLA_STiD135_v1.3.5_06082017/anafe/oxford_anafe_func.o ./source/dev_iNetVu/IIC_iNetVu/IIC_inetvu.o ./source/dev_iNetVu/Flexcan_iNetVu/flexcan_inetvu.o ./source/common/driver_systick.o ./source/common/opentcp.o ./source/fsl_phy.o ./source/hid_generic.o ./source/usb_device_ch9.o ./source/usb_device_class.o ./source/usb_device_descriptor.o ./source/usb_device_hid.o ./middleware/usb_1.6.3/phy/usb_phy.o ./middleware/usb_1.6.3/osa/usb_osa_bm.o ./middleware/usb_1.6.3/device/usb_device_dci.o ./middleware/usb_1.6.3/device/usb_device_ehci.o ./middleware/usb_1.6.3/device/usb_device_khci.o ./middleware/lwip_2.0.0/src/netif/ppp/auth.o ./middleware/lwip_2.0.0/src/netif/ppp/ccp.o ./middleware/lwip_2.0.0/src/netif/ppp/chap-md5.o ./middleware/lwip_2.0.0/src/netif/ppp/chap-new.o ./middleware/lwip_2.0.0/src/netif/ppp/chap_ms.o ./middleware/lwip_2.0.0/src/netif/ppp/demand.o ./middleware/lwip_2.0.0/src/netif/ppp/eap.o ./middleware/lwip_2.0.0/src/netif/ppp/eui64.o ./middleware/lwip_2.0.0/src/netif/ppp/fsm.o ./middleware/lwip_2.0.0/src/netif/ppp/ipcp.o ./middleware/lwip_2.0.0/src/netif/ppp/ipv6cp.o ./middleware/lwip_2.0.0/src/netif/ppp/lcp.o ./middleware/lwip_2.0.0/src/netif/ppp/lwip_ecp.o ./middleware/lwip_2.0.0/src/netif/ppp/magic.o ./middleware/lwip_2.0.0/src/netif/ppp/mppe.o ./middleware/lwip_2.0.0/src/netif/ppp/multilink.o ./middleware/lwip_2.0.0/src/netif/ppp/ppp.o ./middleware/lwip_2.0.0/src/netif/ppp/pppapi.o ./middleware/lwip_2.0.0/src/netif/ppp/pppcrypt.o ./middleware/lwip_2.0.0/src/netif/ppp/pppoe.o ./middleware/lwip_2.0.0/src/netif/ppp/pppol2tp.o ./middleware/lwip_2.0.0/src/netif/ppp/pppos.o ./middleware/lwip_2.0.0/src/netif/ppp/upap.o ./middleware/lwip_2.0.0/src/netif/ppp/utils.o ./middleware/lwip_2.0.0/src/netif/ppp/vj.o ./middleware/lwip_2.0.0/src/netif/ethernet.o ./middleware/lwip_2.0.0/src/netif/ethernetif.o ./middleware/lwip_2.0.0/src/netif/lowpan6.o ./middleware/lwip_2.0.0/src/netif/slipif.o ./middleware/lwip_2.0.0/src/core/ipv6/dhcp6.o ./middleware/lwip_2.0.0/src/core/ipv6/ethip6.o ./middleware/lwip_2.0.0/src/core/ipv6/icmp6.o ./middleware/lwip_2.0.0/src/core/ipv6/inet6.o ./middleware/lwip_2.0.0/src/core/ipv6/ip6.o ./middleware/lwip_2.0.0/src/core/ipv6/ip6_addr.o ./middleware/lwip_2.0.0/src/core/ipv6/ip6_frag.o ./middleware/lwip_2.0.0/src/core/ipv6/mld6.o ./middleware/lwip_2.0.0/src/core/ipv6/nd6.o ./middleware/lwip_2.0.0/src/core/ipv4/autoip.o ./middleware/lwip_2.0.0/src/core/ipv4/dhcp.o ./middleware/lwip_2.0.0/src/core/ipv4/etharp.o ./middleware/lwip_2.0.0/src/core/ipv4/icmp.o ./middleware/lwip_2.0.0/src/core/ipv4/igmp.o ./middleware/lwip_2.0.0/src/core/ipv4/ip4.o ./middleware/lwip_2.0.0/src/core/ipv4/ip4_addr.o ./middleware/lwip_2.0.0/src/core/ipv4/ip4_frag.o ./middleware/lwip_2.0.0/src/core/def.o ./middleware/lwip_2.0.0/src/core/dns.o ./middleware/lwip_2.0.0/src/core/inet_chksum.o ./middleware/lwip_2.0.0/src/core/init.o ./middleware/lwip_2.0.0/src/core/ip.o ./middleware/lwip_2.0.0/src/core/mem.o ./middleware/lwip_2.0.0/src/core/memp.o ./middleware/lwip_2.0.0/src/core/netif.o ./middleware/lwip_2.0.0/src/core/pbuf.o ./middleware/lwip_2.0.0/src/core/raw.o ./middleware/lwip_2.0.0/src/core/stats.o ./middleware/lwip_2.0.0/src/core/sys.o ./middleware/lwip_2.0.0/src/core/tcp.o ./middleware/lwip_2.0.0/src/core/tcp_in.o ./middleware/lwip_2.0.0/src/core/tcp_out.o ./middleware/lwip_2.0.0/src/core/timeouts.o ./middleware/lwip_2.0.0/src/core/udp.o ./middleware/lwip_2.0.0/src/apps/sntp/sntp.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_asn1.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_core.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_mib2.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_mib2_icmp.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_mib2_interfaces.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_mib2_ip.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_mib2_snmp.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_mib2_system.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_mib2_tcp.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_mib2_udp.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_msg.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_netconn.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_pbuf_stream.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_raw.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_scalar.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_table.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_threadsync.o ./middleware/lwip_2.0.0/src/apps/snmp/snmp_traps.o ./middleware/lwip_2.0.0/src/apps/snmp/snmpv3.o ./middleware/lwip_2.0.0/src/apps/snmp/snmpv3_dummy.o ./middleware/lwip_2.0.0/src/apps/snmp/snmpv3_mbedtls.o ./middleware/lwip_2.0.0/src/apps/netbiosns/netbiosns.o ./middleware/lwip_2.0.0/src/apps/lwiperf/lwiperf.o ./middleware/lwip_2.0.0/src/apps/httpd/fs.o ./middleware/lwip_2.0.0/src/apps/httpd/fsdata.o ./middleware/lwip_2.0.0/src/apps/httpd/httpd.o ./middleware/lwip_2.0.0/src/api/api_lib.o ./middleware/lwip_2.0.0/src/api/api_msg.o ./middleware/lwip_2.0.0/src/api/err.o ./middleware/lwip_2.0.0/src/api/netbuf.o ./middleware/lwip_2.0.0/src/api/netdb.o ./middleware/lwip_2.0.0/src/api/netifapi.o ./middleware/lwip_2.0.0/src/api/sockets.o ./middleware/lwip_2.0.0/src/api/tcpip.o ./middleware/lwip_2.0.0/port/ethernetif.o ./middleware/lwip_2.0.0/port/sys_arch.o ./middleware/lwip_2.0.0/contrib/apps/udpecho_raw/udp_client_iNetVu_track.o ./middleware/lwip_2.0.0/contrib/apps/udpecho_raw/udp_server_iNetVu_app.o ./middleware/lwip_2.0.0/contrib/apps/udpecho_raw/udpecho_client_raw.o ./middleware/lwip_2.0.0/contrib/apps/udpecho_raw/udpecho_raw.o ./middleware/lwip_2.0.0/contrib/apps/udpecho/udpecho.o ./middleware/lwip_2.0.0/contrib/apps/tcpecho_raw/tcp_client_HNS.o ./middleware/lwip_2.0.0/contrib/apps/tcpecho_raw/tcpecho_client_raw.o ./middleware/lwip_2.0.0/contrib/apps/tcpecho_raw/tcpecho_raw.o ./middleware/lwip_2.0.0/contrib/apps/tcpecho/tcpecho.o ./middleware/lwip_2.0.0/contrib/apps/socket_examples/socket_examples.o ./middleware/lwip_2.0.0/contrib/apps/snmp_private_mib/lwip_prvmib.o ./middleware/lwip_2.0.0/contrib/apps/smtp/smtp.o ./middleware/lwip_2.0.0/contrib/apps/shell/shell.o ./middleware/lwip_2.0.0/contrib/apps/rtp/rtp.o ./middleware/lwip_2.0.0/contrib/apps/ping/ping.o ./middleware/lwip_2.0.0/contrib/apps/netio/netio.o ./middleware/lwip_2.0.0/contrib/apps/httpserver/httpserver-netconn.o ./middleware/lwip_2.0.0/contrib/apps/chargen/chargen.o ./drivers/fsl_adc16.o ./drivers/fsl_clock.o ./drivers/fsl_cmp.o ./drivers/fsl_cmt.o ./drivers/fsl_common.o ./drivers/fsl_crc.o ./drivers/fsl_dac.o ./drivers/fsl_dmamux.o ./drivers/fsl_dspi.o ./drivers/fsl_dspi_edma.o ./drivers/fsl_edma.o ./drivers/fsl_enet.o ./drivers/fsl_ewm.o ./drivers/fsl_flash.o ./drivers/fsl_flexbus.o ./drivers/fsl_flexcan.o ./drivers/fsl_ftm.o ./drivers/fsl_gpio.o ./drivers/fsl_i2c.o ./drivers/fsl_i2c_edma.o ./drivers/fsl_llwu.o ./drivers/fsl_lmem_cache.o ./drivers/fsl_lptmr.o ./drivers/fsl_lpuart.o ./drivers/fsl_lpuart_edma.o ./drivers/fsl_mpu.o ./drivers/fsl_pdb.o ./drivers/fsl_pit.o ./drivers/fsl_pmc.o ./drivers/fsl_rcm.o ./drivers/fsl_rnga.o ./drivers/fsl_rtc.o ./drivers/fsl_sai.o ./drivers/fsl_sai_edma.o ./drivers/fsl_sdhc.o ./drivers/fsl_sdramc.o ./drivers/fsl_sim.o ./drivers/fsl_smc.o ./drivers/fsl_tpm.o ./drivers/fsl_tsi_v4.o ./drivers/fsl_uart.o ./drivers/fsl_uart_edma.o ./drivers/fsl_vref.o ./drivers/fsl_wdog.o ./board/board.o ./board/clock_config.o ./board/fsl_sdram.o ./board/pin_mux.o ./.metadata/.plugins/org.eclipse.cdt.make.core/specs.o&lt;/P&gt;&lt;P&gt;../middleware/lwip_2.0.0/src/netif/ethernet.c: In function 'ethernet_input':&lt;/P&gt;&lt;P&gt;../middleware/lwip_2.0.0/src/netif/ethernet.c:69:7: internal compiler error: Segmentation fault&lt;/P&gt;&lt;P&gt;err_t ethernet_input(struct pbuf *p, struct netif *netif)&lt;/P&gt;&lt;P&gt;^&lt;/P&gt;&lt;P&gt;Please submit a full bug report,&lt;/P&gt;&lt;P&gt;with preprocessed source if appropriate.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;See &amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fgcc.gnu.org%2Fbugs.html" rel="nofollow" target="_blank"&gt;http://gcc.gnu.org/bugs.html&lt;/A&gt;&lt;SPAN&gt;&amp;gt; for instructions.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;lto-wrapper: arm-none-eabi-g++ returned 1 exit status&lt;/P&gt;&lt;P&gt;c:/fsl32/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/bin/ld.exe: lto-wrapper failed&lt;/P&gt;&lt;P&gt;collect2.exe: error: ld returned 1 exit status&lt;/P&gt;&lt;P&gt;makefile:106: recipe for target 'iNetVu7710_V50_FW.elf' failed&lt;/P&gt;&lt;P&gt;make: *** [iNetVu7710_V50_FW.elf] Error 1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 May 2018 13:48:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731334#M9438</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2018-05-07T13:48:09Z</dc:date>
    </item>
    <item>
      <title>Re:  internal compiler error: Segmentation fault</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731335#M9439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried on http server sample project and did the same thing. I can't use -O3 optimization....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 May 2018 15:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731335#M9439</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2018-05-07T15:02:36Z</dc:date>
    </item>
    <item>
      <title>Re:  internal compiler error: Segmentation fault</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731336#M9440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Christie,&lt;/P&gt;&lt;P&gt;Could you please use the latest KSDKv2.3 ？&lt;/P&gt;&lt;P&gt;I&amp;nbsp; test the the demo "lwip_httpsrv_bm_frdmk66f" of SDKv2.3, set Optimization Level to -o3,&lt;/P&gt;&lt;P&gt;there is no error with build :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/28818iDF4CC6E8AE3DEA6B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 May 2018 09:41:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731336#M9440</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-05-08T09:41:34Z</dc:date>
    </item>
    <item>
      <title>Re:  internal compiler error: Segmentation fault</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731337#M9441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can build&amp;nbsp;my project if I uncheck "-flto" with -O3 and works fine.&lt;/P&gt;&lt;P&gt;When I build my project if I check "-flto" with Os, compiling and linking are fine, but can't run properly. Without "-flto", it works fine as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to know if I have to uncheck "-flto" because it is checked as default? Any reason?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 May 2018 12:11:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731337#M9441</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2018-05-08T12:11:34Z</dc:date>
    </item>
    <item>
      <title>Re:  internal compiler error: Segmentation fault</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731338#M9442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried on another project and got the same result...&lt;/P&gt;&lt;P&gt;More likely, it is related to "-flto" optimization on gcc 4.8.4 because of the following error message :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;" lto-wrapper: arm-none-eabi-g++ returned 1 exit status&lt;/P&gt;&lt;P&gt;c:/fsl32/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/bin/ld.exe: lto-wrapper failed"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you confirm it and give me some workaround?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 May 2018 16:21:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731338#M9442</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2018-05-09T16:21:53Z</dc:date>
    </item>
    <item>
      <title>Re:  internal compiler error: Segmentation fault</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731339#M9443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Christie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems the&amp;nbsp; ethernet_input(struct pbuf *p,&amp;nbsp;&amp;nbsp; struct netif *netif) is opitimized ,&lt;/P&gt;&lt;P&gt;while I havn't find workaround, I will report it to development team.&lt;/P&gt;&lt;P&gt;Sorry for the inconvenient to you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 May 2018 08:13:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731339#M9443</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-05-10T08:13:36Z</dc:date>
    </item>
    <item>
      <title>Re:  internal compiler error: Segmentation fault</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731340#M9444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know what is the solution on this finally?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thx,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 May 2018 12:24:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731340#M9444</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2018-05-10T12:24:45Z</dc:date>
    </item>
    <item>
      <title>Re:  internal compiler error: Segmentation fault</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731341#M9445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Christie,&lt;/P&gt;&lt;P&gt;This case is still in progress statues . I recommend you&amp;nbsp; uncheck "-flto"as a workaround .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jun 2018 08:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/internal-compiler-error-Segmentation-fault/m-p/731341#M9445</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-06-20T08:20:06Z</dc:date>
    </item>
  </channel>
</rss>