<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 How can I use the external interrupt of board KL27Z?</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-use-the-external-interrupt-of-board-KL27Z/m-p/713799#M9323</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Someone could help me? I'm working with the board KL27Z and I've just used digital input and output, but now I want to use external interrupt. Unfortunately, I don't know how to configure and write the programming, for example, which lines or library I've to add in my project.&lt;BR /&gt;For now, I'm just trying to turn it on or off a LED when I push the putton, without use just digital input (that we need to wait to be read the lines in "main" fuction to read the action).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Just one more thing,&amp;nbsp;someone have something (books, links, blogs) to study and improve my knowledge with KL27Z? At now, I'm trying to discover by me (debugging and compiling) and sometimes I'm here to ask help (like now, haha).&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Sep 2017 17:56:26 GMT</pubDate>
    <dc:creator>tiagobmarinho</dc:creator>
    <dc:date>2017-09-25T17:56:26Z</dc:date>
    <item>
      <title>How can I use the external interrupt of board KL27Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-use-the-external-interrupt-of-board-KL27Z/m-p/713799#M9323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Someone could help me? I'm working with the board KL27Z and I've just used digital input and output, but now I want to use external interrupt. Unfortunately, I don't know how to configure and write the programming, for example, which lines or library I've to add in my project.&lt;BR /&gt;For now, I'm just trying to turn it on or off a LED when I push the putton, without use just digital input (that we need to wait to be read the lines in "main" fuction to read the action).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Just one more thing,&amp;nbsp;someone have something (books, links, blogs) to study and improve my knowledge with KL27Z? At now, I'm trying to discover by me (debugging and compiling) and sometimes I'm here to ask help (like now, haha).&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Sep 2017 17:56:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-use-the-external-interrupt-of-board-KL27Z/m-p/713799#M9323</guid>
      <dc:creator>tiagobmarinho</dc:creator>
      <dc:date>2017-09-25T17:56:26Z</dc:date>
    </item>
    <item>
      <title>Re: How can I use the external interrupt of board KL27Z?</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-use-the-external-interrupt-of-board-KL27Z/m-p/713800#M9324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tiago,&lt;/P&gt;&lt;P&gt;I recommend you first view some demo code to learn , for example , the MCUXpresso SDK , it includes&lt;/P&gt;&lt;P&gt;all the basic demos. Please refer to this tutorial to download :&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-333304"&gt;Generating a downloadable MCUXpresso SDK v.2 package&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It supports the below IDEs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31840i92168A5A35D251CE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then refer to "Getting Started with MCUXpresso SDK.pdf" to open it on your IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2017 02:39:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/How-can-I-use-the-external-interrupt-of-board-KL27Z/m-p/713800#M9324</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-09-26T02:39:20Z</dc:date>
    </item>
  </channel>
</rss>