<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 MKV30 using PE components w/out KSDK</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/MKV30-using-PE-components-w-out-KSDK/m-p/712608#M9305</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I cannot&amp;nbsp;select Processor Expert box when I select Kinetis SDK as "None" with the processor MKV30 on project generation. I want to use PE components without SDK but I can't. PE box is selectable while KSDK is selected as "none" on processors like MKV31 or MK60 (I've previously used)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this processor MKV30 not supported by PE w/out KSDK or am I missing something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(KDS version is 3.2.0 and installed KSDK version 1.3.0)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Eray&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Oct 2017 12:45:21 GMT</pubDate>
    <dc:creator>eraykaraca</dc:creator>
    <dc:date>2017-10-23T12:45:21Z</dc:date>
    <item>
      <title>MKV30 using PE components w/out KSDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/MKV30-using-PE-components-w-out-KSDK/m-p/712608#M9305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I cannot&amp;nbsp;select Processor Expert box when I select Kinetis SDK as "None" with the processor MKV30 on project generation. I want to use PE components without SDK but I can't. PE box is selectable while KSDK is selected as "none" on processors like MKV31 or MK60 (I've previously used)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this processor MKV30 not supported by PE w/out KSDK or am I missing something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(KDS version is 3.2.0 and installed KSDK version 1.3.0)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Eray&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Oct 2017 12:45:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/MKV30-using-PE-components-w-out-KSDK/m-p/712608#M9305</guid>
      <dc:creator>eraykaraca</dc:creator>
      <dc:date>2017-10-23T12:45:21Z</dc:date>
    </item>
    <item>
      <title>Re: MKV30 using PE components w/out KSDK</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/MKV30-using-PE-components-w-out-KSDK/m-p/712609#M9306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eray,&lt;/P&gt;&lt;P&gt;the answer is that many of the 'newer' devices like the KV30 only support it in combination with the SDK, but not without. I have ported several components in the McuOnEclipse project (&lt;A class="link-titled" href="https://mcuoneclipse.com/2017/09/25/mcuoneclipse-components-25-sept-2017-release/" title="https://mcuoneclipse.com/2017/09/25/mcuoneclipse-components-25-sept-2017-release/"&gt;McuOnEclipse Components: 25-Sept-2017 Release | MCU on Eclipse&lt;/A&gt;&amp;nbsp;) so they can be used in a native way with Processor Expert, but you still have to use the SDK (or something similar) for the lowest layers. E.g. I can use it with the SDK v2 that way which is imho much better than the old SDK v1.3, see &lt;A class="link-titled" href="https://mcuoneclipse.com/2017/03/25/tutorial-using-eclipse-with-nxp-mcuxpresso-sdk-v2-and-processor-expert/" title="https://mcuoneclipse.com/2017/03/25/tutorial-using-eclipse-with-nxp-mcuxpresso-sdk-v2-and-processor-expert/"&gt;Tutorial: Using Eclipse with NXP MCUXpresso SDK v2 and Processor Expert | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Oct 2017 17:23:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/MKV30-using-PE-components-w-out-KSDK/m-p/712609#M9306</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-10-23T17:23:32Z</dc:date>
    </item>
  </channel>
</rss>