<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: Overflowing flash data issue causing MK22F51212 to hang up in I2C.</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Overflowing-flash-data-issue-causing-MK22F51212-to-hang-up-in/m-p/708116#M9247</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update on this issue: Turns out in the debugger settings the target type was marked as the MK22F12810 version which caused this issue. This is now solved.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Oct 2017 15:04:17 GMT</pubDate>
    <dc:creator>brendanmerna</dc:creator>
    <dc:date>2017-10-17T15:04:17Z</dc:date>
    <item>
      <title>Overflowing flash data issue causing MK22F51212 to hang up in I2C.</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Overflowing-flash-data-issue-causing-MK22F51212-to-hang-up-in/m-p/708115#M9246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working a custom board with the MK22F51212 chip on it. While adding some code to it I noticed the microchip kept malfunctioning. The micro would get stuck in the I2C code in a while loop; waiting for a status flag. Retracing my steps backwards I reached some kind of flash limit. There would be no flag raised by the Kinetis IDE, but if I created 10 bytes to an array the problem would happen, if I took those 10 bytes back out the problem would stop. I also added an include file which caused the problem to happen and removing it causing it to stop.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've made sure to check&amp;nbsp;in the map file and the linker files to confirm flash size and any possible overflow issues. Judging from those files I don't see a problem. But, clearly something has to be either set up wrong or I am actually overflowing.&lt;BR /&gt;&lt;BR /&gt;Does anyone have any ideas on this or other steps to debugging I should start taking?&lt;BR /&gt;&lt;BR /&gt;Environment:&lt;BR /&gt;-Kinetis IDE&lt;BR /&gt;-KSDK 2.0&lt;/P&gt;&lt;P&gt;-MK22F51212 chip&lt;BR /&gt;-Custom board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Oct 2017 17:54:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Overflowing-flash-data-issue-causing-MK22F51212-to-hang-up-in/m-p/708115#M9246</guid>
      <dc:creator>brendanmerna</dc:creator>
      <dc:date>2017-10-16T17:54:24Z</dc:date>
    </item>
    <item>
      <title>Re: Overflowing flash data issue causing MK22F51212 to hang up in I2C.</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Overflowing-flash-data-issue-causing-MK22F51212-to-hang-up-in/m-p/708116#M9247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update on this issue: Turns out in the debugger settings the target type was marked as the MK22F12810 version which caused this issue. This is now solved.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Oct 2017 15:04:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Overflowing-flash-data-issue-causing-MK22F51212-to-hang-up-in/m-p/708116#M9247</guid>
      <dc:creator>brendanmerna</dc:creator>
      <dc:date>2017-10-17T15:04:17Z</dc:date>
    </item>
  </channel>
</rss>