<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: Reboot when try to write flash</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Reboot-when-try-to-write-flash/m-p/692055#M9090</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Denis,&lt;/P&gt;&lt;P&gt;Which board or chip ?&lt;/P&gt;&lt;P&gt;Have you test the demo code or a simple project ?&lt;/P&gt;&lt;P&gt;If still have the error , please share the project you test .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;ALice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 May 2017 03:10:14 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2017-05-25T03:10:14Z</dc:date>
    <item>
      <title>Reboot when try to write flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Reboot-when-try-to-write-flash/m-p/692054#M9089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all, im working with the Kinetis Design Studio, Version: 3.2.0. Now im programming a routine that erases and writes Flash. I took some example Code and that &lt;EM&gt;works fine&lt;/EM&gt; when i run it by singlestep "step into (F5)".&lt;/P&gt;&lt;P&gt;But when i let run it normally the MCU reboots suddenly as when he reaches the execute command:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FTFA_FSTAT = 0x80;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp; // write the CCIF Bit to clear it and start the command&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All associated Interrupts are switched off. What is different in the singlestep mode ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 May 2017 12:38:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Reboot-when-try-to-write-flash/m-p/692054#M9089</guid>
      <dc:creator>denismatt</dc:creator>
      <dc:date>2017-05-24T12:38:17Z</dc:date>
    </item>
    <item>
      <title>Re: Reboot when try to write flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Reboot-when-try-to-write-flash/m-p/692055#M9090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Denis,&lt;/P&gt;&lt;P&gt;Which board or chip ?&lt;/P&gt;&lt;P&gt;Have you test the demo code or a simple project ?&lt;/P&gt;&lt;P&gt;If still have the error , please share the project you test .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;ALice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 May 2017 03:10:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Reboot-when-try-to-write-flash/m-p/692055#M9090</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-05-25T03:10:14Z</dc:date>
    </item>
    <item>
      <title>Re: Reboot when try to write flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Reboot-when-try-to-write-flash/m-p/692056#M9091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;i tought that may be a general problem, so i didnt attach many details.&lt;/P&gt;&lt;P&gt;Curious, in singlestep mode it works fine. It seems to be a conflict, maybe the MCU try to read the next command while the flash write command is still running. I dont know if so, but the Flowchart in the Reference Manual suggest to check the CCIF Bit to check the command is finished. If &lt;EM&gt;not&lt;/EM&gt; two actions at same time are running, the next command will be done after the flash command is done and we not have to check the CCIF Bit.&lt;/P&gt;&lt;P&gt;Error bits i cannot readout, because the MCU reboots directly when it should execute the command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To my setup: I have a board, but there is another MCU implemented as i wants to work with. So i attached a MKV10Z32VLC7 directly to the NXP LPC-Link 2 Programmer and like to program baremetal. I use the "&lt;SPAN class=""&gt;KV10 Sub-Family Reference Manual" Document Number: &lt;/SPAN&gt;KV10P48M75RM. I already programmed the clock, interrupts, PWM, UART..&lt;/P&gt;&lt;P&gt;I also looked into the sample code of "SDK_2.2_MKV10Z32xxx7" and others. But in this case i didnt found anything about this theme. The code in this examples is automatic generated and often too complicated to read for me. Beseides, i like to change it for my special requirements.&lt;/P&gt;&lt;P&gt;Here my nonworking code to write flash:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SetClock75MHz();&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// Sets the system Clock to 75 MHz and the Bus Clock/Flash Clock to 25MHz&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTFA_FCNFG = 0x00;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Command Complete Interrupt and Read Collision Error Interrupt off&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while(((FTFA_FSTAT &amp;amp; 0x10) | (FTFA_FSTAT &amp;amp; 0x20)) &amp;gt; 0){}&amp;nbsp;&amp;nbsp; &amp;nbsp;// check on ACCERR und FPVIOL&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //SIM_SCGC6 |= 0x00000001;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// Clockgate enable, but not needed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;//&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; Erase&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while((FTFA_FSTAT &amp;amp; 0x80) == 0){}&amp;nbsp;&amp;nbsp; &amp;nbsp;// check CCIF Bit, whether a command is still running&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FSTAT = 0x70;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// delete all old Errorbits (also 0x30 may be correct)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FCCOB0 = 0x09;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;//load "Erase Flash Sector" Command&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FCCOB1 = 0x00;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// Adresse High Byte&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FCCOB2 = 0x7C;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// Adresse, Middle Byte&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FCCOB3 = 0x00;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// Adresse Low Byte (must be longword aligned)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FSTAT = 0x80;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// write CCIF Bit to clear it and execute the command&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //while((FTFA_FSTAT &amp;amp; 0x80) != 0){Wait(5);}&amp;nbsp;&amp;nbsp; &amp;nbsp;// from a forum, its needly ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while((FTFA_FSTAT &amp;amp; 0x80) == 0){}&amp;nbsp;&amp;nbsp; &amp;nbsp;// check CCIF Bit&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Write&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;while((FTFA_FSTAT &amp;amp; 0x80) == 0){}&amp;nbsp;&amp;nbsp; &amp;nbsp;// check CCIF Bit, whether a command is still running&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FSTAT = 0x70;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // delete all old Errorbits&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FCCOB0 = 0x06;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// load "Program Longword" Command&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FCCOB1 = 0x00;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// Adresse High Byte&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FCCOB2 = 0x7C;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// Adresse, Middle Byte&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FCCOB3 = 0x00;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// Adresse Low Byte (must be longword aligned)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FCCOB4 = 0xAB;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// load 4. Byte &lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FCCOB5 = 0xCD;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// load 3. Byte &lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FCCOB6 = 0xEF;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// load 2. Byte &lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FCCOB7 = 0x01;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// load 1. Byte &lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;FTFA_FSTAT = 0x80;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// write CCIF Bit to clear it and execute the command&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while((FTFA_FSTAT &amp;amp; 0x80) == 0){}&amp;nbsp;&amp;nbsp; &amp;nbsp;// check CCIF Bit &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried with the associated enabled interrupt (and an IRQ Handler Routine):&lt;/P&gt;&lt;P&gt;NVIC_EnableIRQ(5);&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;// enable Interrupt Vektor&lt;BR /&gt;FTFA_FCNFG = 0x80;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Command Complete Interrupt &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 May 2017 06:59:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Reboot-when-try-to-write-flash/m-p/692056#M9091</guid>
      <dc:creator>denismatt</dc:creator>
      <dc:date>2017-05-25T06:59:48Z</dc:date>
    </item>
    <item>
      <title>Re: Reboot when try to write flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Reboot-when-try-to-write-flash/m-p/692057#M9092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Denis,&lt;/P&gt;&lt;P&gt;- Please first run the flash demo under SDKv2.2 to check whether can work well.&lt;/P&gt;&lt;P&gt;If can't whether can change another debug mode to run.&lt;/P&gt;&lt;P&gt;If it work well, please refer to the code to check your code.&lt;/P&gt;&lt;P&gt;- There is FLASH driver &lt;A class="link-titled" href="http://www.nxp.com/search?client=nxp_search_all_results&amp;amp;site=nxp_en&amp;amp;proxystylesheet=nxp_search_style_fe&amp;amp;sort=date%3AD%3AL%3Ad1&amp;amp;oe=UTF-8&amp;amp;ie=UTF-8&amp;amp;ud=1&amp;amp;output=xml_no_dtd&amp;amp;exclude_apps=1&amp;amp;callback=ss_show&amp;amp;lang_cd=en&amp;amp;filter=0&amp;amp;getfields=*&amp;amp;baseUrl=%2F%2Fwww.nxp.com%2Fwebapp&amp;amp;SEARCH_OPERATOR=Contains&amp;amp;attempt=-1&amp;amp;rc=1&amp;amp;hl=en&amp;amp;dnavs=&amp;amp;q=c90tfs_flash_driver" title="http://www.nxp.com/search?client=nxp_search_all_results&amp;amp;site=nxp_en&amp;amp;proxystylesheet=nxp_search_style_fe&amp;amp;sort=date%3AD%3AL%3Ad1&amp;amp;oe=UTF-8&amp;amp;ie=UTF-8&amp;amp;ud=1&amp;amp;output=xml_no_dtd&amp;amp;exclude_apps=1&amp;amp;callback=ss_show&amp;amp;lang_cd=en&amp;amp;filter=0&amp;amp;getfields=*&amp;amp;baseUrl=%2F%2Fwww.nxp.com%2Fwebapp&amp;amp;SEARCH_OPERATOR=Contains&amp;amp;attempt=-1&amp;amp;rc=1&amp;amp;hl=en&amp;amp;dnavs=&amp;amp;q=c90tfs_flash_driver"&gt;Search Results: c90tfs_flash_driver&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20162iF31634E078376E81/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;it includes flash demo about MKV10Z32xxx4, (under IAR IDE), you can refer to the code to check your code too.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_5.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20210i4E330FAAF717DD7A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;- For I will have holiday from 5.27 to 5.28 , after I come to work , if you still have question about this , I will continue&lt;/P&gt;&lt;P&gt;help .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 May 2017 10:11:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Reboot-when-try-to-write-flash/m-p/692057#M9092</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-05-26T10:11:30Z</dc:date>
    </item>
    <item>
      <title>Re: Reboot when try to write flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Reboot-when-try-to-write-flash/m-p/692058#M9093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I know this is an old thread, but for anyone stumbling onto this one, I encountered a similar issue.&amp;nbsp; I happen to be using an MKV30 bare chip vs a dev kit, but the issue is the same.&amp;nbsp; What I found, and is stated in the manual, but not obvious due to teh relative location in the manual of this information, is that flash access is not allowed in HSRUN mode, or VLP mode.&amp;nbsp; In the case of HSRUN mode, an ACCERR error will be flagged in FSTAT register, where in VLP mode, flash commands are ignored.&amp;nbsp; I found in HSRUN mode, with the debugger attached, I do indeed trigger resets as a result of the Flash Access Error (ACCERR).&amp;nbsp; I hope this might help others.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;JW&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 18:57:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Reboot-when-try-to-write-flash/m-p/692058#M9093</guid>
      <dc:creator>josephwalsh</dc:creator>
      <dc:date>2017-10-12T18:57:56Z</dc:date>
    </item>
  </channel>
</rss>