<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SIM_UID with UART (without printf) in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/SIM-UID-with-UART-without-printf/m-p/679008#M8978</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Arvind,&lt;/P&gt;&lt;P&gt;If your project is baremetal without KSDK, you need overwrite the functions of "_write()" and "_read()",&lt;/P&gt;&lt;P&gt;also configure the UART you want to use . About how to write, you can copy the code of Processor Expert.&lt;/P&gt;&lt;P&gt;I recommend you refer to this doc：&amp;nbsp; &lt;A href="https://community.nxp.com/docs/DOC-104349"&gt;How to use printf() to print string to Console and UART in KDS2.0&lt;/A&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;the part of “2.3 Use printf() in Bare Board Project ”&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18834i2DCFE562077DCAA6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;There is also a demo about use printf() in baremetal project. this is for KDSv2.0, while the method is the same&lt;/P&gt;&lt;P&gt;with KDS3.0 , just copy the files of the below :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18879i73A89673ECE97A04/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 May 2017 07:52:42 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2017-05-16T07:52:42Z</dc:date>
    <item>
      <title>SIM_UID with UART (without printf)</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/SIM-UID-with-UART-without-printf/m-p/679007#M8977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I need help sending the SIM_UID to UART&amp;nbsp;without using printf. We are not using processor expert, we use only the baremetal drivers. The IDE is KDS3.0.&lt;/P&gt;&lt;P&gt;Can anyone please help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 May 2017 04:20:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/SIM-UID-with-UART-without-printf/m-p/679007#M8977</guid>
      <dc:creator>armaram</dc:creator>
      <dc:date>2017-05-15T04:20:30Z</dc:date>
    </item>
    <item>
      <title>Re: SIM_UID with UART (without printf)</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/SIM-UID-with-UART-without-printf/m-p/679008#M8978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Arvind,&lt;/P&gt;&lt;P&gt;If your project is baremetal without KSDK, you need overwrite the functions of "_write()" and "_read()",&lt;/P&gt;&lt;P&gt;also configure the UART you want to use . About how to write, you can copy the code of Processor Expert.&lt;/P&gt;&lt;P&gt;I recommend you refer to this doc：&amp;nbsp; &lt;A href="https://community.nxp.com/docs/DOC-104349"&gt;How to use printf() to print string to Console and UART in KDS2.0&lt;/A&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;the part of “2.3 Use printf() in Bare Board Project ”&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18834i2DCFE562077DCAA6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;There is also a demo about use printf() in baremetal project. this is for KDSv2.0, while the method is the same&lt;/P&gt;&lt;P&gt;with KDS3.0 , just copy the files of the below :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18879i73A89673ECE97A04/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 May 2017 07:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/SIM-UID-with-UART-without-printf/m-p/679008#M8978</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-05-16T07:52:42Z</dc:date>
    </item>
  </channel>
</rss>