<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックDemo eGUI(D4D) project for KDS.</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Demo-eGUI-D4D-project-for-KDS/m-p/662169#M8755</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've successfully compiled and run an eGUI demo project&amp;nbsp; for IAR. Now I'd like to run it on KDS. I'm struggling for two weeks to get it running - no luck. I include all needed files and configure peripherals - all as for the IAR project - and it compiles OK, without errors or warnings. But when I run, it eventually gets some exceptions and gets to Default Handler. I even can not to debug it - it's not traceable - can't see the cause of the problem in the debug perspective.&lt;/P&gt;&lt;P&gt;Can NXP team provide a working demo project for KDS? Is it so hard? Is it to much to ask?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Oct 2016 10:09:30 GMT</pubDate>
    <dc:creator>john71</dc:creator>
    <dc:date>2016-10-24T10:09:30Z</dc:date>
    <item>
      <title>Demo eGUI(D4D) project for KDS.</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Demo-eGUI-D4D-project-for-KDS/m-p/662169#M8755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've successfully compiled and run an eGUI demo project&amp;nbsp; for IAR. Now I'd like to run it on KDS. I'm struggling for two weeks to get it running - no luck. I include all needed files and configure peripherals - all as for the IAR project - and it compiles OK, without errors or warnings. But when I run, it eventually gets some exceptions and gets to Default Handler. I even can not to debug it - it's not traceable - can't see the cause of the problem in the debug perspective.&lt;/P&gt;&lt;P&gt;Can NXP team provide a working demo project for KDS? Is it so hard? Is it to much to ask?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Oct 2016 10:09:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Demo-eGUI-D4D-project-for-KDS/m-p/662169#M8755</guid>
      <dc:creator>john71</dc:creator>
      <dc:date>2016-10-24T10:09:30Z</dc:date>
    </item>
  </channel>
</rss>