<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: printf Through UART0</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-Through-UART0/m-p/662042#M8747</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jace,&lt;/P&gt;&lt;P&gt;If you use the KSDK1.3 +PE， you only need add the component of "fsl_debug_console",&lt;/P&gt;&lt;P&gt;then configure UART0 port and baud rate ,it can use printf*() to UART0 .&lt;/P&gt;&lt;P&gt;About the detail you can refer to this DOC : &lt;A href="https://community.nxp.com/docs/DOC-104349"&gt;How to use printf() to print string to Console and UART in KDS2.0&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;only need refer to the part of this DOC:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12749iD00EFB137AAE77B5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Feb 2017 06:27:54 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2017-02-03T06:27:54Z</dc:date>
    <item>
      <title>printf Through UART0</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-Through-UART0/m-p/662040#M8745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using mk22fv512vlk12 and Kinetis Design Studio Version: 3.2.0&lt;/P&gt;&lt;P&gt;SDK 1.3.0 processor expert.&lt;/P&gt;&lt;P&gt;how do I rough printf to output through the UART0 Console?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am sure this has been done can anyone direct me to the proper post or answer directly?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Feb 2017 18:55:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-Through-UART0/m-p/662040#M8745</guid>
      <dc:creator>jacewalton</dc:creator>
      <dc:date>2017-02-01T18:55:10Z</dc:date>
    </item>
    <item>
      <title>Re: printf Through UART0</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-Through-UART0/m-p/662041#M8746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jace:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you compiled the hello_world example in the SDK's boards/.../demo_apps directory? &amp;nbsp;If so, you'll&amp;nbsp;notice that the SDK defines a PRINTF() macro that behaves like the "ordinary" printf(), but specifically directs its output to UART0, or more properly, whatever the debug console is defined to be in your project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suggest you try compiling the hello_world demo as a starter. &amp;nbsp;Hope this helps!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Feb 2017 20:47:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-Through-UART0/m-p/662041#M8746</guid>
      <dc:creator>robertpoor</dc:creator>
      <dc:date>2017-02-01T20:47:58Z</dc:date>
    </item>
    <item>
      <title>Re: printf Through UART0</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-Through-UART0/m-p/662042#M8747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jace,&lt;/P&gt;&lt;P&gt;If you use the KSDK1.3 +PE， you only need add the component of "fsl_debug_console",&lt;/P&gt;&lt;P&gt;then configure UART0 port and baud rate ,it can use printf*() to UART0 .&lt;/P&gt;&lt;P&gt;About the detail you can refer to this DOC : &lt;A href="https://community.nxp.com/docs/DOC-104349"&gt;How to use printf() to print string to Console and UART in KDS2.0&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;only need refer to the part of this DOC:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/12749iD00EFB137AAE77B5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 06:27:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/printf-Through-UART0/m-p/662042#M8747</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-02-03T06:27:54Z</dc:date>
    </item>
  </channel>
</rss>