<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design StudioのトピックRe: No UART Tx on one pin using Processor Expert</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/No-UART-Tx-on-one-pin-using-Processor-Expert/m-p/654504#M8568</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jorge,&lt;/P&gt;&lt;P&gt;Yep that would be it. Not sure how I missed it in the datasheet. That's what I get for "rapid prototyping" lol.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Dec 2016 17:21:31 GMT</pubDate>
    <dc:creator>mrentz</dc:creator>
    <dc:date>2016-12-08T17:21:31Z</dc:date>
    <item>
      <title>No UART Tx on one pin using Processor Expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/No-UART-Tx-on-one-pin-using-Processor-Expert/m-p/654500#M8564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm new to KDS and processor expert and I'm trying to get the UART working on a new design. I can't seem to get the UART Tx to work on one of the available pins (PTA3) but I can if I mux it to the other possible pin for that peripheral (PTB1).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I run the code the pin always stays logic low when using PTA3. If I just change the pin muxing using the hardware configuration tools it works fine on PTB1.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Receiving works fine using the PTA2 port so it seems I've set it up correctly.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Has anyone else seen something similar or maybe could give some pointers on how to troubleshoot this?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;MCU: MKE06Z128VLH4&lt;/P&gt;&lt;P&gt;KDS version: 3.2.0&lt;/P&gt;&lt;P&gt;Debugger: Multilink Universal FX&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Dec 2016 01:37:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/No-UART-Tx-on-one-pin-using-Processor-Expert/m-p/654500#M8564</guid>
      <dc:creator>mrentz</dc:creator>
      <dc:date>2016-12-07T01:37:12Z</dc:date>
    </item>
    <item>
      <title>Re: No UART Tx on one pin using Processor Expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/No-UART-Tx-on-one-pin-using-Processor-Expert/m-p/654501#M8565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;What about your board, the custom board or demo board FRDM-KE06 ?&lt;/P&gt;&lt;P&gt;I test on FRDM-KE06, UART0, the TX-PTA3 can work well , i also attached my project.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15346iA53B398C1221323F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15388i6D75BE7D869754CE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If you also use this board , please be sure R47 and R39 is connected (be default this is disconnected).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/15432i06ECDC9BF7F86A4B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If you use the custom board , could you please change another chip to have a try .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Dec 2016 03:49:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/No-UART-Tx-on-one-pin-using-Processor-Expert/m-p/654501#M8565</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2016-12-07T03:49:29Z</dc:date>
    </item>
    <item>
      <title>Re: No UART Tx on one pin using Processor Expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/No-UART-Tx-on-one-pin-using-Processor-Expert/m-p/654502#M8566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;It is a custom board and the UART is set up similar to what you have. I've now tried your project with no luck. I've also tried another chip with no success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The weird part is that I can get the Rx to work with the settings I'm using and Tx works on PTB1. I will try to build another board tomorrow with only the necessary components to see if something is causing the pin to malfunction.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2016 16:11:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/No-UART-Tx-on-one-pin-using-Processor-Expert/m-p/654502#M8566</guid>
      <dc:creator>mrentz</dc:creator>
      <dc:date>2016-12-08T16:11:38Z</dc:date>
    </item>
    <item>
      <title>Re: No UART Tx on one pin using Processor Expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/No-UART-Tx-on-one-pin-using-Processor-Expert/m-p/654503#M8567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matthew,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You might be missing a pull-up resistor. PTA3 is a true open-drain pin as output as noted in the manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11610i335B0377B40D93A7/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you need an external pull-up resistor to get a signal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2016 16:34:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/No-UART-Tx-on-one-pin-using-Processor-Expert/m-p/654503#M8567</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-12-08T16:34:17Z</dc:date>
    </item>
    <item>
      <title>Re: No UART Tx on one pin using Processor Expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/No-UART-Tx-on-one-pin-using-Processor-Expert/m-p/654504#M8568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Jorge,&lt;/P&gt;&lt;P&gt;Yep that would be it. Not sure how I missed it in the datasheet. That's what I get for "rapid prototyping" lol.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2016 17:21:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/No-UART-Tx-on-one-pin-using-Processor-Expert/m-p/654504#M8568</guid>
      <dc:creator>mrentz</dc:creator>
      <dc:date>2016-12-08T17:21:31Z</dc:date>
    </item>
  </channel>
</rss>