<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Design Studio中的主题 Re: Segger SystemView FRDM-K64F</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Segger-SystemView-FRDM-K64F/m-p/650267#M8504</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Walter,&lt;/P&gt;&lt;P&gt;Just to make sure:&lt;/P&gt;&lt;P&gt;a) you need a Segger J-Link or the J-Link firmware on the openSDA of the FRDM board&lt;/P&gt;&lt;P&gt;b) make sure you are using the same J-Link version both in KDS and the one used by Segger (mismatch of DLLs can have strange side effects). If you install the Segger software, it does ask you to update the version in KDS (use KDS v3.2.0)&lt;/P&gt;&lt;P&gt;c) Check if the RTT is properly initialized. You can do with the SEGGER RTT Viewer channel infos menu:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13532i7BA152048061FEF3/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Here you have to see the SysView channels:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13576iF521DB337C7A5EB7/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have an example project for the FRDM-K64F on GitHub (&lt;A class="link-titled" href="https://github.com/ErichStyger/mcuoneclipse/tree/master/Examples/KDS/FRDM-K64F120M/FRDM-K64F_Demo" title="https://github.com/ErichStyger/mcuoneclipse/tree/master/Examples/KDS/FRDM-K64F120M/FRDM-K64F_Demo"&gt;mcuoneclipse/Examples/KDS/FRDM-K64F120M/FRDM-K64F_Demo at master · ErichStyger/mcuoneclipse · GitHub&lt;/A&gt;&amp;nbsp;) which uses the Segger RTT with SystemView. I have attached the project to this reply as well, so you can try that project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 19 Feb 2017 16:32:13 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2017-02-19T16:32:13Z</dc:date>
    <item>
      <title>Segger SystemView FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Segger-SystemView-FRDM-K64F/m-p/650266#M8503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just received my FRDM-K64F and i am trying to get the the Segger SystemView working. The OpenSDA is installed and the debug works fine. &amp;nbsp;I followed this guide:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fmcuoneclipse.com%2F2015%2F11%2F16%2Fsegger-systemview-realtime-analysis-and-visualization-for-freertos%2F" rel="nofollow" target="_blank"&gt;Segger SystemView: Realtime Analysis and Visualization for FreeRTOS | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But it wont connect. &amp;nbsp;I am trying to run in debug mode. &amp;nbsp;Is that wrong? &amp;nbsp;Any ideas? &amp;nbsp;Thanks !&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Feb 2017 15:11:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Segger-SystemView-FRDM-K64F/m-p/650266#M8503</guid>
      <dc:creator>waltermarchewka</dc:creator>
      <dc:date>2017-02-19T15:11:26Z</dc:date>
    </item>
    <item>
      <title>Re: Segger SystemView FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Segger-SystemView-FRDM-K64F/m-p/650267#M8504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Walter,&lt;/P&gt;&lt;P&gt;Just to make sure:&lt;/P&gt;&lt;P&gt;a) you need a Segger J-Link or the J-Link firmware on the openSDA of the FRDM board&lt;/P&gt;&lt;P&gt;b) make sure you are using the same J-Link version both in KDS and the one used by Segger (mismatch of DLLs can have strange side effects). If you install the Segger software, it does ask you to update the version in KDS (use KDS v3.2.0)&lt;/P&gt;&lt;P&gt;c) Check if the RTT is properly initialized. You can do with the SEGGER RTT Viewer channel infos menu:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13532i7BA152048061FEF3/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Here you have to see the SysView channels:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/13576iF521DB337C7A5EB7/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have an example project for the FRDM-K64F on GitHub (&lt;A class="link-titled" href="https://github.com/ErichStyger/mcuoneclipse/tree/master/Examples/KDS/FRDM-K64F120M/FRDM-K64F_Demo" title="https://github.com/ErichStyger/mcuoneclipse/tree/master/Examples/KDS/FRDM-K64F120M/FRDM-K64F_Demo"&gt;mcuoneclipse/Examples/KDS/FRDM-K64F120M/FRDM-K64F_Demo at master · ErichStyger/mcuoneclipse · GitHub&lt;/A&gt;&amp;nbsp;) which uses the Segger RTT with SystemView. I have attached the project to this reply as well, so you can try that project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Feb 2017 16:32:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Segger-SystemView-FRDM-K64F/m-p/650267#M8504</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2017-02-19T16:32:13Z</dc:date>
    </item>
    <item>
      <title>Re: Segger SystemView FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Segger-SystemView-FRDM-K64F/m-p/650268#M8505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess i should have start with "i'm on a mac" lol. &amp;nbsp;I was able to get it working in Windows, however i'm still having trouble on my Mac. &amp;nbsp;I see this in the console, which leads to believe i have the openSDA set up correctly. &amp;nbsp;Whenever i run the SystemView and select the Target to start recording, i select USB, my target device, SWD and Auto detect. But i receive a "Could not connect".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;SEGGER J-Link GDB Server V5.10n Command Line Version&lt;/P&gt;&lt;P class=""&gt;JLinkARM.dll V5.10n (DLL compiled Feb 19 2016 18:41:43)&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;-----GDB Server start settings-----&lt;/P&gt;&lt;P class=""&gt;GDBInit file:&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;none&lt;/P&gt;&lt;P class=""&gt;GDB Server Listening port: &lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;2331&lt;/P&gt;&lt;P class=""&gt;SWO raw output listening port: 2332&lt;/P&gt;&lt;P class=""&gt;Terminal I/O port: &lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;2333&lt;/P&gt;&lt;P class=""&gt;Accept remote connection:&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;localhost only&lt;/P&gt;&lt;P class=""&gt;Generate logfile:&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;off&lt;/P&gt;&lt;P class=""&gt;Verify download: &lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;on&lt;/P&gt;&lt;P class=""&gt;Init regs on start:&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;on&lt;/P&gt;&lt;P class=""&gt;Silent mode: &lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;off&lt;/P&gt;&lt;P class=""&gt;Single run mode: &lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;on&lt;/P&gt;&lt;P class=""&gt;Target connection timeout: &lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;0 ms&lt;/P&gt;&lt;P class=""&gt;------J-Link related settings------&lt;/P&gt;&lt;P class=""&gt;J-Link Host interface: &lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;USB&lt;/P&gt;&lt;P class=""&gt;J-Link script: &lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;none&lt;/P&gt;&lt;P class=""&gt;J-Link settings file:&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;none&lt;/P&gt;&lt;P class=""&gt;------Target related settings------&lt;/P&gt;&lt;P class=""&gt;Target device: &lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;MK64FN1M0xxx12&lt;/P&gt;&lt;P class=""&gt;Target interface:&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;SWD&lt;/P&gt;&lt;P class=""&gt;Target interface speed:&lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;1000kHz&lt;/P&gt;&lt;P class=""&gt;Target endian: &lt;SPAN class=""&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;/SPAN&gt;little&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;Connecting to J-Link...&lt;/P&gt;&lt;P class=""&gt;J-Link is connected.&lt;/P&gt;&lt;P class=""&gt;Firmware: J-Link OpenSDA 2 compiled Feb 14 2017 15:54:11&lt;/P&gt;&lt;P class=""&gt;Hardware: V1.00&lt;/P&gt;&lt;P class=""&gt;S/N: 621000000&lt;/P&gt;&lt;P class=""&gt;Checking target voltage...&lt;/P&gt;&lt;P class=""&gt;Target voltage: 3.30 V&lt;/P&gt;&lt;P class=""&gt;Listening on TCP/IP port 2331&lt;/P&gt;&lt;P class=""&gt;Connecting to target...Connected to target&lt;/P&gt;&lt;P class=""&gt;Waiting for GDB connection...Connected to 127.0.0.1&lt;/P&gt;&lt;P class=""&gt;Reading all registers&lt;/P&gt;&lt;P class=""&gt;Read 4 bytes @ address 0x00000000 (Data = 0x20030000)&lt;/P&gt;&lt;P class=""&gt;Target interface speed set to 30 kHz&lt;/P&gt;&lt;P class=""&gt;Resetting target&lt;/P&gt;&lt;P class=""&gt;Halting target CPU...&lt;/P&gt;&lt;P class=""&gt;...Target halted (PC = 0x00000D90)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Feb 2017 02:08:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Segger-SystemView-FRDM-K64F/m-p/650268#M8505</guid>
      <dc:creator>waltermarchewka</dc:creator>
      <dc:date>2017-02-20T02:08:20Z</dc:date>
    </item>
  </channel>
</rss>