<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Loading/running Kinetis app at offset in Kinetis Design Studio</title>
    <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Loading-running-Kinetis-app-at-offset/m-p/639060#M8233</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I saw that, and wondered if it would work, but wasn't sure if the VTOR register would still be a problem. Anyhow, I will give it a try today.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Dec 2016 07:34:47 GMT</pubDate>
    <dc:creator>jarnoldbrown</dc:creator>
    <dc:date>2016-12-01T07:34:47Z</dc:date>
    <item>
      <title>Loading/running Kinetis app at offset</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Loading-running-Kinetis-app-at-offset/m-p/639058#M8231</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;#KDS #kinetis&lt;/P&gt;&lt;P&gt;I am developing an application that will ultimately have a bootloader which sits at 0x00000, and takes up 8k or so. I would like to be able to develop this app without having to include the bootloader in every iteration.&lt;/P&gt;&lt;P&gt;A while back, using an arm from Atmel, and their tools, I had the option to load the app at an offset address, and the programmer/debugger did something clever(wrote a value to the SCB-&amp;gt;VOR register?) so that I could load and run the application at a higher address, regardless of whether or not there was bootloader code at 0x0000(I think).&lt;/P&gt;&lt;P&gt;Is there a way to achieve something similar using KDS and a P&amp;amp;E Multilink?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Dec 2016 00:16:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Loading-running-Kinetis-app-at-offset/m-p/639058#M8231</guid>
      <dc:creator>jarnoldbrown</dc:creator>
      <dc:date>2016-12-01T00:16:46Z</dc:date>
    </item>
    <item>
      <title>Re: Loading/running Kinetis app at offset</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Loading-running-Kinetis-app-at-offset/m-p/639059#M8232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KDS debug configuration can set executable offset.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9675i3FBA51E261B59031/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For RAM based projects, the user may want to specify a PC value as an entry point for a secondary debug session. For FLASH based projects, please leave the Set PC checkbox and corresponding value box unchecked.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Dec 2016 07:26:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Loading-running-Kinetis-app-at-offset/m-p/639059#M8232</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-12-01T07:26:19Z</dc:date>
    </item>
    <item>
      <title>Re: Loading/running Kinetis app at offset</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Loading-running-Kinetis-app-at-offset/m-p/639060#M8233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I saw that, and wondered if it would work, but wasn't sure if the VTOR register would still be a problem. Anyhow, I will give it a try today.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Dec 2016 07:34:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Loading-running-Kinetis-app-at-offset/m-p/639060#M8233</guid>
      <dc:creator>jarnoldbrown</dc:creator>
      <dc:date>2016-12-01T07:34:47Z</dc:date>
    </item>
    <item>
      <title>Re: Loading/running Kinetis app at offset</title>
      <link>https://community.nxp.com/t5/Kinetis-Design-Studio/Loading-running-Kinetis-app-at-offset/m-p/639061#M8234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did this work for you?&amp;nbsp; I need to do the same thing and it didn't work for me...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jan 2017 22:12:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Design-Studio/Loading-running-Kinetis-app-at-offset/m-p/639061#M8234</guid>
      <dc:creator>jdavid75</dc:creator>
      <dc:date>2017-01-09T22:12:41Z</dc:date>
    </item>
  </channel>
</rss>